<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAudio lost during Encoding at Higher mbps with quick mouse movement</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Audio-lost-during-Encoding-at-Higher-mbps-with-quick-mouse/m-p/301838#M38119</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to encoding 1280x720 H264 at 14mbps.&lt;/P&gt;&lt;P&gt;Encoding content is write to SATA disk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Normally encoding is going without any issue but When we do mouse movement and audio stutters during this time.&lt;/P&gt;&lt;P&gt;If we do encoding at lower 8 mbps , encoding content has a perfect audio. no effects on mouse movement. Everything works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What could be the reason behind this issue?&lt;/P&gt;&lt;P&gt;Does VPU load effect on another peripherals?&lt;/P&gt;&lt;P&gt;Or Higher data write rate to SATA disc creates the issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Check following debug message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: ENCODING SLOW &lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;W/AudioFlinger( 2375): RecordThread: buffer overflow&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;ERROR: ENCODING SLOW &lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 21 ms total 218 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 1852&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 40 ms total 258 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 3528&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 51 ms total 309 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 4498&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 10 ms total 319 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 882&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 31 ms total 350 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 2734&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 10 ms total 360 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 882&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 70 ms total 430 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 6174&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 37 ms total 467 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 3262&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 25 ms total 492 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 2204&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 23 Mar 2014 11:42:48 GMT</pubDate>
    <dc:creator>saurabh206</dc:creator>
    <dc:date>2014-03-23T11:42:48Z</dc:date>
    <item>
      <title>Audio lost during Encoding at Higher mbps with quick mouse movement</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-lost-during-Encoding-at-Higher-mbps-with-quick-mouse/m-p/301838#M38119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to encoding 1280x720 H264 at 14mbps.&lt;/P&gt;&lt;P&gt;Encoding content is write to SATA disk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Normally encoding is going without any issue but When we do mouse movement and audio stutters during this time.&lt;/P&gt;&lt;P&gt;If we do encoding at lower 8 mbps , encoding content has a perfect audio. no effects on mouse movement. Everything works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What could be the reason behind this issue?&lt;/P&gt;&lt;P&gt;Does VPU load effect on another peripherals?&lt;/P&gt;&lt;P&gt;Or Higher data write rate to SATA disc creates the issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Check following debug message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: ENCODING SLOW &lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;W/AudioFlinger( 2375): RecordThread: buffer overflow&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;ERROR: ENCODING SLOW &lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 21 ms total 218 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 1852&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 40 ms total 258 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 3528&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 51 ms total 309 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 4498&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 10 ms total 319 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 882&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;I/FslCameraHAL( 2375): no buffer in v4l2, continue&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 31 ms total 350 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 2734&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 10 ms total 360 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 882&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 70 ms total 430 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 6174&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 37 ms total 467 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 3262&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): LEVEL: 1 FUNCTION: ProcessDataBuffer LINE: 293&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioSource::ProcessDataBuffer, GetOneFrameFromDevice Failed&lt;/P&gt;&lt;P&gt;W/audio_hw_primary( 2375): in_get_input_frames_lost 25 ms total 492 ms&lt;/P&gt;&lt;P&gt;I/OMXPlayer( 2375): AudioRecord lost bytes: 2204&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Mar 2014 11:42:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-lost-during-Encoding-at-Higher-mbps-with-quick-mouse/m-p/301838#M38119</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-03-23T11:42:48Z</dc:date>
    </item>
    <item>
      <title>Re: Audio lost during Encoding at Higher mbps with quick mouse movement</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-lost-during-Encoding-at-Higher-mbps-with-quick-mouse/m-p/301839#M38120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any suggestions to fix this issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 May 2014 10:13:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-lost-during-Encoding-at-Higher-mbps-with-quick-mouse/m-p/301839#M38120</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-05-16T10:13:37Z</dc:date>
    </item>
  </channel>
</rss>