<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMx6 BOOT_CFG4[6] Recovery Devices in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMx6-BOOT-CFG4-6-Recovery-Devices/m-p/301706#M38094</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In reference manual section 8.9 it says that if BOOT_CFG4[6] fuse is set, "the chip supports recovery devices".&lt;/P&gt;&lt;P&gt;What does it mean exactly ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If no valid U-Boot is found it try to load on recovery SPI flash ?&lt;/P&gt;&lt;P&gt;or if BOOT_CFG4[6] is set it forces load on recovery SPI flash even if valid U-Boot is in primary device ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is BOOT_CFG4[6] GPIO is taking into account in internal boot mode instead of eFuse ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for you help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yannick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 May 2014 14:28:02 GMT</pubDate>
    <dc:creator>yannickc</dc:creator>
    <dc:date>2014-05-20T14:28:02Z</dc:date>
    <item>
      <title>iMx6 BOOT_CFG4[6] Recovery Devices</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMx6-BOOT-CFG4-6-Recovery-Devices/m-p/301706#M38094</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In reference manual section 8.9 it says that if BOOT_CFG4[6] fuse is set, "the chip supports recovery devices".&lt;/P&gt;&lt;P&gt;What does it mean exactly ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If no valid U-Boot is found it try to load on recovery SPI flash ?&lt;/P&gt;&lt;P&gt;or if BOOT_CFG4[6] is set it forces load on recovery SPI flash even if valid U-Boot is in primary device ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is BOOT_CFG4[6] GPIO is taking into account in internal boot mode instead of eFuse ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for you help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yannick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 May 2014 14:28:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMx6-BOOT-CFG4-6-Recovery-Devices/m-p/301706#M38094</guid>
      <dc:creator>yannickc</dc:creator>
      <dc:date>2014-05-20T14:28:02Z</dc:date>
    </item>
    <item>
      <title>Re: iMx6 BOOT_CFG4[6] Recovery Devices</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMx6-BOOT-CFG4-6-Recovery-Devices/m-p/301707#M38095</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yannick&lt;/P&gt;&lt;P&gt;if no valid U-Boot is found it will try to load on recovery SPI flash,&lt;/P&gt;&lt;P&gt;if Uboot is valid it will boot from primary device.&lt;/P&gt;&lt;P&gt;By default If no valid U-Boot is found it try to load from USB -&lt;/P&gt;&lt;P&gt;Serial downloader (USB OTG). From sect.8.9:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"If primary boot device fails, boot ROM will try to&lt;/P&gt;&lt;P&gt;boot from recovery device using one of I2C or ECSPI ports."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 May 2014 06:47:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMx6-BOOT-CFG4-6-Recovery-Devices/m-p/301707#M38095</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-05-21T06:47:36Z</dc:date>
    </item>
    <item>
      <title>Re: iMx6 BOOT_CFG4[6] Recovery Devices</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMx6-BOOT-CFG4-6-Recovery-Devices/m-p/301708#M38096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you chip it's clear for me now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yannick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jun 2014 15:30:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMx6-BOOT-CFG4-6-Recovery-Devices/m-p/301708#M38096</guid>
      <dc:creator>yannickc</dc:creator>
      <dc:date>2014-06-03T15:30:55Z</dc:date>
    </item>
    <item>
      <title>Re: iMx6 BOOT_CFG4[6] Recovery Devices</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMx6-BOOT-CFG4-6-Recovery-Devices/m-p/301709#M38097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;chipexpert, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is SPI Flasth the only option?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would it be possible to try booting from eMMC on USDHC-3 and if there's no image, try booting from microSD on USDHC-1?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 18:35:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMx6-BOOT-CFG4-6-Recovery-Devices/m-p/301709#M38097</guid>
      <dc:creator>petertaylor</dc:creator>
      <dc:date>2014-06-10T18:35:55Z</dc:date>
    </item>
    <item>
      <title>Re: iMx6 BOOT_CFG4[6] Recovery Devices</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMx6-BOOT-CFG4-6-Recovery-Devices/m-p/301710#M38098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For i.MX6DQ there is no such option.&lt;/P&gt;&lt;P&gt;For i.MX6SDL, i.MX6SDL Reference Manual (rev.1&amp;nbsp; 5/2013)&lt;/P&gt;&lt;P&gt;sect.8.11 "SD/MMC Manufacture Mode":&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"When internal boot and recover boot (if enabled) failed, boot will go to SD/MMC&lt;/P&gt;&lt;P&gt;manufacture mode before serial download mode. In manufacture mode, one bit bus width&lt;/P&gt;&lt;P&gt;is used despite of the fuse setting.&lt;/P&gt;&lt;P&gt;In manufacture mode, SD or MMC card will be scanned on uSDHC1 and uSDHC2."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;Best regards&lt;/P&gt;&lt;P style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit;"&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jun 2014 04:05:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMx6-BOOT-CFG4-6-Recovery-Devices/m-p/301710#M38098</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-06-11T04:05:29Z</dc:date>
    </item>
  </channel>
</rss>