<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: &amp;quot;VPU blocking: timeout&amp;quot; with 5MP h264 compression using gstreamer in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/quot-VPU-blocking-timeout-quot-with-5MP-h264-compression-using/m-p/301433#M38014</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Can you share the fix please I have&amp;nbsp;mxc_vpu 2040000.vpu_fsl: VPU blocking: timeout. for jpeg-&amp;gt;yuv.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Tony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Nov 2016 15:12:39 GMT</pubDate>
    <dc:creator>tonypusok</dc:creator>
    <dc:date>2016-11-24T15:12:39Z</dc:date>
    <item>
      <title>"VPU blocking: timeout" with 5MP h264 compression using gstreamer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/quot-VPU-blocking-timeout-quot-with-5MP-h264-compression-using/m-p/301429#M38010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using sabrelite with ov5640 mipi sensors.&lt;/P&gt;&lt;P&gt;is working fine (it takes snapshot at full resolution.)&lt;/P&gt;&lt;P&gt;If i try to capture a movie at fulHd resolution 30 fps it produce ok, but if i try to make a movie at full resolution (5Mp) at 15 fps. I have the following error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mxc_vpu 2040000.vpu: VPU blocking:timeout.&lt;/P&gt;&lt;P&gt;mxc_vpu 2040000.vpu: VPU blocking:timeout.&lt;/P&gt;&lt;P&gt;mxc_vpu 2040000.vpu: VPU blocking:timeout.&lt;/P&gt;&lt;P&gt;mxc_vpu 2040000.vpu: VPU blocking:timeout.&lt;/P&gt;&lt;P&gt;mxc_vpu 2040000.vpu: VPU blocking:timeout.&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;after a while&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;mxc_vpu 2040000.vpu: fatal error: can't gate/power off when VPU is busy&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00000001&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and then the vpu seems to be blocked i have to reboot the system to have the control again. &lt;/P&gt;&lt;P&gt;I'm using the fsl-image-test as "image"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it does the same even with mpeg4 compression.&lt;/P&gt;&lt;P&gt;here the pipelines used:&lt;/P&gt;&lt;P&gt;this one is working (mode=5 mean fullHD)&lt;/P&gt;&lt;P&gt;gst-launch mfw_v4lsrc capture-mode=5 fps-n=30 ! queue ! vpuenc codec=6 ! matroskamux ! filesink location=/mnt/nfs/home/test_1080p.mkv&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this one is not:&lt;/P&gt;&lt;P&gt;gst-launch mfw_v4lsrc capture-mode=6 fps-n=15 ! queue ! vpuenc codec=6 ! matroskamux ! filesink location=/mnt/nfs/home/test_5mpix.mkv&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Omar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2014 16:12:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/quot-VPU-blocking-timeout-quot-with-5MP-h264-compression-using/m-p/301429#M38010</guid>
      <dc:creator>Selea</dc:creator>
      <dc:date>2014-03-21T16:12:21Z</dc:date>
    </item>
    <item>
      <title>Re: "VPU blocking: timeout" with 5MP h264 compression using gstreamer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/quot-VPU-blocking-timeout-quot-with-5MP-h264-compression-using/m-p/301430#M38011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;could you tell me what mode do you use? for mx6 IPU can support up to 3.2MP camera, 15fps, yuv422 format, 8 bit interface, and vpu supports up to 1080@30fps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Apr 2014 07:34:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/quot-VPU-blocking-timeout-quot-with-5MP-h264-compression-using/m-p/301430#M38011</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2014-04-09T07:34:47Z</dc:date>
    </item>
    <item>
      <title>Re: "VPU blocking: timeout" with 5MP h264 compression using gstreamer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/quot-VPU-blocking-timeout-quot-with-5MP-h264-compression-using/m-p/301431#M38012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Omar&lt;/P&gt;&lt;P&gt;Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jun 2014 08:21:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/quot-VPU-blocking-timeout-quot-with-5MP-h264-compression-using/m-p/301431#M38012</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-06-16T08:21:54Z</dc:date>
    </item>
    <item>
      <title>Re: "VPU blocking: timeout" with 5MP h264 compression using gstreamer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/quot-VPU-blocking-timeout-quot-with-5MP-h264-compression-using/m-p/301432#M38013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes thanks it seems to be solved....&lt;/P&gt;&lt;P&gt;sorry... &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jun 2014 09:40:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/quot-VPU-blocking-timeout-quot-with-5MP-h264-compression-using/m-p/301432#M38013</guid>
      <dc:creator>Selea</dc:creator>
      <dc:date>2014-06-16T09:40:41Z</dc:date>
    </item>
    <item>
      <title>Re: "VPU blocking: timeout" with 5MP h264 compression using gstreamer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/quot-VPU-blocking-timeout-quot-with-5MP-h264-compression-using/m-p/301433#M38014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Can you share the fix please I have&amp;nbsp;mxc_vpu 2040000.vpu_fsl: VPU blocking: timeout. for jpeg-&amp;gt;yuv.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Tony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Nov 2016 15:12:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/quot-VPU-blocking-timeout-quot-with-5MP-h264-compression-using/m-p/301433#M38014</guid>
      <dc:creator>tonypusok</dc:creator>
      <dc:date>2016-11-24T15:12:39Z</dc:date>
    </item>
  </channel>
</rss>