<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PF0100 SW1A/B output voltage in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1A-B-output-voltage/m-p/300783#M37793</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Muthu Nagarajan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white;"&gt;Yes, by default, the 1.375V from SW1AB_VOLT&lt;/SPAN&gt;&lt;SPAN style="background: white;"&gt; for the F3 version&lt;/SPAN&gt; &lt;SPAN style="background: white;"&gt;is in the sequence of&lt;/SPAN&gt;&lt;SPAN style="background: white;"&gt; SW1AB_SEQ&lt;/SPAN&gt;&lt;SPAN style="background: white;"&gt; =&lt;/SPAN&gt;&lt;SPAN style="background: white;"&gt; 2.&lt;/SPAN&gt;&lt;SPAN style="background: white;"&gt; This means that the &lt;/SPAN&gt;&lt;SPAN style="background: white;"&gt;PF0100 SW1A/B output voltage of 1.375V will be enabled about 0.5 to 4.0 ms &lt;/SPAN&gt;(depending on the tD4 configuration (Table 11 of the datasheet)) after the SW2 Turn-on, even if the internal LDO_ARM in the iMX6SL is enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About bypassing the internal LDO_ ARM in the i.MX6SL, yes, it is possible to bypass it for normal operation and about the &lt;SPAN style="background: white;"&gt;SW1A/B and SW1C output voltages, these are programmable from 0.300 to 1.875 V in steps of 25 mV. The output voltage set point is independently programmed for Normal, Standby, and Sleep mode by setting the SW1x[5:0], SW1xSTBY[5:0], and SW1xOFF[5:0] bits respectively. Table 41 of the data sheet shows the output voltage coding for SW1A/B or SW1C.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMPF0100 Datasheet: &lt;A href="http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf"&gt;http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 May 2014 16:21:53 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2014-05-07T16:21:53Z</dc:date>
    <item>
      <title>PF0100 SW1A/B output voltage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1A-B-output-voltage/m-p/300781#M37791</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does the PF0100 SW1A/B output voltage of 1.375V during startup (F3 option for iMX6SoloLite) assume that the internal LDO_ARM in the iMX6SL is enabled? Follow on question, Once everything has powered-up, can I reduce the PF0100 SW1A/B output to 1.2V and bypass the internal LDO_ARM in the iMX6SL for normal operation? Same question for the PF0100 SW1C output for VDD_SOC_IN and VDD_PU_IN.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Apr 2014 19:14:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1A-B-output-voltage/m-p/300781#M37791</guid>
      <dc:creator>muthunagarajan</dc:creator>
      <dc:date>2014-04-21T19:14:24Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 SW1A/B output voltage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1A-B-output-voltage/m-p/300782#M37792</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your post, however please consider moving it to the right community place (e.g. &lt;A _jive_internal="true" class="jivecontainerTT-hover-container jive-link-community-small" data-containerid="1" data-containertype="14" data-objectid="2004" data-objecttype="14" href="https://community.nxp.com/community/imx"&gt;i.MX Community&lt;/A&gt; ) to get it visible for active members.&lt;/P&gt;&lt;P&gt;For details please see general advice &lt;A _jive_internal="true" data-containerid="2001" data-containertype="14" data-objectid="99909" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99909"&gt;Where to post a Discussion?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using Freescale Community.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Apr 2014 08:46:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1A-B-output-voltage/m-p/300782#M37792</guid>
      <dc:creator>Wlodek_D_</dc:creator>
      <dc:date>2014-04-29T08:46:13Z</dc:date>
    </item>
    <item>
      <title>Re: PF0100 SW1A/B output voltage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1A-B-output-voltage/m-p/300783#M37793</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Muthu Nagarajan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white;"&gt;Yes, by default, the 1.375V from SW1AB_VOLT&lt;/SPAN&gt;&lt;SPAN style="background: white;"&gt; for the F3 version&lt;/SPAN&gt; &lt;SPAN style="background: white;"&gt;is in the sequence of&lt;/SPAN&gt;&lt;SPAN style="background: white;"&gt; SW1AB_SEQ&lt;/SPAN&gt;&lt;SPAN style="background: white;"&gt; =&lt;/SPAN&gt;&lt;SPAN style="background: white;"&gt; 2.&lt;/SPAN&gt;&lt;SPAN style="background: white;"&gt; This means that the &lt;/SPAN&gt;&lt;SPAN style="background: white;"&gt;PF0100 SW1A/B output voltage of 1.375V will be enabled about 0.5 to 4.0 ms &lt;/SPAN&gt;(depending on the tD4 configuration (Table 11 of the datasheet)) after the SW2 Turn-on, even if the internal LDO_ARM in the iMX6SL is enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About bypassing the internal LDO_ ARM in the i.MX6SL, yes, it is possible to bypass it for normal operation and about the &lt;SPAN style="background: white;"&gt;SW1A/B and SW1C output voltages, these are programmable from 0.300 to 1.875 V in steps of 25 mV. The output voltage set point is independently programmed for Normal, Standby, and Sleep mode by setting the SW1x[5:0], SW1xSTBY[5:0], and SW1xOFF[5:0] bits respectively. Table 41 of the data sheet shows the output voltage coding for SW1A/B or SW1C.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MMPF0100 Datasheet: &lt;A href="http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf"&gt;http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose Reyes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 May 2014 16:21:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0100-SW1A-B-output-voltage/m-p/300783#M37793</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2014-05-07T16:21:53Z</dc:date>
    </item>
  </channel>
</rss>