<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx28 cpu is blocked when acm modem is opened without read/write in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx28-cpu-is-blocked-when-acm-modem-is-opened-without-read-write/m-p/300139#M37664</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have striven for a few weeks but there is no good result. Isn't there anyone who can help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Mar 2014 14:18:03 GMT</pubDate>
    <dc:creator>mehmet</dc:creator>
    <dc:date>2014-03-21T14:18:03Z</dc:date>
    <item>
      <title>imx28 cpu is blocked when acm modem is opened without read/write</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-cpu-is-blocked-when-acm-modem-is-opened-without-read-write/m-p/300138#M37663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a critical problem with imx28. We use Telit HE910 module for GSM and GPS, it has 7 ACM interface under /dev/ directory and /dev/ttyACM0 is for GSM, /dev/ttyACM2 is for GPS. When we opened any 2 ports of /dev/ttyACMx, cpu is blocked for a few milliseconds. Because of imx28 has 16 bytes uart fifo, data loss would occur. The funny part is that there is no transfer, no read/write request on /dev/ttyACMx's, only opened any 2 of them. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So thanks.&lt;/P&gt;&lt;P&gt;Mehmetmet&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Mar 2014 08:51:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-cpu-is-blocked-when-acm-modem-is-opened-without-read-write/m-p/300138#M37663</guid>
      <dc:creator>mehmet</dc:creator>
      <dc:date>2014-03-20T08:51:40Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 cpu is blocked when acm modem is opened without read/write</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-cpu-is-blocked-when-acm-modem-is-opened-without-read-write/m-p/300139#M37664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have striven for a few weeks but there is no good result. Isn't there anyone who can help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2014 14:18:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-cpu-is-blocked-when-acm-modem-is-opened-without-read-write/m-p/300139#M37664</guid>
      <dc:creator>mehmet</dc:creator>
      <dc:date>2014-03-21T14:18:03Z</dc:date>
    </item>
    <item>
      <title>Re: imx28 cpu is blocked when acm modem is opened without read/write</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx28-cpu-is-blocked-when-acm-modem-is-opened-without-read-write/m-p/300140#M37665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There was discussion about AUART data loss in mainline Linux, but it was fixed in the end. You might want to take a look in there (or use mainline).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Mar 2014 04:37:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx28-cpu-is-blocked-when-acm-modem-is-opened-without-read-write/m-p/300140#M37665</guid>
      <dc:creator>MarekVasut</dc:creator>
      <dc:date>2014-03-27T04:37:46Z</dc:date>
    </item>
  </channel>
</rss>