<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Yocto Linux defconfig question</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-defconfig-question/m-p/299840#M37605</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;imx_v7_defconfig builds all the imx that are armv7: mx51, mx53 and mx6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the past we used to have a defconfig per board. Currently we tend to group the defconfigs as much as we can.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 May 2014 20:27:26 GMT</pubDate>
    <dc:creator>fabio_estevam</dc:creator>
    <dc:date>2014-05-16T20:27:26Z</dc:date>
    <item>
      <title>Yocto Linux defconfig question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-defconfig-question/m-p/299838#M37603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi There, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the LTIB 4.1.0 BSP release it was very clear which files defined the platform in the arch/mach-imx6 along with a imx6_defconfig file. However, no such luck in the Yocto 1.0.0 BSP. As far as I can tell there is only one defconfig file (imx_v7_defconfig), that confusingly enough defines&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CONFIG_SOC_IMX53=y&lt;/P&gt;&lt;P&gt;CONFIG_SOC_IMX6Q=y&lt;/P&gt;&lt;P&gt;CONFIG_SOC_IMX6SL=y&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this the correct defconfig file for a imx6qsabresd ? And if so, how can one figure that out ? How is the kernel customized if I wanted to build for an imx3 device instead ? I realize the changes to the kernel is made to make it easier to maintain and increase code-reuse and I'm sure it will all make a lot of sense to me later, but not yet. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance and have a great weekend !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Otto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 May 2014 17:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-defconfig-question/m-p/299838#M37603</guid>
      <dc:creator>ottoblom</dc:creator>
      <dc:date>2014-05-16T17:14:04Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Linux defconfig question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-defconfig-question/m-p/299839#M37604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, maybe this can help someone else - The Yocto 1.0.0 BSP uses device trees for most of the board-specific items. The top-level dts file for the imx6qsabresd is located at tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.10.17-r0/git/arch/arm/boot/dts/imx6q-sabresd.dts. Note that it in turn includes several other files. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Still confusing that the imx_v7_defconfig defines three different IMX SOCs, but maybe there are good reasons for that&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 May 2014 19:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-defconfig-question/m-p/299839#M37604</guid>
      <dc:creator>ottoblom</dc:creator>
      <dc:date>2014-05-16T19:43:23Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Linux defconfig question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-defconfig-question/m-p/299840#M37605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;imx_v7_defconfig builds all the imx that are armv7: mx51, mx53 and mx6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the past we used to have a defconfig per board. Currently we tend to group the defconfigs as much as we can.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 May 2014 20:27:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-defconfig-question/m-p/299840#M37605</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2014-05-16T20:27:26Z</dc:date>
    </item>
  </channel>
</rss>