<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic gpu-sdk1008.tgz samples aborting in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/gpu-sdk1008-tgz-samples-aborting/m-p/299749#M37596</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The sample programs in the GPUSDK abort almost immediately when I try to run them on my i.MX537.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ ./es1_lesson02_fbdev &lt;/P&gt;&lt;P&gt;chooseconfig, &lt;/P&gt;&lt;P&gt;es1_lesson02_fbdev: lesson02_imx.c:182: int init(): Assertion `eglGetError() == 0x3000' failed.&lt;/P&gt;&lt;P&gt;Aborted&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ ./vg_audiohmi_fbdev &lt;/P&gt;&lt;P&gt;Freescale VG HMI Demo&lt;/P&gt;&lt;P&gt;++Starting Initialization&lt;/P&gt;&lt;P&gt;*eglInitialize &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; eglBindAPI &lt;/P&gt;&lt;P&gt;*eglChooseConfig &lt;/P&gt;&lt;P&gt;EGL Fail = EGL_NOT_INITIALIZED (0x3001) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running on an i.MX537 using an ltib image I built based on a Freescale 2.6.35 kernel.&amp;nbsp; The GPU shared libraries in my ltib rootfs came from the amd-gpu-bin-mx51-11.09.01 package.&amp;nbsp; I compiled the GPUSDK samples to use the frame buffer because my image does not have X11 nor do I want it.&amp;nbsp; I configured the GPUSDK buildvars.mk as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FSL_PLATFORM = MX53&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#if building on an LTIB system, set CROSS_COMPILE as below&lt;/P&gt;&lt;P&gt;CROSS_COMPILE = /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#directory with GLES, VG, and EGL headers&lt;/P&gt;&lt;P&gt;FSL_GPU_INC =&amp;nbsp; $(LTIB_ROOTFS)/usr/include&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#all other system headers&lt;/P&gt;&lt;P&gt;FSL_PLATFORM_INC = $(LTIB_ROOTFS)/usr/include&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#location of libEGL.so, etc.&lt;/P&gt;&lt;P&gt;FSL_GPU_LIB = $(LTIB_ROOTFS)/usr/lib&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#location of other system libraries&lt;/P&gt;&lt;P&gt;FSL_PLATFORM_LIB = $(LTIB_ROOTFS)/usr/lib&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C2D_FLAGS = -l2dz430&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Something must be very wrong for EGL to fail.&amp;nbsp; Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Frank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Mar 2014 17:38:47 GMT</pubDate>
    <dc:creator>fvasquez</dc:creator>
    <dc:date>2014-03-19T17:38:47Z</dc:date>
    <item>
      <title>gpu-sdk1008.tgz samples aborting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gpu-sdk1008-tgz-samples-aborting/m-p/299749#M37596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The sample programs in the GPUSDK abort almost immediately when I try to run them on my i.MX537.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ ./es1_lesson02_fbdev &lt;/P&gt;&lt;P&gt;chooseconfig, &lt;/P&gt;&lt;P&gt;es1_lesson02_fbdev: lesson02_imx.c:182: int init(): Assertion `eglGetError() == 0x3000' failed.&lt;/P&gt;&lt;P&gt;Aborted&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ ./vg_audiohmi_fbdev &lt;/P&gt;&lt;P&gt;Freescale VG HMI Demo&lt;/P&gt;&lt;P&gt;++Starting Initialization&lt;/P&gt;&lt;P&gt;*eglInitialize &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; eglBindAPI &lt;/P&gt;&lt;P&gt;*eglChooseConfig &lt;/P&gt;&lt;P&gt;EGL Fail = EGL_NOT_INITIALIZED (0x3001) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running on an i.MX537 using an ltib image I built based on a Freescale 2.6.35 kernel.&amp;nbsp; The GPU shared libraries in my ltib rootfs came from the amd-gpu-bin-mx51-11.09.01 package.&amp;nbsp; I compiled the GPUSDK samples to use the frame buffer because my image does not have X11 nor do I want it.&amp;nbsp; I configured the GPUSDK buildvars.mk as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FSL_PLATFORM = MX53&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#if building on an LTIB system, set CROSS_COMPILE as below&lt;/P&gt;&lt;P&gt;CROSS_COMPILE = /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-none-linux-gnueabi-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#directory with GLES, VG, and EGL headers&lt;/P&gt;&lt;P&gt;FSL_GPU_INC =&amp;nbsp; $(LTIB_ROOTFS)/usr/include&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#all other system headers&lt;/P&gt;&lt;P&gt;FSL_PLATFORM_INC = $(LTIB_ROOTFS)/usr/include&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#location of libEGL.so, etc.&lt;/P&gt;&lt;P&gt;FSL_GPU_LIB = $(LTIB_ROOTFS)/usr/lib&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#location of other system libraries&lt;/P&gt;&lt;P&gt;FSL_PLATFORM_LIB = $(LTIB_ROOTFS)/usr/lib&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C2D_FLAGS = -l2dz430&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Something must be very wrong for EGL to fail.&amp;nbsp; Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Frank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Mar 2014 17:38:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gpu-sdk1008-tgz-samples-aborting/m-p/299749#M37596</guid>
      <dc:creator>fvasquez</dc:creator>
      <dc:date>2014-03-19T17:38:47Z</dc:date>
    </item>
    <item>
      <title>Re: gpu-sdk1008.tgz samples aborting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gpu-sdk1008-tgz-samples-aborting/m-p/299750#M37597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Frank Vasquez,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your post, however please consider moving it to the right community place (e.g. &lt;A href="https://community.nxp.com/space/2004"&gt;i.MX Community&lt;/A&gt; ) for better visibility.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For details please see general advice &lt;/SPAN&gt;&lt;A class="jive-link-wiki-small" data-containerid="2001" data-containertype="14" data-objectid="99909" data-objecttype="102" href="https://community.freescale.com/docs/DOC-99909"&gt;https://community.freescale.com/docs/DOC-99909&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using Freescale Community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Wlodek_D. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Mar 2014 09:07:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gpu-sdk1008-tgz-samples-aborting/m-p/299750#M37597</guid>
      <dc:creator>Wlodek_D_</dc:creator>
      <dc:date>2014-03-20T09:07:43Z</dc:date>
    </item>
    <item>
      <title>Re: gpu-sdk1008.tgz samples aborting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gpu-sdk1008-tgz-samples-aborting/m-p/299751#M37598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;please refer this: &lt;A _jive_internal="true" href="https://community.nxp.com/message/302919#302919" title="https://community.freescale.com/message/302919#302919"&gt;https://community.freescale.com/message/302919#302919&lt;/A&gt;&lt;/P&gt;&lt;P&gt;If still not work, please let me know.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2014 03:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gpu-sdk1008-tgz-samples-aborting/m-p/299751#M37598</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2014-03-21T03:33:27Z</dc:date>
    </item>
    <item>
      <title>Re: gpu-sdk1008.tgz samples aborting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gpu-sdk1008-tgz-samples-aborting/m-p/299752#M37599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I read that thread before posting here.&amp;nbsp; I built my own image using ltib and have the amd-gpu-bin-mx51 package rather than amd-gpu-x11-bin-mx51 selected.&amp;nbsp; The amd-gpu-bin-mx51 package is supposedly the one without X11.&amp;nbsp; I do suspect a problem with my kernel configuration though.&amp;nbsp; Namely, "MXC GPU support" is not selected under "Device Drivers".&amp;nbsp; Will let you know if enabling that fixes my problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Mar 2014 00:42:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gpu-sdk1008-tgz-samples-aborting/m-p/299752#M37599</guid>
      <dc:creator>fvasquez</dc:creator>
      <dc:date>2014-03-22T00:42:57Z</dc:date>
    </item>
    <item>
      <title>Re: gpu-sdk1008.tgz samples aborting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/gpu-sdk1008-tgz-samples-aborting/m-p/299753#M37600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Enabling the following setting kernel configuration option during ./ltib -c fixed my problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Device Drivers --&amp;gt; MXC Support drivers ---&amp;gt; MXC GPU Support ---&amp;gt; MXC GPU Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This step is described in section 16.6 of mx53_start_linux.pdf from L2.6.35_11.09.01_ER_docs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Mar 2014 17:09:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/gpu-sdk1008-tgz-samples-aborting/m-p/299753#M37600</guid>
      <dc:creator>fvasquez</dc:creator>
      <dc:date>2014-03-24T17:09:39Z</dc:date>
    </item>
  </channel>
</rss>