<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How could I configure a GPIO as an input?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299489#M37547</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your detailed answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I have found these entries:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;iomux-mx6q.h&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MX6Q_PAD_GPIO_2_GPIO_1_2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IOMUX_PAD(0x0604, 0x0234, 5, 0x0000, 0, 0)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That seems right.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;board-mx6q_sabresd.h&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static iomux_v3_cfg_t mx6q_sabresd_pads[] = {&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;MX6Q_PAD_GPIO_2_GPIO_1_2.&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That also seems right.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;board-mx6q_sabresd.c&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;#define SABRESD_USR_DEF_RED_LED&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IMX_GPIO_NR(1, 2)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, I think something like gpio:output(SABRESD_USR_DEF_RED_LED) has to follow in this file.&lt;/P&gt;&lt;P&gt;However there ist not such an entry. Actually it is configured as an output. We can see this due to the led.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you know why these function calls are missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if (gpio_request(SABRESD_TEST_PIN, "TEST PIN") &amp;lt; 0) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pr_err("%s() can't get TEST PIN", __func__);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;gpio_direction_output(SABRESD_TEST_PIN, 1); // output high&lt;/P&gt;&lt;P&gt;or &lt;/P&gt;&lt;P&gt;gpio_direction_input(SABRESD_TEST_PIN); // input&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Perhaps I have understood something wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 May 2014 10:34:59 GMT</pubDate>
    <dc:creator>janr_</dc:creator>
    <dc:date>2014-05-16T10:34:59Z</dc:date>
    <item>
      <title>How could I configure a GPIO as an input?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299485#M37543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i have to figure out how to configure an gpio register as an input.&lt;/P&gt;&lt;P&gt;We use Linux verrsion 3.0.35_4.1.0_130816.&lt;/P&gt;&lt;P&gt;I think board_mx6q_sabresd.c and board_mx6q_sabresd.h are the most important files for the configuration.&lt;/P&gt;&lt;P&gt;I just want to understand where all these gpios are configuraed as inputs or outputs.&lt;/P&gt;&lt;P&gt;In the headerfile there is a MX6Q_PAD_GPIO_1_2. But I can't find these definition in the .c-file.&lt;/P&gt;&lt;P&gt;The names of the gpios seems to change from file to file and I don't know how to go on...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then there is a gpio.txt, which says to use the gpio_input() and gpio_output() functions. However MX6Q_PAD_GPIO_1_2 is never used as a&lt;/P&gt;&lt;P&gt;parameter in one of these two funtions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking forward to any help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 May 2014 07:54:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299485#M37543</guid>
      <dc:creator>janr_</dc:creator>
      <dc:date>2014-05-16T07:54:38Z</dc:date>
    </item>
    <item>
      <title>Re: How could I configure a GPIO as an input?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299486#M37544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To configuration a PAD to GPIO as an input or as an output mode, can follow up below steps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. set SoC PAD to GPIO mode in board_mx6q_sabresd.h&lt;/P&gt;&lt;P&gt;2. confirm which GPIO group and number belong to by check iMX6 datasheet or by Tool (IOMux Tool v3.2.1.0)&lt;/P&gt;&lt;P&gt;3. add new define in board_mx6q_sabresd.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define SABRESD_TEST_PIN&amp;nbsp;&amp;nbsp;&amp;nbsp; IMX_GPIO_NR(GPIO_GROUP, GPIO_NUMBER)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4. request GPIO by using kernel API&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if (gpio_request(SABRESD_TEST_PIN, "TEST PIN") &amp;lt; 0) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pr_err("%s() can't get TEST PIN", __func__);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;gpio_direction_output(SABRESD_TEST_PIN, 1); // output high&lt;/P&gt;&lt;P&gt;or &lt;/P&gt;&lt;P&gt;gpio_direction_input(SABRESD_TEST_PIN); // input&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can keep trace source code to get full picture in kernel source codes.&lt;/P&gt;&lt;P&gt;Hope this information help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 May 2014 08:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299486#M37544</guid>
      <dc:creator>rickchu</dc:creator>
      <dc:date>2014-05-16T08:39:45Z</dc:date>
    </item>
    <item>
      <title>Re: How could I configure a GPIO as an input?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299487#M37545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Concerning the first step:&lt;/P&gt;&lt;P&gt;1. set SoC PAD to GPIO mode in board_mx6q_sabresd.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the board_mx6q_sbresd.h, I can add a variable like "MX6Q_PAD_GPIO_2_GPIO_1_2" to an array.&lt;BR /&gt;Perhaps do you mean iomux-mx6q.h?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;There I can configure it like this:&lt;/P&gt;&lt;P&gt;#define _MX6Q_PAD_GPIO_7_GPIO_1_7&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;IOMUX_PAD(ox0610, 0x0240, 5, 0x0000, 0, 0)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 May 2014 09:39:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299487#M37545</guid>
      <dc:creator>janr_</dc:creator>
      <dc:date>2014-05-16T09:39:52Z</dc:date>
    </item>
    <item>
      <title>Re: Re: How could I configure a GPIO as an input?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299488#M37546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes, in your example "&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;MX6Q_PAD_GPIO_2_GPIO_1_2&lt;/SPAN&gt;" means to configuration "PAD_GPIO_2" as an GPIO mode in GPIO bank 1, bit 2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you trace in iomux-mx6q.h, you can found that PAD_GPIO_2 can be configuration to other function too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define&amp;nbsp; MX6Q_PAD_GPIO_2__ESAI1_FST \&lt;/P&gt;&lt;P&gt;#define&amp;nbsp; MX6Q_PAD_GPIO_2__OBSERVE_MUX_OBSRV_INT_OUT2 \&lt;/P&gt;&lt;P&gt;#define&amp;nbsp; MX6Q_PAD_GPIO_2__KPP_ROW_6 \&lt;/P&gt;&lt;P&gt;#define&amp;nbsp; MX6Q_PAD_GPIO_2__CCM_CCM_OUT_1 \&lt;/P&gt;&lt;P&gt;#define&amp;nbsp; MX6Q_PAD_GPIO_2__CSU_CSU_ALARM_AUT_0 \&lt;/P&gt;&lt;P&gt;#define&amp;nbsp; MX6Q_PAD_GPIO_2__GPIO_1_2 \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (_MX6Q_PAD_GPIO_2__GPIO_1_2 | MUX_PAD_CTRL(NO_PAD_CTRL))&lt;/P&gt;&lt;P&gt;#define&amp;nbsp; MX6Q_PAD_GPIO_2__USDHC2_WP \&lt;/P&gt;&lt;P&gt;#define&amp;nbsp; MX6Q_PAD_GPIO_2__MLB_MLBDAT \&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define _MX6Q_PAD_GPIO_2__GPIO_1_2&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; IOMUX_PAD(&lt;SPAN style="color: #ff0000;"&gt;0x0604&lt;/SPAN&gt;, &lt;SPAN style="color: #ff0000;"&gt;0x0234&lt;/SPAN&gt;, 5, 0x0000, 0, 0)&lt;/P&gt;&lt;P&gt;=============================================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you look in iomux-v3.h, you can found what IOMUX_PAD() doing.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44226iE90E37DAFDB18D5F/image-size/large?v=v2&amp;amp;px=999" title="00.jpg" alt="00.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;offset: 0x604&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44278i2D8DF15F6790F130/image-size/large?v=v2&amp;amp;px=999" title="01.jpg" alt="01.jpg" /&gt;&lt;/span&gt;&lt;BR /&gt;offset: 0x234&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 May 2014 10:09:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299488#M37546</guid>
      <dc:creator>rickchu</dc:creator>
      <dc:date>2014-05-16T10:09:48Z</dc:date>
    </item>
    <item>
      <title>Re: How could I configure a GPIO as an input?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299489#M37547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your detailed answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I have found these entries:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;iomux-mx6q.h&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MX6Q_PAD_GPIO_2_GPIO_1_2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IOMUX_PAD(0x0604, 0x0234, 5, 0x0000, 0, 0)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That seems right.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;board-mx6q_sabresd.h&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static iomux_v3_cfg_t mx6q_sabresd_pads[] = {&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;MX6Q_PAD_GPIO_2_GPIO_1_2.&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That also seems right.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;board-mx6q_sabresd.c&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;#define SABRESD_USR_DEF_RED_LED&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IMX_GPIO_NR(1, 2)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, I think something like gpio:output(SABRESD_USR_DEF_RED_LED) has to follow in this file.&lt;/P&gt;&lt;P&gt;However there ist not such an entry. Actually it is configured as an output. We can see this due to the led.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you know why these function calls are missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if (gpio_request(SABRESD_TEST_PIN, "TEST PIN") &amp;lt; 0) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pr_err("%s() can't get TEST PIN", __func__);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;gpio_direction_output(SABRESD_TEST_PIN, 1); // output high&lt;/P&gt;&lt;P&gt;or &lt;/P&gt;&lt;P&gt;gpio_direction_input(SABRESD_TEST_PIN); // input&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Perhaps I have understood something wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 May 2014 10:34:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299489#M37547</guid>
      <dc:creator>janr_</dc:creator>
      <dc:date>2014-05-16T10:34:59Z</dc:date>
    </item>
    <item>
      <title>Re: Re: How could I configure a GPIO as an input?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299490#M37548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;SABRESD_TEST_PIN&lt;/SPAN&gt;" is an example not really in source code, sorry confuse you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for your another question, you can found "SABRESD_BT_RESET" using the same GPIO define, and it has assigned to control Bluetooth.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;#define SABRESD_BT_RESET&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IMX_GPIO_NR(1, 2)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;#define SABRESD_USR_DEF_RED_LED&amp;nbsp;&amp;nbsp;&amp;nbsp; IMX_GPIO_NR(1, 2)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static void mx6q_sd_bt_reset(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; printk(KERN_INFO "mx6q_sd_bt_reset");&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;SPAN style="color: #ff0000;"&gt; gpio_request(SABRESD_BT_RESET, "bt-reset");&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; gpio_direction_output(SABRESD_BT_RESET, 0);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* pull down reset pin at least &amp;gt;5ms */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; mdelay(6);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* pull up after power supply BT */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; gpio_direction_output(SABRESD_BT_RESET, 1);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; gpio_free(SABRESD_BT_RESET);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; msleep(100);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 May 2014 01:02:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299490#M37548</guid>
      <dc:creator>rickchu</dc:creator>
      <dc:date>2014-05-19T01:02:31Z</dc:date>
    </item>
    <item>
      <title>Re: How could I configure a GPIO as an input?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299491#M37549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;thanks for your response.&lt;/P&gt;&lt;P&gt;It was my fault. Of course there is no gpio_request(TEST_PIN).&lt;/P&gt;&lt;P&gt;Actually I can't find&amp;nbsp; gpio_direction_output(SABRESD_USR_DEF_RED_LED).&lt;/P&gt;&lt;P&gt;Perhaps the initialization takes place in a different file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Jan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 May 2014 08:55:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-could-I-configure-a-GPIO-as-an-input/m-p/299491#M37549</guid>
      <dc:creator>janr_</dc:creator>
      <dc:date>2014-05-23T08:55:56Z</dc:date>
    </item>
  </channel>
</rss>