<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6S CLKO1 does not output 32kHz. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6S-CLKO1-does-not-output-32kHz/m-p/299085#M37471</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just tried it on i.MX6DL sabresd board, and CLKO1 can output 32KHz clock. Below is the config&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;r159 on i.MX6DL SabreSD board, pin GPIO_0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x20e020c set to 0 to select it as CLKO1;&lt;/P&gt;&lt;P&gt;0x20e05dc set to 0x1b0b0;&lt;/P&gt;&lt;P&gt;0x20c4060 set to 0x8e to select ckil sync clock output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then there will be 32KHz clock output on r159.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried GPIO_5 pin, set 0x20e0230 to 3, we can see 32KHz clock on r66 of i.MX6DL SabreSD board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Mar 2014 03:14:48 GMT</pubDate>
    <dc:creator>AnsonHuang</dc:creator>
    <dc:date>2014-03-27T03:14:48Z</dc:date>
    <item>
      <title>i.MX6S CLKO1 does not output 32kHz.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6S-CLKO1-does-not-output-32kHz/m-p/299081#M37467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about i.MX6S CLKO.&lt;/P&gt;&lt;P&gt;I tried output 32kHz from CCM_CLKO1 with the following settings.&lt;/P&gt;&lt;P&gt;However, it does not output even though external 32kHz crystal oscillates certainly.&lt;/P&gt;&lt;P&gt;=====&lt;/P&gt;&lt;P&gt;IOMUXC_SW_MUX_CTL_PAD_GPIO05 = 3; (Select CCM_CLKO1, SION=0)&lt;/P&gt;&lt;P&gt;IOMUXC_SW_PAD_CTL_PAD_GPIO05 = 0x0001B0B0;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CCM Clock Output Source Register (CCM_CCOSR)&lt;/P&gt;&lt;P&gt;8 CLK_OUT_SEL ： 0 CCM_CLKO1 output drives CCM_CLKO1 clock&lt;/P&gt;&lt;P&gt;7 CLKO1_EN ： 1 CCM_CLKO1 enabled.&lt;/P&gt;&lt;P&gt;6-4 CLKO1_DIV ： 000 divide by 1(default)&lt;/P&gt;&lt;P&gt;3-0 CLKO1_SEL ： 1110 ckil_sync_clk_root&lt;/P&gt;&lt;P&gt;=====&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Q]&lt;/P&gt;&lt;P&gt;Is any additional setting needed to output 32kHz from CCM_CLKO1?&lt;/P&gt;&lt;P&gt;If no additional setting is needed, could you let me know what is considered as a possibility of a root cause?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your information, 24MHz is output from CCM_CLKO2 with similar setting as above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Mar 2014 06:30:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6S-CLKO1-does-not-output-32kHz/m-p/299081#M37467</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-03-19T06:30:05Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6S CLKO1 does not output 32kHz.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6S-CLKO1-does-not-output-32kHz/m-p/299082#M37468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anyone reply me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Mar 2014 04:19:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6S-CLKO1-does-not-output-32kHz/m-p/299082#M37468</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-03-26T04:19:27Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6S CLKO1 does not output 32kHz.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6S-CLKO1-does-not-output-32kHz/m-p/299083#M37469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is CLKO 32 KHz output just a DC level or some waveforms (which look as some kind of noise) may be observed ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Mar 2014 06:17:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6S-CLKO1-does-not-output-32kHz/m-p/299083#M37469</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-03-26T06:17:15Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6S CLKO1 does not output 32kHz.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6S-CLKO1-does-not-output-32kHz/m-p/299084#M37470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm checking it to measurement member.&lt;/P&gt;&lt;P&gt;Just a moment please?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Mar 2014 09:42:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6S-CLKO1-does-not-output-32kHz/m-p/299084#M37470</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-03-26T09:42:10Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6S CLKO1 does not output 32kHz.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6S-CLKO1-does-not-output-32kHz/m-p/299085#M37471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just tried it on i.MX6DL sabresd board, and CLKO1 can output 32KHz clock. Below is the config&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;r159 on i.MX6DL SabreSD board, pin GPIO_0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x20e020c set to 0 to select it as CLKO1;&lt;/P&gt;&lt;P&gt;0x20e05dc set to 0x1b0b0;&lt;/P&gt;&lt;P&gt;0x20c4060 set to 0x8e to select ckil sync clock output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then there will be 32KHz clock output on r159.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried GPIO_5 pin, set 0x20e0230 to 3, we can see 32KHz clock on r66 of i.MX6DL SabreSD board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Mar 2014 03:14:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6S-CLKO1-does-not-output-32kHz/m-p/299085#M37471</guid>
      <dc:creator>AnsonHuang</dc:creator>
      <dc:date>2014-03-27T03:14:48Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6S CLKO1 does not output 32kHz.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6S-CLKO1-does-not-output-32kHz/m-p/299086#M37472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri, Yongcai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your cooperation.&lt;/P&gt;&lt;P&gt;I got a report from measurement member about root cause.&lt;/P&gt;&lt;P&gt;It was a board pattern issue, the pattern was cut by high temperature.&lt;/P&gt;&lt;P&gt;So now, 32kHz is output correctly from CLKO1 on other board that has no pattern issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I appreciate your great support!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Mar 2014 04:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6S-CLKO1-does-not-output-32kHz/m-p/299086#M37472</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2014-03-27T04:26:35Z</dc:date>
    </item>
  </channel>
</rss>