<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 multiple video streams in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-multiple-video-streams/m-p/299050#M37449</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to playback multiple video streams on imx6 to multiple independent displays.&lt;/P&gt;&lt;P&gt;What are the technical limitations on imx6 in terms of&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;number of concurrent independent video streams&lt;/LI&gt;&lt;LI&gt;resolution per stream&lt;/LI&gt;&lt;LI&gt;frame rate per stream&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when using Windows or Linux OS?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;Claus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Apr 2014 21:14:18 GMT</pubDate>
    <dc:creator>--claus</dc:creator>
    <dc:date>2014-04-17T21:14:18Z</dc:date>
    <item>
      <title>i.MX6 multiple video streams</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-multiple-video-streams/m-p/299050#M37449</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to playback multiple video streams on imx6 to multiple independent displays.&lt;/P&gt;&lt;P&gt;What are the technical limitations on imx6 in terms of&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;number of concurrent independent video streams&lt;/LI&gt;&lt;LI&gt;resolution per stream&lt;/LI&gt;&lt;LI&gt;frame rate per stream&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when using Windows or Linux OS?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;Claus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Apr 2014 21:14:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-multiple-video-streams/m-p/299050#M37449</guid>
      <dc:creator>--claus</dc:creator>
      <dc:date>2014-04-17T21:14:18Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 multiple video streams</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-multiple-video-streams/m-p/299051#M37450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I.MX6Q can support 4 independent displays. i.MX6S can support 2 independent displays.&lt;/P&gt;&lt;P&gt;Support two 1080p@24fps independent video. &lt;/P&gt;&lt;P&gt;using Linux for the test.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Apr 2014 14:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-multiple-video-streams/m-p/299051#M37450</guid>
      <dc:creator>justin_jiang</dc:creator>
      <dc:date>2014-04-18T14:20:19Z</dc:date>
    </item>
  </channel>
</rss>