<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: SMFC 0 frame lost error interrupt</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SMFC-0-frame-lost-error-interrupt/m-p/299045#M37444</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Perhaps we have a performance issue in the case ; please use Table 38-35 (Error &lt;/P&gt;&lt;P&gt;Interrupts Summary) of the i.MX6 S Reference Manual to define what registers can be &lt;/P&gt;&lt;P&gt;checked. &lt;/P&gt;&lt;P&gt;&amp;nbsp; According to section 38.4.12.3 (Interrupt Generator) of the Reference Manual :&lt;/P&gt;&lt;P&gt;“The table below describes the error interrupts. The panic column indicates if &lt;/P&gt;&lt;P&gt;this signal is part of the logic generating the ipu_panic signal. The ipu_panic &lt;/P&gt;&lt;P&gt;signal can be used for indicating about errors that are result of data rate &lt;/P&gt;&lt;P&gt;problems. Such problems may be a result of the IPU running in slower clock then &lt;/P&gt;&lt;P&gt;required by the use case. This signal can be used in order to indicate the &lt;/P&gt;&lt;P&gt;system that the IPU can't handle the desired data rate. In that case the system &lt;/P&gt;&lt;P&gt;may need to increase the clock to the IPU or simplify the use case.” &lt;/P&gt;&lt;P&gt;&amp;nbsp; If the panic signals are asserted for the case, please try to decrease screen &lt;/P&gt;&lt;P&gt;resolution and / or frame rate. Also, other system resource consuming processes, &lt;/P&gt;&lt;P&gt;such as USB / SD / SATA transfer, may affect. As result a general performance &lt;/P&gt;&lt;P&gt;issue may take place in the case. Perhaps it makes sense to try system prioritization &lt;/P&gt;&lt;P&gt;(such as provided by Linux nice command).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Mar 2014 03:20:23 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2014-03-21T03:20:23Z</dc:date>
    <item>
      <title>SMFC 0 frame lost error interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SMFC-0-frame-lost-error-interrupt/m-p/299044#M37443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working on i.MX6 S platform.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are getting SMFC0 Frame lost error interrupt while doing the below operation&lt;/P&gt;&lt;P&gt;Camera --&amp;gt;&amp;nbsp; CSI--&amp;gt; SMFC --&amp;gt; IDMAC CH0 --&amp;gt; Memory.&lt;/P&gt;&lt;P&gt;Could anyone provide the information about cause of the problem? Is there any document related SMFC FIFO?&lt;/P&gt;&lt;P&gt;How to fix the issue? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;SuryaG&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Mar 2014 06:13:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SMFC-0-frame-lost-error-interrupt/m-p/299044#M37443</guid>
      <dc:creator>suryag</dc:creator>
      <dc:date>2014-03-19T06:13:14Z</dc:date>
    </item>
    <item>
      <title>Re: SMFC 0 frame lost error interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SMFC-0-frame-lost-error-interrupt/m-p/299045#M37444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Perhaps we have a performance issue in the case ; please use Table 38-35 (Error &lt;/P&gt;&lt;P&gt;Interrupts Summary) of the i.MX6 S Reference Manual to define what registers can be &lt;/P&gt;&lt;P&gt;checked. &lt;/P&gt;&lt;P&gt;&amp;nbsp; According to section 38.4.12.3 (Interrupt Generator) of the Reference Manual :&lt;/P&gt;&lt;P&gt;“The table below describes the error interrupts. The panic column indicates if &lt;/P&gt;&lt;P&gt;this signal is part of the logic generating the ipu_panic signal. The ipu_panic &lt;/P&gt;&lt;P&gt;signal can be used for indicating about errors that are result of data rate &lt;/P&gt;&lt;P&gt;problems. Such problems may be a result of the IPU running in slower clock then &lt;/P&gt;&lt;P&gt;required by the use case. This signal can be used in order to indicate the &lt;/P&gt;&lt;P&gt;system that the IPU can't handle the desired data rate. In that case the system &lt;/P&gt;&lt;P&gt;may need to increase the clock to the IPU or simplify the use case.” &lt;/P&gt;&lt;P&gt;&amp;nbsp; If the panic signals are asserted for the case, please try to decrease screen &lt;/P&gt;&lt;P&gt;resolution and / or frame rate. Also, other system resource consuming processes, &lt;/P&gt;&lt;P&gt;such as USB / SD / SATA transfer, may affect. As result a general performance &lt;/P&gt;&lt;P&gt;issue may take place in the case. Perhaps it makes sense to try system prioritization &lt;/P&gt;&lt;P&gt;(such as provided by Linux nice command).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2014 03:20:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SMFC-0-frame-lost-error-interrupt/m-p/299045#M37444</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-03-21T03:20:23Z</dc:date>
    </item>
    <item>
      <title>Re: SMFC 0 frame lost error interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SMFC-0-frame-lost-error-interrupt/m-p/299046#M37445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Tahoma;"&gt;Hi Yuri,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Tahoma;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Tahoma;"&gt;Thanks for your response.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Tahoma;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Tahoma;"&gt;Currently we are working on LCD and Camera interfaces only. We are not using any other peripherals like USB/SD/SATA.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Tahoma; font-size: 10pt; line-height: 1.5em;"&gt;Please find the below environment settings:&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #000000; font-family: Tahoma;"&gt;&lt;BR /&gt;&lt;STRONG style="text-decoration: underline;"&gt;Default:&lt;/STRONG&gt;&lt;BR /&gt;Camera clock (Ipu csi clk) : 75 MHz &lt;BR /&gt;Camera VSYNC( IPU_CSI_VSYNC) : 30 fps&lt;BR /&gt;HSP CLK : 254 MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Camera will support different resolution (frame size) and different FPS.&lt;BR /&gt;When we change the frame height value only SMFC frame lose interrupt is generating.&lt;/STRONG&gt;&lt;/P&gt;&lt;DIV&gt;&lt;BR /&gt;Scenario 1:&lt;BR /&gt;Camera capture frame size: 1280x720 @30 FPS means 30 vsync per second&lt;BR /&gt;IDMAC CH0 frame size: 1280x720, IDMAC CH0 EOF interrupt is generating 30 times and there is no SMFC0 frame lost interrupt.&lt;P&gt;&lt;/P&gt;Scenario 2::&lt;BR /&gt;Camera capture frame size: 1280x360 @30 FPS means 30 vsync per second&lt;BR /&gt;IDMAC CH0 frame size: 1280x360, IDMAC CH0 EOF interrupt is generating only 15 times and SMFC0 frame lost interrupt is generating 15 times&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Tahoma;"&gt;Camera clock (Ipu csi clk) : 75 MHz &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Tahoma;"&gt;Camera VSYNC( IPU_CSI_VSYNC) : 30 fps&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Tahoma;"&gt;HSP CLK : 254 MHz&lt;/SPAN&gt;&lt;/P&gt;Scenario 3:&lt;BR /&gt;Camera capture frame size: 1280x720 @15 FPS means 15 vsync per second&lt;BR /&gt;IDMAC CH0 frame size: 1280x720, IDMAC CH0 EOF interrupt is generating 15 times and there is no SMFC0 frame lost interrupt.&lt;P&gt;&lt;/P&gt;Scenario 4::&lt;BR /&gt;Camera capture frame size: 1280x360 @15 FPS means 15 vsync per second&lt;BR /&gt;IDMAC CH0 frame size: 1280x360, IDMAC CH0 EOF interrupt is generating only 7.5 times and SMFC0 frame lost interrupt is generating 7.5 times&lt;DIV&gt;&lt;P&gt;&lt;/P&gt;Could you please analyse the above scenario's and provide root cause of the problem?&lt;BR /&gt;Where can i get the SMFC DMA channels information?&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2014 04:18:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SMFC-0-frame-lost-error-interrupt/m-p/299046#M37445</guid>
      <dc:creator>suryag</dc:creator>
      <dc:date>2014-03-21T04:18:45Z</dc:date>
    </item>
    <item>
      <title>Re: SMFC 0 frame lost error interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SMFC-0-frame-lost-error-interrupt/m-p/299047#M37446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The above mentioned issue got solved.&lt;/P&gt;&lt;P&gt;Earlier, we are not updating the &lt;STRONG style="color: #000000; font-family: Tahoma;"&gt;IPU_CSI0_SENS_FRM_SIZE&lt;/STRONG&gt; register value with respect to capture frame size. We fixed the sensor frame size to 1280x720.&lt;/P&gt;&lt;P&gt;When we updating the &lt;STRONG style="color: #000000; font-family: Tahoma;"&gt;IPU_CSI0_SENS_FRM_SIZE&lt;/STRONG&gt; values, IDMAC CH0 EOF interrupt is generating perfectly what we expect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;SuryaG&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Mar 2014 05:54:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SMFC-0-frame-lost-error-interrupt/m-p/299047#M37446</guid>
      <dc:creator>suryag</dc:creator>
      <dc:date>2014-03-26T05:54:28Z</dc:date>
    </item>
    <item>
      <title>Re: SMFC 0 frame lost error interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SMFC-0-frame-lost-error-interrupt/m-p/299048#M37447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am using same &lt;STRONG style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Camera --&amp;gt;&amp;nbsp; CSI--&amp;gt; SMFC --&amp;gt; IDMAC CH0 --&amp;gt; Memory &lt;/STRONG&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt; method, But i didn't get EOF interrupt. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;i got this error &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0&lt;/P&gt;&lt;P&gt;VIDIOC_DQBUF failed.&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued&lt;/P&gt;&lt;P&gt;VIDIOC_QBUF failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help me how to fix this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2016 11:01:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SMFC-0-frame-lost-error-interrupt/m-p/299048#M37447</guid>
      <dc:creator>aravinthkumarja</dc:creator>
      <dc:date>2016-02-04T11:01:13Z</dc:date>
    </item>
    <item>
      <title>Re: SMFC 0 frame lost error interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SMFC-0-frame-lost-error-interrupt/m-p/299049#M37448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following may be helpful :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;”Unable to capture video on IMX6Q”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="moz-txt-link-rfc2396E" href="https://community.nxp.com/message/607111#607111"&gt;&amp;lt; &lt;/A&gt;&lt;A href="https://community.freescale.com/message/607111#607111" target="test_blank"&gt;https://community.freescale.com/message/607111#607111&lt;/A&gt; &amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;“CSI preview demo not working!”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="moz-txt-link-rfc2396E" href="https://community.nxp.com/message/610124#610124"&gt;&amp;lt; &lt;/A&gt;&lt;A href="https://community.freescale.com/message/610124#610124" target="test_blank"&gt;https://community.freescale.com/message/610124#610124&lt;/A&gt; &amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2016 07:45:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SMFC-0-frame-lost-error-interrupt/m-p/299049#M37448</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-02-05T07:45:54Z</dc:date>
    </item>
  </channel>
</rss>