<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX53 Third USB host</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Third-USB-host/m-p/298438#M37325</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please note that the Lower USB Host jack and the Micro USB Device jack&lt;/P&gt;&lt;P&gt;are cross connected. You can plug one cable into either jack,&lt;/P&gt;&lt;P&gt;but cannot plug cables into both jacks at the same time.&lt;/P&gt;&lt;P&gt;I can suggest to use some external USB hub to attach more USB devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Apr 2014 02:03:02 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2014-04-22T02:03:02Z</dc:date>
    <item>
      <title>i.MX53 Third USB host</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Third-USB-host/m-p/298437#M37324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have custom board based on i.MX53 with MC34708 PMIC.&lt;/P&gt;&lt;P&gt;I know that this board have 3 usb ports, but only two of them are used (one host and one OTG).&lt;/P&gt;&lt;P&gt;How to enable third USB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Apr 2014 05:51:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Third-USB-host/m-p/298437#M37324</guid>
      <dc:creator>ToxicAvenger</dc:creator>
      <dc:date>2014-04-17T05:51:38Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 Third USB host</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Third-USB-host/m-p/298438#M37325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please note that the Lower USB Host jack and the Micro USB Device jack&lt;/P&gt;&lt;P&gt;are cross connected. You can plug one cable into either jack,&lt;/P&gt;&lt;P&gt;but cannot plug cables into both jacks at the same time.&lt;/P&gt;&lt;P&gt;I can suggest to use some external USB hub to attach more USB devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Apr 2014 02:03:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-Third-USB-host/m-p/298438#M37325</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2014-04-22T02:03:02Z</dc:date>
    </item>
  </channel>
</rss>