<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Single Channel LVDS Display with 1920x1080@60Hz in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298180#M37253</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Stephan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you really undersatand our RM document deeply.&lt;/P&gt;&lt;P&gt;there is indeed two way to meet your requirement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;while I recommend you use two LVDS port to do this.&lt;/P&gt;&lt;P&gt;because I don't think 148.5MHz dotclock is a good thing for us( jitter, PCB layout, EMI.......). &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Mar 2014 01:11:04 GMT</pubDate>
    <dc:creator>alfred_liu</dc:creator>
    <dc:date>2014-03-19T01:11:04Z</dc:date>
    <item>
      <title>Single Channel LVDS Display with 1920x1080@60Hz</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298173#M37246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use a LVDS display with a resolution of 1920x1080 Pixel @60Hz (Dotclock = 148.5 MHz). The display has only a single LVDS Channel with 4 differntial data lines.&lt;/P&gt;&lt;P&gt;I think the limitation is the serializer clock of the LDB which must not be higher than 595 MHz. When I calculate the clock for my display (148.5 MHz Dotclock * 7 Databit = &lt;STRONG&gt;1039.5 MHz&lt;/STRONG&gt; Serializer Clock) this will not work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Is this up to this point correct?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The solution now is to use the SPLIT mode. But then I have to use both LVDS channels of the i.MX6. One for the ODD data and one for the EVEN data. I have then a SerialzerClock of 519.75MHz, which is lower than the 595 MHz. But than I need an other display that supports the two LVDS channels.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Is this up to this point correct?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The last question is now: Where can I find the information which LVDS channel is responsible for the ODD data and which one for the EVEN data?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Stephan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Mar 2014 08:29:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298173#M37246</guid>
      <dc:creator>schulerstephan</dc:creator>
      <dc:date>2014-03-18T08:29:42Z</dc:date>
    </item>
    <item>
      <title>Re: Single Channel LVDS Display with 1920x1080@60Hz</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298174#M37247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Stephan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1, yes, your caculation is exactly correct, signle LVDS cannot reach 1920*1080/60Hz, we need two LVDS port to support this.&lt;/P&gt;&lt;P&gt;2, I believe the ODD data and EVEN data are configured in our i.mx side, you can refer to our BSP reference code to get it. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Mar 2014 08:45:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298174#M37247</guid>
      <dc:creator>alfred_liu</dc:creator>
      <dc:date>2014-03-18T08:45:46Z</dc:date>
    </item>
    <item>
      <title>Re: Single Channel LVDS Display with 1920x1080@60Hz</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298175#M37248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Stephan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please pay attention on page 482 of the reference manual (dual-quad): max. frequency for single channel is 85mhz, so it is not possible to achieve 1920x1080@60.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manuel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Mar 2014 08:49:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298175#M37248</guid>
      <dc:creator>EgleTeam</dc:creator>
      <dc:date>2014-03-18T08:49:33Z</dc:date>
    </item>
    <item>
      <title>Re: Single Channel LVDS Display with 1920x1080@60Hz</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298176#M37249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi,Stephan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the attached LCD is a dual LVDS panel, Maybe you can refer to. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Mar 2014 08:50:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298176#M37249</guid>
      <dc:creator>alfred_liu</dc:creator>
      <dc:date>2014-03-18T08:50:46Z</dc:date>
    </item>
    <item>
      <title>Re: Single Channel LVDS Display with 1920x1080@60Hz</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298177#M37250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manuel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks! The 85MHz Pixelclock are exactly the maximum serializer clock (85MHz * 7 Bit = 595 MHz). That will confirm my calculation! :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Stephan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Mar 2014 09:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298177#M37250</guid>
      <dc:creator>schulerstephan</dc:creator>
      <dc:date>2014-03-18T09:34:01Z</dc:date>
    </item>
    <item>
      <title>Re: Single Channel LVDS Display with 1920x1080@60Hz</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298178#M37251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weisong Liu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for you answer!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have to check the configuration for odd an even with my colleagues. Maybe I will come back later to this point.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To solve the hardware point I think there are two possible solutions:&lt;/P&gt;&lt;P&gt;1. We have to change the display to a dual channel LVDS type&lt;/P&gt;&lt;P&gt;2. We will use the parallel RGB interface which supports a pixelclock up to 264 MHz (single port) and then we have to use a external LVDS seralizer that support a higher bitrate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any other thinks to regard relating to the parallel RGB interface with a FullHD resolution? For lower resolutions this works fine for us!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Stephan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Mar 2014 09:41:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298178#M37251</guid>
      <dc:creator>schulerstephan</dc:creator>
      <dc:date>2014-03-18T09:41:50Z</dc:date>
    </item>
    <item>
      <title>Re: Single Channel LVDS Display with 1920x1080@60Hz</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298179#M37252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Stephan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In our modules we only did the fanout of one channel. Sounds interesting to use a LVDS serializer from RGB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Manuel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Mar 2014 12:45:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298179#M37252</guid>
      <dc:creator>EgleTeam</dc:creator>
      <dc:date>2014-03-18T12:45:06Z</dc:date>
    </item>
    <item>
      <title>Re: Single Channel LVDS Display with 1920x1080@60Hz</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298180#M37253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Stephan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you really undersatand our RM document deeply.&lt;/P&gt;&lt;P&gt;there is indeed two way to meet your requirement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;while I recommend you use two LVDS port to do this.&lt;/P&gt;&lt;P&gt;because I don't think 148.5MHz dotclock is a good thing for us( jitter, PCB layout, EMI.......). &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Mar 2014 01:11:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298180#M37253</guid>
      <dc:creator>alfred_liu</dc:creator>
      <dc:date>2014-03-19T01:11:04Z</dc:date>
    </item>
    <item>
      <title>Re: Single Channel LVDS Display with 1920x1080@60Hz</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298181#M37254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weisong Liu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am completely with you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Furthermore I couldn't find a RGB to LVDS bridge which supports the 148 MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many Thanks for your help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Stephan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Mar 2014 07:05:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298181#M37254</guid>
      <dc:creator>schulerstephan</dc:creator>
      <dc:date>2014-03-19T07:05:21Z</dc:date>
    </item>
    <item>
      <title>Re: Single Channel LVDS Display with 1920x1080@60Hz</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298182#M37255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;TI has few transmitters for &amp;gt;150Mhz. Unfortunately those work at 1.8V: almost sure due the arguments that said Weisong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Manuel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Mar 2014 13:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298182#M37255</guid>
      <dc:creator>EgleTeam</dc:creator>
      <dc:date>2014-03-19T13:38:15Z</dc:date>
    </item>
    <item>
      <title>Re: Single Channel LVDS Display with 1920x1080@60Hz</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298183#M37256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo Stephan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had similar problemes with the same display (I guess).&lt;/P&gt;&lt;P&gt;I build an android with the sabrelite BSP and changed my parameters &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; described in:&amp;nbsp; &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-93617"&gt;https://community.freescale.com/docs/DOC-93617&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After I set a frequency lower than 148.5 M pixel / s, I got a running system with a flickering screen. ( pixclock approx. 9000 )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Later I changed an entry kernel_imx/arch/arck/mach-mx6/ckolck.c in function int __init mx6_clocks_init(. . .)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; clk_set_parent(&amp;amp;ldb_di0_clk, &amp;amp;pll2_pfd_352M);&lt;/P&gt;&lt;P&gt;to:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; clk_set_parent(&amp;amp;ldb_di0_clk, &amp;amp;pll5_video_main_clk);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To exclude a conflict while initialising I switched off some entrys in init.rc: &lt;/P&gt;&lt;P&gt;I found, that android boots without the console:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#service console /system/bin/sh&lt;/P&gt;&lt;P&gt;#&amp;nbsp;&amp;nbsp;&amp;nbsp; class core&lt;/P&gt;&lt;P&gt;#&amp;nbsp;&amp;nbsp;&amp;nbsp; console&lt;/P&gt;&lt;P&gt;#&amp;nbsp;&amp;nbsp;&amp;nbsp; user root&lt;/P&gt;&lt;P&gt;#&amp;nbsp;&amp;nbsp;&amp;nbsp; group root&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The system didn't flicker any more, but it became so instable, that a mouse movement turned the screen to black for a second.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am new in building android, so I don't know if that means, you can reach higher values, than described in the imx6q-specs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I think you're right, and the 595 MHz is the maximum for single channel lvds.&amp;nbsp; I was irritated&amp;nbsp; by some other entries in the datasheets of imx and/or sabrelite.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Mar 2014 13:15:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Single-Channel-LVDS-Display-with-1920x1080-60Hz/m-p/298183#M37256</guid>
      <dc:creator>sebastiannowack</dc:creator>
      <dc:date>2014-03-27T13:15:06Z</dc:date>
    </item>
  </channel>
</rss>