<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックPlug-ins: Direct mode examples</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Plug-ins-Direct-mode-examples/m-p/162697#M3718</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've modified the demo code to display alternating black and white frames at a 10 Hz rate and am not all that happy with the results.&amp;nbsp; The demo is running in Buffered mode which appears to be the easiest to use.&amp;nbsp; I would like to be able to display runtime gen'd arrays of icon sized array data (32x32x16bpp) in an area about 400x300.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q1)&amp;nbsp; Does anyone have an example of using direct mode?&lt;/P&gt;&lt;P&gt;Q2)&amp;nbsp; Has anyone tried using OpenGL ES 2.0 directly?&amp;nbsp; I would like to setup a simple double buffered arrangement but not experienced using OpenGL.&amp;nbsp; I did this using WinCE 6.0 R3, Silverlight for Embedded, and DirectDraw with excellent results but not sure how to do this with OpenGL 2.0 ES.&lt;/P&gt;&lt;P&gt;Q3) Does OpenGL ES 2.0 have the capability to upscale a low res image (32x32) into a higher res image (400x300) and do it using an interpolating algorithm on the GPU?&amp;nbsp; If so, does anyone have sample code I could look at?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My current task is to evaluate Inflexion UI on Linux with the primary functionality being to display runtime gen'd bitmaps of 32x32 at a 10 Hz rate onto a field about 400x300.&amp;nbsp; I'm&amp;nbsp;developing this evaluation on an&amp;nbsp;i.MX53 QSB.&amp;nbsp; I've taken the approach of using Inflexion plug-ins.&amp;nbsp; For expediency, I've chosen to simply modify the code-behind file of the&amp;nbsp;plug-in module in the demo code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help is greatly appreciated.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jul 2011 20:58:31 GMT</pubDate>
    <dc:creator>TxPomeroy</dc:creator>
    <dc:date>2011-07-19T20:58:31Z</dc:date>
    <item>
      <title>Plug-ins: Direct mode examples</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Plug-ins-Direct-mode-examples/m-p/162697#M3718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've modified the demo code to display alternating black and white frames at a 10 Hz rate and am not all that happy with the results.&amp;nbsp; The demo is running in Buffered mode which appears to be the easiest to use.&amp;nbsp; I would like to be able to display runtime gen'd arrays of icon sized array data (32x32x16bpp) in an area about 400x300.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Q1)&amp;nbsp; Does anyone have an example of using direct mode?&lt;/P&gt;&lt;P&gt;Q2)&amp;nbsp; Has anyone tried using OpenGL ES 2.0 directly?&amp;nbsp; I would like to setup a simple double buffered arrangement but not experienced using OpenGL.&amp;nbsp; I did this using WinCE 6.0 R3, Silverlight for Embedded, and DirectDraw with excellent results but not sure how to do this with OpenGL 2.0 ES.&lt;/P&gt;&lt;P&gt;Q3) Does OpenGL ES 2.0 have the capability to upscale a low res image (32x32) into a higher res image (400x300) and do it using an interpolating algorithm on the GPU?&amp;nbsp; If so, does anyone have sample code I could look at?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My current task is to evaluate Inflexion UI on Linux with the primary functionality being to display runtime gen'd bitmaps of 32x32 at a 10 Hz rate onto a field about 400x300.&amp;nbsp; I'm&amp;nbsp;developing this evaluation on an&amp;nbsp;i.MX53 QSB.&amp;nbsp; I've taken the approach of using Inflexion plug-ins.&amp;nbsp; For expediency, I've chosen to simply modify the code-behind file of the&amp;nbsp;plug-in module in the demo code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help is greatly appreciated.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2011 20:58:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Plug-ins-Direct-mode-examples/m-p/162697#M3718</guid>
      <dc:creator>TxPomeroy</dc:creator>
      <dc:date>2011-07-19T20:58:31Z</dc:date>
    </item>
  </channel>
</rss>