<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIBIS Model IMX6 Series</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IBIS-Model-IMX6-Series/m-p/297485#M37085</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using MCIMX6Q6AVT10AC processor in one of our project. The layout has been done and we want to do the SIgnal integrity analysis for high speed signal but the IBIS model for this series does not support PCIe, HDMI and SATA . How can i do that i have written to technical support but they have not replied any satisfactory answer. Kindly help me , if any one is having the Modelled IBIS file kindly provide me .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sandeep&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Apr 2014 06:45:26 GMT</pubDate>
    <dc:creator>sandeepkumar</dc:creator>
    <dc:date>2014-04-16T06:45:26Z</dc:date>
    <item>
      <title>IBIS Model IMX6 Series</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IBIS-Model-IMX6-Series/m-p/297485#M37085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using MCIMX6Q6AVT10AC processor in one of our project. The layout has been done and we want to do the SIgnal integrity analysis for high speed signal but the IBIS model for this series does not support PCIe, HDMI and SATA . How can i do that i have written to technical support but they have not replied any satisfactory answer. Kindly help me , if any one is having the Modelled IBIS file kindly provide me .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sandeep&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Apr 2014 06:45:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IBIS-Model-IMX6-Series/m-p/297485#M37085</guid>
      <dc:creator>sandeepkumar</dc:creator>
      <dc:date>2014-04-16T06:45:26Z</dc:date>
    </item>
    <item>
      <title>Re: IBIS Model IMX6 Series</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IBIS-Model-IMX6-Series/m-p/297486#M37086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi sundeep, currently thete models are not available.&lt;/P&gt;&lt;P&gt;You can use guidelines given in Hardware Development Guide.&lt;/P&gt;&lt;P&gt;Usually signal problems with these interfaces are related &lt;/P&gt;&lt;P&gt;more directly to the dielectric being used, which may be good but &lt;/P&gt;&lt;P&gt;not a high frequency dielectric. That could explain the signal &lt;/P&gt;&lt;P&gt;degradation one is experiencing as dielectrics such as FR4 might &lt;/P&gt;&lt;P&gt;not suffice when handling SATA or PCIe. The characteristic impedance can &lt;/P&gt;&lt;P&gt;be way off at the high frequency if the material is not rated to &lt;/P&gt;&lt;P&gt;go that fast.&lt;/P&gt;&lt;P&gt;A higher grade of board dielectric material typically needs to be specified &lt;/P&gt;&lt;P&gt;in order to guarantee that the characteristic impedance of the high speed &lt;/P&gt;&lt;P&gt;lines is what it should be at the operational frequency and edge rates &lt;/P&gt;&lt;P&gt;of the fastest signals on the board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Apr 2014 10:20:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IBIS-Model-IMX6-Series/m-p/297486#M37086</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-04-18T10:20:01Z</dc:date>
    </item>
  </channel>
</rss>