<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 setplayspeed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/setplayspeed/m-p/297333#M37056</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found android API in the Android_codec_release_note as below . The "setPlaySpeed" is only for audio track ? Or it can make the video frame rewind/forward ?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;6 Extend Android Multimedia Framework APIs&lt;BR /&gt;In Jelly Bean, Freescale has extended only one Android API, set playback speed.&lt;BR /&gt;/* trick mode */&lt;BR /&gt;/**&lt;BR /&gt;* Set playback speed.&lt;BR /&gt;*&lt;BR /&gt;* @param Speed[] contains only one item which is normalized speed multiplied by 0x10000&lt;BR /&gt;* Range of normalized speed is:&lt;BR /&gt;* [-16,-2] means rewind, [0.1, 16] means fast forward, step is 0.1&lt;BR /&gt;* when normalized speed is [0.1, 1.9] audio is outputted, otherwise audio&lt;BR /&gt;* is not outputted.&lt;BR /&gt;* After this function call returns, result speed is stored in Speed[0], to show whether&lt;BR /&gt;it succeeds or fails.&lt;BR /&gt;*/&lt;BR /&gt;public native void setPlaySpeed(int[] Speed);&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Apr 2014 03:40:48 GMT</pubDate>
    <dc:creator>weikeng-jimmy</dc:creator>
    <dc:date>2014-04-16T03:40:48Z</dc:date>
    <item>
      <title>setplayspeed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/setplayspeed/m-p/297333#M37056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sir,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found android API in the Android_codec_release_note as below . The "setPlaySpeed" is only for audio track ? Or it can make the video frame rewind/forward ?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;6 Extend Android Multimedia Framework APIs&lt;BR /&gt;In Jelly Bean, Freescale has extended only one Android API, set playback speed.&lt;BR /&gt;/* trick mode */&lt;BR /&gt;/**&lt;BR /&gt;* Set playback speed.&lt;BR /&gt;*&lt;BR /&gt;* @param Speed[] contains only one item which is normalized speed multiplied by 0x10000&lt;BR /&gt;* Range of normalized speed is:&lt;BR /&gt;* [-16,-2] means rewind, [0.1, 16] means fast forward, step is 0.1&lt;BR /&gt;* when normalized speed is [0.1, 1.9] audio is outputted, otherwise audio&lt;BR /&gt;* is not outputted.&lt;BR /&gt;* After this function call returns, result speed is stored in Speed[0], to show whether&lt;BR /&gt;it succeeds or fails.&lt;BR /&gt;*/&lt;BR /&gt;public native void setPlaySpeed(int[] Speed);&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Apr 2014 03:40:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/setplayspeed/m-p/297333#M37056</guid>
      <dc:creator>weikeng-jimmy</dc:creator>
      <dc:date>2014-04-16T03:40:48Z</dc:date>
    </item>
    <item>
      <title>Re: setplayspeed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/setplayspeed/m-p/297334#M37057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've updated in your SR, if any update, pls let me know it, if no, pls close this thread.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Apr 2014 07:58:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/setplayspeed/m-p/297334#M37057</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2014-04-17T07:58:59Z</dc:date>
    </item>
  </channel>
</rss>