<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6SLEVK debug uart problems</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SLEVK-debug-uart-problems/m-p/297060#M36979</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, seems the problem was in flow control.&lt;/P&gt;&lt;P&gt;It is very strange....cu doesn't have flow control options and i use it whithout such problems with other devices.&lt;/P&gt;&lt;P&gt;In fact i tried minicom and it worked better.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Mar 2014 04:22:19 GMT</pubDate>
    <dc:creator>egorrumjantsev</dc:creator>
    <dc:date>2014-03-17T04:22:19Z</dc:date>
    <item>
      <title>IMX6SLEVK debug uart problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SLEVK-debug-uart-problems/m-p/297058#M36977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I received IMX6SLEVK and try to bring up u-boot working for it. I compiled U-Boot from Denx site for this board.&lt;/P&gt;&lt;P&gt;I see that U-Boot send debug output to debug UART, via serial console on my Linux PC but i can't sent anything back. TX line doesn't work....even i tri to see with oscilloscope - no data from FT232RQ TX pin.&lt;/P&gt;&lt;P&gt;Maybe the problem in ftdi_sio driver in mt PC? I'm using kernel 2.6.39, so i took driver from 3.4 branch and put it in my current kernel. The reason the same - no TX data.&lt;/P&gt;&lt;P&gt;I checked Android's images from cards that shipped with board, but had same situation.&lt;/P&gt;&lt;P&gt;Why that can happen?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WBR,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Mar 2014 06:25:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6SLEVK-debug-uart-problems/m-p/297058#M36977</guid>
      <dc:creator>egorrumjantsev</dc:creator>
      <dc:date>2014-03-16T06:25:02Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6SLEVK debug uart problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SLEVK-debug-uart-problems/m-p/297059#M36978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Double check your terminal settings, such as no flow control.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Mar 2014 14:22:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6SLEVK-debug-uart-problems/m-p/297059#M36978</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2014-03-16T14:22:30Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6SLEVK debug uart problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SLEVK-debug-uart-problems/m-p/297060#M36979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, seems the problem was in flow control.&lt;/P&gt;&lt;P&gt;It is very strange....cu doesn't have flow control options and i use it whithout such problems with other devices.&lt;/P&gt;&lt;P&gt;In fact i tried minicom and it worked better.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Mar 2014 04:22:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6SLEVK-debug-uart-problems/m-p/297060#M36979</guid>
      <dc:creator>egorrumjantsev</dc:creator>
      <dc:date>2014-03-17T04:22:19Z</dc:date>
    </item>
  </channel>
</rss>