<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Boot Contact Pins in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Contact-Pins/m-p/162460#M3679</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Folks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anybody give me any advice on the best way to set up the boot contact pins on the IMX257?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wish to know if they all MUST be connected or can I connect the ones corresponding to NAND Flash (which I am using) to high, whilst leaving the non-required pins as no-connect. &amp;nbsp;I know this is classed as floating and may not be a good idea.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Else, I must use pull down resistors, but I worry that this may affect the use of the peripherals associated with these pins, such as CSPI2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any advice would be most gratefully received&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ddB&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Jul 2011 07:47:54 GMT</pubDate>
    <dc:creator>DaviddeBethel</dc:creator>
    <dc:date>2011-07-15T07:47:54Z</dc:date>
    <item>
      <title>Boot Contact Pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Contact-Pins/m-p/162460#M3679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Folks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anybody give me any advice on the best way to set up the boot contact pins on the IMX257?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wish to know if they all MUST be connected or can I connect the ones corresponding to NAND Flash (which I am using) to high, whilst leaving the non-required pins as no-connect. &amp;nbsp;I know this is classed as floating and may not be a good idea.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Else, I must use pull down resistors, but I worry that this may affect the use of the peripherals associated with these pins, such as CSPI2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any advice would be most gratefully received&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ddB&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2011 07:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Contact-Pins/m-p/162460#M3679</guid>
      <dc:creator>DaviddeBethel</dc:creator>
      <dc:date>2011-07-15T07:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: Boot Contact Pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Contact-Pins/m-p/162461#M3680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Instead of using the external IO you can use the e-fuses to determine how the SoC boots.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Renato Frias&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2011 20:10:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Contact-Pins/m-p/162461#M3680</guid>
      <dc:creator>Frias</dc:creator>
      <dc:date>2011-07-15T20:10:27Z</dc:date>
    </item>
    <item>
      <title>Re: Boot Contact Pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Contact-Pins/m-p/162462#M3681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;yes this is interesting, but is there any tool to read/blow fuses status for prototipe and production?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Nov 2011 10:19:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Contact-Pins/m-p/162462#M3681</guid>
      <dc:creator>OmarPighi</dc:creator>
      <dc:date>2011-11-02T10:19:02Z</dc:date>
    </item>
  </channel>
</rss>