<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to Disable Watchdog on SABRE-SD? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Disable-Watchdog-on-SABRE-SD/m-p/295717#M36614</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been trying to use KGDB with the SABRE-SD in order to debug a driver. It seems to be working but once I drop into KGDB the SABRE-SD board resets after about five seconds. I expect this is due to a watchdog timer expiring now that the kernel is not petting the dog. What is the easiest way to disable the watchdog timer or enable KGDB to resest it periodically while the kernel is halted?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Android JB4.3 from Freescale.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Carson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Apr 2014 15:23:58 GMT</pubDate>
    <dc:creator>carsongreen</dc:creator>
    <dc:date>2014-04-14T15:23:58Z</dc:date>
    <item>
      <title>How to Disable Watchdog on SABRE-SD?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Disable-Watchdog-on-SABRE-SD/m-p/295717#M36614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been trying to use KGDB with the SABRE-SD in order to debug a driver. It seems to be working but once I drop into KGDB the SABRE-SD board resets after about five seconds. I expect this is due to a watchdog timer expiring now that the kernel is not petting the dog. What is the easiest way to disable the watchdog timer or enable KGDB to resest it periodically while the kernel is halted?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Android JB4.3 from Freescale.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Carson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Apr 2014 15:23:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-Disable-Watchdog-on-SABRE-SD/m-p/295717#M36614</guid>
      <dc:creator>carsongreen</dc:creator>
      <dc:date>2014-04-14T15:23:58Z</dc:date>
    </item>
    <item>
      <title>Re: How to Disable Watchdog on SABRE-SD?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Disable-Watchdog-on-SABRE-SD/m-p/295718#M36615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carson,&lt;/P&gt;&lt;P&gt;once enabled watchdog can not be disabled. So one needs&lt;/P&gt;&lt;P&gt;to rebuild sources, procedure is described in i.MX_6Dual6Quad_Linux_Reference_Manual.pdf&lt;/P&gt;&lt;P&gt;Chapter 43 Watchdog (WDOG) Driver :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;use the ./ltib -c&lt;/P&gt;&lt;P&gt;command when located in the &amp;lt;ltib dir&amp;gt;. On the screen displayed, select Configure the&lt;/P&gt;&lt;P&gt;Kernel and exit. When the next screen appears, select the following option to enable this&lt;/P&gt;&lt;P&gt;module:&lt;/P&gt;&lt;P&gt;• CONFIG_IMX2_WDT-Enables Watchdog timer module. This option is available&lt;/P&gt;&lt;P&gt;under Device Drivers &amp;gt; Watchdog Timer Support &amp;gt; IMX2+ Watchdog.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;or just comment function imx6q_add_imx2_wdt (board-mx6q_sabresd.c)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Otherwise seems there is no other option as to pet the dog manually. :smileywink:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Apr 2014 11:42:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-Disable-Watchdog-on-SABRE-SD/m-p/295718#M36615</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-04-15T11:42:12Z</dc:date>
    </item>
  </channel>
</rss>