<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Installing QT 5 or above in Ltib L3.0.35_4.1.0 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Installing-QT-5-or-above-in-Ltib-L3-0-35-4-1-0/m-p/295680#M36593</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom iMX6q board running with L3.0.35_4.1.0 kernel. I am using Ltib. I have added qt4.6.0 to it and i am able to run a few applications,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However now I am trying to install QT 5 or above in Ltib L3.0.35_4.1.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone tell me a procedure how to do it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;nishad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Apr 2014 13:31:54 GMT</pubDate>
    <dc:creator>nishad_kamdar</dc:creator>
    <dc:date>2014-04-14T13:31:54Z</dc:date>
    <item>
      <title>Installing QT 5 or above in Ltib L3.0.35_4.1.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-QT-5-or-above-in-Ltib-L3-0-35-4-1-0/m-p/295680#M36593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom iMX6q board running with L3.0.35_4.1.0 kernel. I am using Ltib. I have added qt4.6.0 to it and i am able to run a few applications,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However now I am trying to install QT 5 or above in Ltib L3.0.35_4.1.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone tell me a procedure how to do it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;nishad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Apr 2014 13:31:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-QT-5-or-above-in-Ltib-L3-0-35-4-1-0/m-p/295680#M36593</guid>
      <dc:creator>nishad_kamdar</dc:creator>
      <dc:date>2014-04-14T13:31:54Z</dc:date>
    </item>
    <item>
      <title>Re: Installing QT 5 or above in Ltib L3.0.35_4.1.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-QT-5-or-above-in-Ltib-L3-0-35-4-1-0/m-p/295681#M36594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are two ways to archive this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Either with Yocto (There is already a layer with all configs done for you, meta-qt5) or cross-compiling against a LTIB rootfs. For the primer, please follow the meta-freescale distribution list, for the latter there is a page on the community, look for 'qt5' results (https://community.freescale.com/docs/DOC-94066?).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Apr 2014 15:30:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-QT-5-or-above-in-Ltib-L3-0-35-4-1-0/m-p/295681#M36594</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2014-04-14T15:30:36Z</dc:date>
    </item>
  </channel>
</rss>