<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 BitBlit function on GC320 in i.MX6SDL.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/BitBlit-function-on-GC320-in-i-MX6SDL/m-p/295353#M36514</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to use the BitBlit function on GC320 of i.MX6SDL in Linux.&lt;/P&gt;&lt;P&gt;When using the feature of 2D BitBlit, I think that the Vivante's API must be used.&lt;/P&gt;&lt;P&gt;To use the API of Vivante, the header file of Vivante becomes necessary.&lt;/P&gt;&lt;P&gt;Is it possible to get the source code of the graphics function of Vivante?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Keita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Apr 2014 08:14:59 GMT</pubDate>
    <dc:creator>keitanagashima</dc:creator>
    <dc:date>2014-04-14T08:14:59Z</dc:date>
    <item>
      <title>BitBlit function on GC320 in i.MX6SDL.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BitBlit-function-on-GC320-in-i-MX6SDL/m-p/295353#M36514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to use the BitBlit function on GC320 of i.MX6SDL in Linux.&lt;/P&gt;&lt;P&gt;When using the feature of 2D BitBlit, I think that the Vivante's API must be used.&lt;/P&gt;&lt;P&gt;To use the API of Vivante, the header file of Vivante becomes necessary.&lt;/P&gt;&lt;P&gt;Is it possible to get the source code of the graphics function of Vivante?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Keita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Apr 2014 08:14:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BitBlit-function-on-GC320-in-i-MX6SDL/m-p/295353#M36514</guid>
      <dc:creator>keitanagashima</dc:creator>
      <dc:date>2014-04-14T08:14:59Z</dc:date>
    </item>
    <item>
      <title>Re: BitBlit function on GC320 in i.MX6SDL.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BitBlit-function-on-GC320-in-i-MX6SDL/m-p/295354#M36515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Freescale does not provide GPU drivers sources because they are license protected.&lt;/P&gt;&lt;P&gt;Sources should be obtained only through local Freescale marketing channel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Apr 2014 09:12:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BitBlit-function-on-GC320-in-i-MX6SDL/m-p/295354#M36515</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-04-15T09:12:15Z</dc:date>
    </item>
    <item>
      <title>Re: BitBlit function on GC320 in i.MX6SDL.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BitBlit-function-on-GC320-in-i-MX6SDL/m-p/295355#M36516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear chipexpert,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;I understood that we can't get the GPU drivers source.&lt;/P&gt;&lt;P&gt;But, is it possible to use function of 2D BitBlit without the API's source code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Keita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Apr 2014 10:39:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BitBlit-function-on-GC320-in-i-MX6SDL/m-p/295355#M36516</guid>
      <dc:creator>keitanagashima</dc:creator>
      <dc:date>2014-04-15T10:39:41Z</dc:date>
    </item>
    <item>
      <title>Re: BitBlit function on GC320 in i.MX6SDL.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BitBlit-function-on-GC320-in-i-MX6SDL/m-p/295356#M36517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Keita&lt;/P&gt;&lt;P&gt;yes, 2D functions can be used please refer to&lt;/P&gt;&lt;P&gt;i.MX_6_G2D_API_User's_Guide.pdf included in&lt;/P&gt;&lt;P&gt;Linux documentation&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"L3.10.17_1.0.0_IMX6QDLS_BUNDLE&amp;nbsp; : Source Code Download Steps Documentation and Demo Images."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;nodeId=018rH3ZrDRB24A&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX6Q: i.MX 6Quad Family of Applications Processors&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;chip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 May 2014 07:29:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BitBlit-function-on-GC320-in-i-MX6SDL/m-p/295356#M36517</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2014-05-16T07:29:42Z</dc:date>
    </item>
  </channel>
</rss>