<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic g_ether/RNDIS not stable in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/g-ether-RNDIS-not-stable/m-p/162287#M3649</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are using 2.6.28 kernel on i.mx25. I am trying to establish RNDIS connection with Win XP computer.&lt;/P&gt;&lt;P&gt;It works on majority of XP SP3 computers, however not on all of them. On some computers I get 'Cannot start driver' (code 10) error. RNDIS driver is ver. 5.1.2600.5512 everywhere.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is also a computer with XP SP2. I tried installing hotfix as suggested in&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.droidforums.net/forum/tech-issues-bug-reports-suggestions/66688-solution-windows-xp-sp2-lower-problem-usb-tethering.html"&gt;http://www.droidforums.net/forum/tech-issues-bug-reports-suggestions/66688-solution-windows-xp-sp2-lower-problem-usb-tethering.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;unfortunately without success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Quite often I see kernel panic:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;[4294742.714000] Unable to handle kernel NULL pointer dereference at virtual address 00000002&lt;BR /&gt; [4294742.714000] pgd = c0004000&lt;BR /&gt; [4294742.714000] [00000002] *pgd=00000000&lt;BR /&gt; [4294742.714000] Internal error: Oops: 17 [#1] PREEMPT&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Seems that it happens if the board is connected to USB1.1 port after I install driver and unplug the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anybody know about the state of the RNDIS driver on the Linux side, which windows versions it is supposed to work with? Will updating to 2.6.31 solve the issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 May 2012 00:11:51 GMT</pubDate>
    <dc:creator>Pav</dc:creator>
    <dc:date>2012-05-18T00:11:51Z</dc:date>
    <item>
      <title>g_ether/RNDIS not stable</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/g-ether-RNDIS-not-stable/m-p/162287#M3649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are using 2.6.28 kernel on i.mx25. I am trying to establish RNDIS connection with Win XP computer.&lt;/P&gt;&lt;P&gt;It works on majority of XP SP3 computers, however not on all of them. On some computers I get 'Cannot start driver' (code 10) error. RNDIS driver is ver. 5.1.2600.5512 everywhere.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is also a computer with XP SP2. I tried installing hotfix as suggested in&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.droidforums.net/forum/tech-issues-bug-reports-suggestions/66688-solution-windows-xp-sp2-lower-problem-usb-tethering.html"&gt;http://www.droidforums.net/forum/tech-issues-bug-reports-suggestions/66688-solution-windows-xp-sp2-lower-problem-usb-tethering.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;unfortunately without success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Quite often I see kernel panic:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;[4294742.714000] Unable to handle kernel NULL pointer dereference at virtual address 00000002&lt;BR /&gt; [4294742.714000] pgd = c0004000&lt;BR /&gt; [4294742.714000] [00000002] *pgd=00000000&lt;BR /&gt; [4294742.714000] Internal error: Oops: 17 [#1] PREEMPT&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Seems that it happens if the board is connected to USB1.1 port after I install driver and unplug the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anybody know about the state of the RNDIS driver on the Linux side, which windows versions it is supposed to work with? Will updating to 2.6.31 solve the issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 May 2012 00:11:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/g-ether-RNDIS-not-stable/m-p/162287#M3649</guid>
      <dc:creator>Pav</dc:creator>
      <dc:date>2012-05-18T00:11:51Z</dc:date>
    </item>
  </channel>
</rss>