<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックFrame data shift issue while Integrating SE3300 Scan Engine with IMX25</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Frame-data-shift-issue-while-Integrating-SE3300-Scan-Engine-with/m-p/294535#M36353</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to integarte a SE3300(Sensor from motorola) with Imx25 through CSI interface.This sensor is 752x480 WVGA.I am facing frame data shift issue.After debugging i found if i set DMA BURST SIZE = 4 and RXFIFO = 96 ,i am not seeing the data shift issue in snap shot mode but with video mode there is always 2nd frame is shifted,&lt;/P&gt;&lt;P&gt;Apart from the mentioned settings ,none of the combination of these settiings works even in snap shot mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PFA the problem statement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please Help me on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Priti&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 May 2014 11:25:40 GMT</pubDate>
    <dc:creator>priti1z</dc:creator>
    <dc:date>2014-05-09T11:25:40Z</dc:date>
    <item>
      <title>Frame data shift issue while Integrating SE3300 Scan Engine with IMX25</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Frame-data-shift-issue-while-Integrating-SE3300-Scan-Engine-with/m-p/294535#M36353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to integarte a SE3300(Sensor from motorola) with Imx25 through CSI interface.This sensor is 752x480 WVGA.I am facing frame data shift issue.After debugging i found if i set DMA BURST SIZE = 4 and RXFIFO = 96 ,i am not seeing the data shift issue in snap shot mode but with video mode there is always 2nd frame is shifted,&lt;/P&gt;&lt;P&gt;Apart from the mentioned settings ,none of the combination of these settiings works even in snap shot mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PFA the problem statement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please Help me on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Priti&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 May 2014 11:25:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Frame-data-shift-issue-while-Integrating-SE3300-Scan-Engine-with/m-p/294535#M36353</guid>
      <dc:creator>priti1z</dc:creator>
      <dc:date>2014-05-09T11:25:40Z</dc:date>
    </item>
    <item>
      <title>Re: Frame data shift issue while Integrating SE3300 Scan Engine with IMX25</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Frame-data-shift-issue-while-Integrating-SE3300-Scan-Engine-with/m-p/294536#M36354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your post, however please consider moving it to the right community place (e.g. &lt;A _jive_internal="true" class="jivecontainerTT-hover-container jive-link-community-small" data-containerid="1" data-containertype="14" data-content-finding="Community" data-objectid="2004" data-objecttype="14" href="https://community.nxp.com/community/imx"&gt;i.MX Community&lt;/A&gt; ) to get it visible for active members.&lt;/P&gt;&lt;P&gt;For details please see general advice &lt;A _jive_internal="true" data-containerid="2001" data-containertype="14" data-content-finding="Community" data-objectid="99909" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99909"&gt;Where to post a Discussion?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for using Freescale Community. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 May 2014 12:42:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Frame-data-shift-issue-while-Integrating-SE3300-Scan-Engine-with/m-p/294536#M36354</guid>
      <dc:creator>Wlodek_D_</dc:creator>
      <dc:date>2014-05-09T12:42:42Z</dc:date>
    </item>
  </channel>
</rss>