<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Need help for beginner with imx233! in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Need-help-for-beginner-with-imx233/m-p/294532#M36350</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I intended to use imx233, so I need some your point to understand quickly about it, such as I want to build an application (&lt;STRONG&gt;standalone&lt;/STRONG&gt;):&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; What is minimium of hardware required? ( imx233+ SDRAM +...?)&lt;/P&gt;&lt;P&gt;2. When I have bin file (created by such iar arm) , how can I do in-circuit flash programmer as other microcontroller?&lt;/P&gt;&lt;P&gt;Thanks for help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Apr 2014 16:38:05 GMT</pubDate>
    <dc:creator>TuanNguyen</dc:creator>
    <dc:date>2014-04-11T16:38:05Z</dc:date>
    <item>
      <title>Need help for beginner with imx233!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Need-help-for-beginner-with-imx233/m-p/294532#M36350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I intended to use imx233, so I need some your point to understand quickly about it, such as I want to build an application (&lt;STRONG&gt;standalone&lt;/STRONG&gt;):&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; What is minimium of hardware required? ( imx233+ SDRAM +...?)&lt;/P&gt;&lt;P&gt;2. When I have bin file (created by such iar arm) , how can I do in-circuit flash programmer as other microcontroller?&lt;/P&gt;&lt;P&gt;Thanks for help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Apr 2014 16:38:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Need-help-for-beginner-with-imx233/m-p/294532#M36350</guid>
      <dc:creator>TuanNguyen</dc:creator>
      <dc:date>2014-04-11T16:38:05Z</dc:date>
    </item>
    <item>
      <title>Re: Need help for beginner with imx233!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Need-help-for-beginner-with-imx233/m-p/294533#M36351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd recommend:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- i.MX233&lt;/P&gt;&lt;P&gt;- SDRAM&lt;/P&gt;&lt;P&gt;- Boot source: NAND flash, NOR flash or SD card&lt;/P&gt;&lt;P&gt;- JTAG interface&lt;/P&gt;&lt;P&gt;- Debug UART interface&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That way you can generate test codes running from internal memory (through JTAG) and also test a real boot program that runs from an external memory and debug it from UART.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;BR /&gt;Jorge.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Apr 2014 17:00:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Need-help-for-beginner-with-imx233/m-p/294533#M36351</guid>
      <dc:creator>JorgeRama_rezRi</dc:creator>
      <dc:date>2014-04-11T17:00:34Z</dc:date>
    </item>
    <item>
      <title>Re: Need help for beginner with imx233!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Need-help-for-beginner-with-imx233/m-p/294534#M36352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try to get access to a mx23 olinuxino board and then you can flash U-boot into the SD card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-boot allows you to launch standalone applications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Apr 2014 20:34:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Need-help-for-beginner-with-imx233/m-p/294534#M36352</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2014-04-11T20:34:38Z</dc:date>
    </item>
  </channel>
</rss>