<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Uboot configuration</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-configuration/m-p/294530#M36348</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you &lt;/P&gt;&lt;P&gt;Vasilis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Mar 2014 11:12:41 GMT</pubDate>
    <dc:creator>vasileiostzizil</dc:creator>
    <dc:date>2014-03-17T11:12:41Z</dc:date>
    <item>
      <title>Uboot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-configuration/m-p/294528#M36346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;/P&gt;&lt;P&gt;I want to change the configuration of the Uboot for iMX6.&lt;/P&gt;&lt;P&gt;The uboot as I understand has a configuration that goes that after you download it to eMMC or SD card goes and writes that configuration in the emmc before the main partition.&lt;/P&gt;&lt;P&gt;So even if you change uboot that configuration remainsis it is not formatted. You can change that configuration if you run some commands from the uboot have installed and write that conf.&lt;/P&gt;&lt;P&gt;That configuration is if the uboot will look from ethernet the linux image and etc.&lt;/P&gt;&lt;P&gt;My problem is that in the board I have I do not have a console output to set the configuration file after I download this uboot, So I have to set them up in the bin.&lt;/P&gt;&lt;P&gt;The ltib I am using has just the basic for building the uboot. Does anyone knows where exactly is the source&amp;nbsp; file for that or another more detail way to configure uboot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Vasilis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Mar 2014 13:44:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-configuration/m-p/294528#M36346</guid>
      <dc:creator>vasileiostzizil</dc:creator>
      <dc:date>2014-03-12T13:44:18Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-configuration/m-p/294529#M36347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First run command&amp;nbsp; "dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1536 count=16" to clean up u-boot parameter in&amp;nbsp; SD/eMMC card. If there is no boot parameter in SD/eMMC&amp;nbsp; card, the default boot parameter will be used. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then modify u-boot-2009.08/include/configs/mx6dl_sabresd.h(depends which platform you use&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define CONFIG_EXTRA_ENV_SETTINGS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "netdev=eth0\0"&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "ethprime=FEC0\0"&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "uboot=u-boot.bin\0"&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "kernel=uImage\0"&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "nfsroot=/opt/eldk/arm\0"&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "bootargs_base=setenv bootargs console=ttymxc0,115200\0"\&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs "\&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp\0"\&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "bootcmd_net=run bootargs_base bootargs_nfs; "&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "tftpboot ${loadaddr} ${kernel}; bootm\0" \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "bootargs_mmc=setenv bootargs ${bootargs} ip=dhcp "&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "root=/dev/mmcblk0p1 rootwait\0"&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "bootcmd_mmc=run bootargs_base bootargs_mmc; "&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "mmc dev 3; " \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "mmc read ${loadaddr} 0x800 0x2000; bootm\0"&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; "bootcmd=run bootcmd_net\0"&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Grace&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Mar 2014 03:33:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-configuration/m-p/294529#M36347</guid>
      <dc:creator>GraceH</dc:creator>
      <dc:date>2014-03-17T03:33:49Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-configuration/m-p/294530#M36348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you &lt;/P&gt;&lt;P&gt;Vasilis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Mar 2014 11:12:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-configuration/m-p/294530#M36348</guid>
      <dc:creator>vasileiostzizil</dc:creator>
      <dc:date>2014-03-17T11:12:41Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-configuration/m-p/294531#M36349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Grace,&lt;/P&gt;&lt;P&gt;Am facing the same problem in the 2017.03 uboot.... We have got imx6s processor custom board... So using config for imx6dl defconfigs for building uboot... But it is not detecting emmc as a boot device... It is taking sd3 as boot device and tells mmc card not found.... Where to set this... can u plz help me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2018 01:05:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-configuration/m-p/294531#M36349</guid>
      <dc:creator>prasannakulkarni</dc:creator>
      <dc:date>2018-04-11T01:05:17Z</dc:date>
    </item>
  </channel>
</rss>