<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Source and Sink Current on i.MX6 SoloLite</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Source-and-Sink-Current-on-i-MX6-SoloLite/m-p/294509#M36336</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to find the maximum recommended source and sink currents for pins on the MCIMX6L2EVN10AB when used as GPIO.&amp;nbsp; Any help would be appreciated.&amp;nbsp; I have looked in the hardware development guide, reference manual, and datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;dave boling&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Apr 2014 16:00:08 GMT</pubDate>
    <dc:creator>davidboling</dc:creator>
    <dc:date>2014-04-11T16:00:08Z</dc:date>
    <item>
      <title>Source and Sink Current on i.MX6 SoloLite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Source-and-Sink-Current-on-i-MX6-SoloLite/m-p/294509#M36336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to find the maximum recommended source and sink currents for pins on the MCIMX6L2EVN10AB when used as GPIO.&amp;nbsp; Any help would be appreciated.&amp;nbsp; I have looked in the hardware development guide, reference manual, and datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;dave boling&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Apr 2014 16:00:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Source-and-Sink-Current-on-i-MX6-SoloLite/m-p/294509#M36336</guid>
      <dc:creator>davidboling</dc:creator>
      <dc:date>2014-04-11T16:00:08Z</dc:date>
    </item>
    <item>
      <title>Re: Source and Sink Current on i.MX6 SoloLite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Source-and-Sink-Current-on-i-MX6-SoloLite/m-p/294510#M36337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; There are values of load current in the Datasheet(s), which relate to some typical configurations, &lt;/P&gt;&lt;P&gt;in particular - in order to guarantee specified output voltages. For more &lt;/P&gt;&lt;P&gt;accurate (application depended) estimations IBIS models should be applied. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Really the data of i.MX Datasheets specify maximum / minimum voltage levels &lt;/P&gt;&lt;P&gt;in relation with current loads. These current values should not be considered as &lt;/P&gt;&lt;P&gt;maximum allowed ones, just as reasonable. IBIS model provides current-voltage &lt;/P&gt;&lt;P&gt;curves for pins in order to calculate real currents and voltages on pins. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Another case, that corresponding voltage (high, low) levels may not be in &lt;/P&gt;&lt;P&gt;ranges, shown in Datasheet and defined as logical 0 or 1.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Maximum current values (which do not decrease life time and do not damage the device) &lt;/P&gt;&lt;P&gt;are not specified, because they are application dependent and relate to general thermal &lt;/P&gt;&lt;P&gt;estimations. Say, if a separate pin can sink high current, say greater than 8 mA, this does not &lt;/P&gt;&lt;P&gt;mean that all pins may be loaded (simultaneously) with such values. Strictly speaking the i.MX6&lt;/P&gt;&lt;P&gt;is not intended to be used as high current GPIO source or sink, assuming that special buffers&lt;/P&gt;&lt;P&gt;or I/O expanders should be applied for it. &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Apr 2014 08:02:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Source-and-Sink-Current-on-i-MX6-SoloLite/m-p/294510#M36337</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-04-14T08:02:14Z</dc:date>
    </item>
    <item>
      <title>Re: Source and Sink Current on i.MX6 SoloLite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Source-and-Sink-Current-on-i-MX6-SoloLite/m-p/294511#M36338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the clarification.&lt;/P&gt;&lt;P&gt;It is very clear that " MX6 is not intended to be used as high current GPIO source or sink" But while doing FMEA we have a case where a MX6 GPIO output (LOW) is shorted with 3V3 externally. In that case what max sink current will flow? How does it impact MX6?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this sink current is limited by GPIO buffer output impedance i.e Sink Current = 3.3/Impedance?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Vinod&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Sep 2015 10:11:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Source-and-Sink-Current-on-i-MX6-SoloLite/m-p/294511#M36338</guid>
      <dc:creator>vinodhodal</dc:creator>
      <dc:date>2015-09-07T10:11:30Z</dc:date>
    </item>
    <item>
      <title>Re: Source and Sink Current on i.MX6 SoloLite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Source-and-Sink-Current-on-i-MX6-SoloLite/m-p/294512#M36339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I am afraid, we cannot guarantee proper operations after the short circuit cases.&lt;/P&gt;&lt;P&gt;There are no specifications for the max current for "critical" cases. &lt;/P&gt;&lt;P&gt;Nevertheless, the approach "&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Sink Current = 3.3/Impedance?&lt;/SPAN&gt;" may be used for estimations.&lt;/P&gt;&lt;P&gt;Generally : several tens of mA during short time will not cause "mortal"&amp;nbsp; result.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 10:18:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Source-and-Sink-Current-on-i-MX6-SoloLite/m-p/294512#M36339</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-09-08T10:18:55Z</dc:date>
    </item>
    <item>
      <title>Re: Source and Sink Current on i.MX6 SoloLite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Source-and-Sink-Current-on-i-MX6-SoloLite/m-p/294513#M36340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any safe limit sink current&amp;nbsp; or source current value of GPIO that will be OK for IMX6? We want to calculate minimum external series resistance value that will protect from such short circuit cases.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vinod&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 12:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Source-and-Sink-Current-on-i-MX6-SoloLite/m-p/294513#M36340</guid>
      <dc:creator>vinodhodal</dc:creator>
      <dc:date>2015-09-08T12:25:51Z</dc:date>
    </item>
  </channel>
</rss>