<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6q OpenCL drivers (Ubuntu) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6q-OpenCL-drivers-Ubuntu/m-p/294393#M36313</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am currently working on a research project where we build up a cluster consisting of nine Wandboard Quads. One is the head and eight nodes.&lt;/P&gt;&lt;P&gt;We started the project with the standart Ubuntu SD Image with kernel Version 3.0.35+&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OpenCL was then working very fine&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Due to a network conflict and the need to have the cluster in a seperate network we bought an USB network adapter to connect the head with the internet and the onboard ethernet chips are used for the closed network.&lt;/P&gt;&lt;P&gt;so far so good&lt;/P&gt;&lt;P&gt;due to incompatability with the used kernel version the kernel had to be updated to version 3.10.17 and the network driver has been backported successfully.&lt;/P&gt;&lt;P&gt;But now OpenCL is not working, when i try to start a programm i get the message&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ioctl(3, 0x7530, 0x7e9191d8)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = -1 ENOTTY (Inappropriate ioctl for device)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So i guess the Kernel API changed in the new used kernel&lt;/P&gt;&lt;P&gt;are there any OpenCL sources for this specific Kernel version to get OpenCL running again?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Mar 2014 13:30:15 GMT</pubDate>
    <dc:creator>mathiasradtke</dc:creator>
    <dc:date>2014-03-12T13:30:15Z</dc:date>
    <item>
      <title>iMX6q OpenCL drivers (Ubuntu)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6q-OpenCL-drivers-Ubuntu/m-p/294393#M36313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am currently working on a research project where we build up a cluster consisting of nine Wandboard Quads. One is the head and eight nodes.&lt;/P&gt;&lt;P&gt;We started the project with the standart Ubuntu SD Image with kernel Version 3.0.35+&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OpenCL was then working very fine&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Due to a network conflict and the need to have the cluster in a seperate network we bought an USB network adapter to connect the head with the internet and the onboard ethernet chips are used for the closed network.&lt;/P&gt;&lt;P&gt;so far so good&lt;/P&gt;&lt;P&gt;due to incompatability with the used kernel version the kernel had to be updated to version 3.10.17 and the network driver has been backported successfully.&lt;/P&gt;&lt;P&gt;But now OpenCL is not working, when i try to start a programm i get the message&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ioctl(3, 0x7530, 0x7e9191d8)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = -1 ENOTTY (Inappropriate ioctl for device)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So i guess the Kernel API changed in the new used kernel&lt;/P&gt;&lt;P&gt;are there any OpenCL sources for this specific Kernel version to get OpenCL running again?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Mar 2014 13:30:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6q-OpenCL-drivers-Ubuntu/m-p/294393#M36313</guid>
      <dc:creator>mathiasradtke</dc:creator>
      <dc:date>2014-03-12T13:30:15Z</dc:date>
    </item>
  </channel>
</rss>