<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6 Reset Image in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Reset-Image/m-p/293706#M36191</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Poussemoousse&lt;/P&gt;&lt;P&gt;Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel &lt;/P&gt;&lt;P&gt;free to reply with an update to this discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Feb 2014 07:40:48 GMT</pubDate>
    <dc:creator>YixingKong</dc:creator>
    <dc:date>2014-02-21T07:40:48Z</dc:date>
    <item>
      <title>iMX6 Reset Image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Reset-Image/m-p/293703#M36188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;Is there any pin on iMX6 (Solo) which is the image of the processor Reset internal state.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;I would like to use it in order to warn external component that the processor is in Reset state.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;I am wondering if &lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;SRC_ONOFF or PMIC_ON_REQ&lt;/SPAN&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt; could be used.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif'; font-size: 12pt;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif'; font-size: 12pt;"&gt;Any idea is welcome,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;&lt;SPAN style="font-size: 12pt;"&gt;Poussemousse&lt;/SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2013 15:50:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Reset-Image/m-p/293703#M36188</guid>
      <dc:creator>Poussemousse</dc:creator>
      <dc:date>2013-09-09T15:50:05Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Reset Image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Reset-Image/m-p/293704#M36189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't know of such a pin on iMX6 but perhaps I didn't see it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyway, you can use a simple GPIO for this task. Add a pull-up or pull-down. At reset, GPIO are defined as inputs. When your system is ready, switch it to output and toggle it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That's the way I would do as you're free to choose when you consider the system is operational.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Frederic Thierry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Sep 2013 15:24:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Reset-Image/m-p/293704#M36189</guid>
      <dc:creator>fredericthierry</dc:creator>
      <dc:date>2013-09-12T15:24:08Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Reset Image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Reset-Image/m-p/293705#M36190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Haven't seen such reset output signal we may had in previous architectures. ONOFF can generate reset but is an input. PMIC-ON-REQ is a wake up request after ON OFF has been pushed but only if you use this optional scenario. The real reset signal is POR/. Even if it is asserted by PMIC once voltages are stables, you can use the same if the intent is to propagate it to your peripherals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To manage further cold or warm resets, you need to analyse the possible sources in your system (check SRCF_SRSR for the list) to disable or combine them :&lt;/P&gt;&lt;P&gt;* Warm reset : software reset, can be disabled or obviously managed by software&lt;/P&gt;&lt;P&gt;* Jtag : you can use same external signal if hardware, probably avoid software jtag reset&lt;/P&gt;&lt;P&gt;* Watchdog&amp;nbsp; : WDOG_B signals can be configured as output&lt;/P&gt;&lt;P&gt;* Ipp_user : ON OFF button if used&lt;/P&gt;&lt;P&gt;* Csu : if security / tamper is enabled&lt;/P&gt;&lt;P&gt;* Ipp : POR/ pin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards, Philippe.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Sep 2013 12:36:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Reset-Image/m-p/293705#M36190</guid>
      <dc:creator>ZeeFrench</dc:creator>
      <dc:date>2013-09-13T12:36:16Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Reset Image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Reset-Image/m-p/293706#M36191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Poussemoousse&lt;/P&gt;&lt;P&gt;Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel &lt;/P&gt;&lt;P&gt;free to reply with an update to this discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Feb 2014 07:40:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Reset-Image/m-p/293706#M36191</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-21T07:40:48Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Reset Image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Reset-Image/m-p/293707#M36192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Poussemoous&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2014 07:47:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Reset-Image/m-p/293707#M36192</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-26T07:47:12Z</dc:date>
    </item>
  </channel>
</rss>