<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6DQ LPDDR2 Initialization Issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-LPDDR2-Initialization-Issue/m-p/293693#M36185</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please use signal channel mode, and the reference dram setting is attached&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Aven&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Sep 2013 06:19:47 GMT</pubDate>
    <dc:creator>aven_tsao</dc:creator>
    <dc:date>2013-09-13T06:19:47Z</dc:date>
    <item>
      <title>iMX6DQ LPDDR2 Initialization Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-LPDDR2-Initialization-Issue/m-p/293692#M36184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to configure LPDDR2 on a custom iMX6DQ board and am having issues. Every time I perform a read I get back something different and when I write I do not see it being stored.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(gdb) monitor mdw 0x80000000 8&lt;/P&gt;&lt;P&gt;0x80000000: 10e63e50 d13f3450 f43ec9c5 728b8190 080050cf 65507050 dc391598 0010f206 &lt;/P&gt;&lt;P&gt;(gdb) monitor mww 0x80000000 0xffffffff&lt;/P&gt;&lt;P&gt;(gdb) monitor mdw 0x80000000 8&lt;/P&gt;&lt;P&gt;0x80000000: 100000ff 908b0050 08ffffc5 723f3490 ffb4c95e d1108184 d0395098 00507006 &lt;/P&gt;&lt;P&gt;(gdb) monitor mdw 0x80000000 8&lt;/P&gt;&lt;P&gt;0x80000000: 10e660ff 10e66050 10e660c5 723f8190 08ffc95e d18b3484 ff00ff98 0050f206 &lt;/P&gt;&lt;P&gt;(gdb) monitor mdw 0x80000000 8&lt;/P&gt;&lt;P&gt;0x80000000: 08e66050 72e62090 ffe6c9c5 d18b8150 d000ffff 003f3406 dcff1598 6510f284 &lt;/P&gt;&lt;P&gt;(gdb) monitor mdw 0x80000000 8&lt;/P&gt;&lt;P&gt;0x80000000: 10e66050 d1e66050 ffe6ffc5 723f3490 08ffc9ff 658b8150 dc005098 00507006 &lt;/P&gt;&lt;P&gt;(gdb) monitor mdw 0x80000000 8&lt;/P&gt;&lt;P&gt;0x80000000: ffe66050 d1e66050 080060c5 728b8190 dcffc9ff 653f3450 d0b4ff98 0010f206 &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The board is a single channel configuration using Micron’s DDR2 MT42L256M32D2LG-18 WT:A&lt;/P&gt;&lt;P&gt;I set the memory mapping mode to Dual channel (2x 32-bit), Fixed mapping (LPDDR2) (which starts from 0x80000000 and 0x10000000 -&amp;gt; 7FFFFFFFF is not used)&lt;/P&gt;&lt;P&gt;I then used a flyswatter2 and openocd tcl script to perform the DCD initializations. (attached to this email)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Am I supposed to reduce the clock speed before setting the DCD settings? ( I don’t see this done in any of your sample code but the LPDDR2 spec says something of the sort should be done)&lt;/P&gt;&lt;P&gt;Also I am unable to execute the following due to JTAG-DP STICKY ERROR&lt;/P&gt;&lt;P&gt;# Switch PL301_FAST2 to DDR Dual-channel mapping &lt;/P&gt;&lt;P&gt;mww 0x00B00000 0x1&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What could be causing my reads to be corrupt? Could this be a delay/calibration issue? I have played around with my delay and impedance settings but am having the same issue.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Your input would be much appreciated&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-335990"&gt;lpddr2_mmdc_dcd_settings.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-335990"&gt;jtag_init_script.cfg.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2013 15:13:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-LPDDR2-Initialization-Issue/m-p/293692#M36184</guid>
      <dc:creator>rp123</dc:creator>
      <dc:date>2013-09-09T15:13:50Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6DQ LPDDR2 Initialization Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-LPDDR2-Initialization-Issue/m-p/293693#M36185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please use signal channel mode, and the reference dram setting is attached&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Aven&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Sep 2013 06:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-LPDDR2-Initialization-Issue/m-p/293693#M36185</guid>
      <dc:creator>aven_tsao</dc:creator>
      <dc:date>2013-09-13T06:19:47Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6DQ LPDDR2 Initialization Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-LPDDR2-Initialization-Issue/m-p/293694#M36186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;I am afraid the i.MX6Q supports &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;only dual-channel LPDDR2 (both CS0 and CS1 are active).&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Sep 2013 04:27:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-LPDDR2-Initialization-Issue/m-p/293694#M36186</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-09-16T04:27:50Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6DQ LPDDR2 Initialization Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-LPDDR2-Initialization-Issue/m-p/293695#M36187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The dual channel mode only support LPDDR2 device, but the signal channel mode support both LPDDR2 and DDR3.&lt;/P&gt;&lt;P&gt;In this case, it should use signal channel mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Aven&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Sep 2013 09:01:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6DQ-LPDDR2-Initialization-Issue/m-p/293695#M36187</guid>
      <dc:creator>aven_tsao</dc:creator>
      <dc:date>2013-09-16T09:01:30Z</dc:date>
    </item>
  </channel>
</rss>