<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックmemory layout - 'Physical memory allocation error!' - Wandboard-solo</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/memory-layout-Physical-memory-allocation-error-Wandboard-solo/m-p/293578#M36144</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for a while now I try to get 1080p playback within QtMultimedia (using gstreamer) to working on Wandboard-solo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The core problem is that as soon as gstreamer tries to allocate the pipeline, the kernel errors occur:&lt;/P&gt;&lt;P&gt;"...&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 222.738637] Physical memory allocation error!&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 222.759710] Physical memory allocation error!&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;(I don't have the complete kernel log at hand right now, but if it's useful I can provide it)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On application side the gstreamer-error is:&lt;/P&gt;&lt;P&gt;[ERR]&amp;nbsp;&amp;nbsp; mem allocation failed!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's workign flawlessly with 720p&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried the wandboard mailinglist: &lt;A href="https://groups.google.com/forum/#!topic/wandboard/XvF_kjEKC2c" title="https://groups.google.com/forum/#!topic/wandboard/XvF_kjEKC2c"&gt;https://groups.google.com/forum/#!topic/wandboard/XvF_kjEKC2c&lt;/A&gt;&lt;/P&gt;&lt;P&gt; .. without success&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is also another thread here where this discussion started: &lt;A _jive_internal="true" href="https://community.nxp.com/thread/307038" title="https://community.freescale.com/thread/307038"&gt;https://community.freescale.com/thread/307038&lt;/A&gt;&lt;/P&gt;&lt;P&gt;(as it's marked answered and its' a bit overloaded, starting a new thread made sense)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gst playbin is working, but only(!) if frame-"bufferplus" is reduced from 6 to a lower value .. but:&lt;/P&gt;&lt;P&gt; 1. This is only working with a plain gst-launch, not when gstreamer is running within QtMultimedia (I assume it's the fact that someone else is allocating OpenGL memory, but I'm not sure)&lt;/P&gt;&lt;P&gt; 2. It makes the gstreamer pipeline unstable&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my conclusion is either:&lt;/P&gt;&lt;P&gt; A: This is a HW-limitation of 512mb i.MX6 board,s which would mean there is no clean way to combine 1080p and OpenGL based application (e.g. QtQuick2.)&lt;/P&gt;&lt;P&gt; B: There is a problem with the memory layout in the wandboard-solo kernel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone an idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Greets&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Sep 2013 11:28:17 GMT</pubDate>
    <dc:creator>senykthomas</dc:creator>
    <dc:date>2013-09-09T11:28:17Z</dc:date>
    <item>
      <title>memory layout - 'Physical memory allocation error!' - Wandboard-solo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/memory-layout-Physical-memory-allocation-error-Wandboard-solo/m-p/293578#M36144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for a while now I try to get 1080p playback within QtMultimedia (using gstreamer) to working on Wandboard-solo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The core problem is that as soon as gstreamer tries to allocate the pipeline, the kernel errors occur:&lt;/P&gt;&lt;P&gt;"...&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 222.738637] Physical memory allocation error!&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 222.759710] Physical memory allocation error!&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;(I don't have the complete kernel log at hand right now, but if it's useful I can provide it)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On application side the gstreamer-error is:&lt;/P&gt;&lt;P&gt;[ERR]&amp;nbsp;&amp;nbsp; mem allocation failed!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's workign flawlessly with 720p&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried the wandboard mailinglist: &lt;A href="https://groups.google.com/forum/#!topic/wandboard/XvF_kjEKC2c" title="https://groups.google.com/forum/#!topic/wandboard/XvF_kjEKC2c"&gt;https://groups.google.com/forum/#!topic/wandboard/XvF_kjEKC2c&lt;/A&gt;&lt;/P&gt;&lt;P&gt; .. without success&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is also another thread here where this discussion started: &lt;A _jive_internal="true" href="https://community.nxp.com/thread/307038" title="https://community.freescale.com/thread/307038"&gt;https://community.freescale.com/thread/307038&lt;/A&gt;&lt;/P&gt;&lt;P&gt;(as it's marked answered and its' a bit overloaded, starting a new thread made sense)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gst playbin is working, but only(!) if frame-"bufferplus" is reduced from 6 to a lower value .. but:&lt;/P&gt;&lt;P&gt; 1. This is only working with a plain gst-launch, not when gstreamer is running within QtMultimedia (I assume it's the fact that someone else is allocating OpenGL memory, but I'm not sure)&lt;/P&gt;&lt;P&gt; 2. It makes the gstreamer pipeline unstable&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my conclusion is either:&lt;/P&gt;&lt;P&gt; A: This is a HW-limitation of 512mb i.MX6 board,s which would mean there is no clean way to combine 1080p and OpenGL based application (e.g. QtQuick2.)&lt;/P&gt;&lt;P&gt; B: There is a problem with the memory layout in the wandboard-solo kernel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone an idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Greets&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2013 11:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/memory-layout-Physical-memory-allocation-error-Wandboard-solo/m-p/293578#M36144</guid>
      <dc:creator>senykthomas</dc:creator>
      <dc:date>2013-09-09T11:28:17Z</dc:date>
    </item>
  </channel>
</rss>