<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMouse not work with fsl-image-gui</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Mouse-not-work-with-fsl-image-gui/m-p/293173#M36039</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all, &lt;/P&gt;&lt;P&gt;I have built the fsl-image-gui by yocto, when booting it shows udev cannot setup, because my kernel doesn't support udev, so I add the "exit 0" at the top of /etc/iniit.d/udev,&lt;/P&gt;&lt;P&gt;then I can see the login part on terminal, but when I insert my usb mouse, it cannot work.&lt;/P&gt;&lt;P&gt;When inserting, log shows:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;root@imx53qsb:/# &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;root@imx53qsb:/# &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;root@imx53qsb:/# usb 2-1.3: USB disconnect, address 4&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;usb 2-1.4: new low speed USB device using fsl-ehci and address 5&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;input: USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1.4/2-1.4:1.0/input/input8&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;generic-usb 0003:1BCF:0007.0003: input: USB HID v1.10 Mouse [USB Optical Mouse] on usb-fsl-ehci.1-1.4/input0&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I use the qt4e-demo-image, I can using my mouse for selecting each QT demo, but I cannot use it by fsl-image-gui.&lt;/P&gt;&lt;P&gt;Is there some command I forget to type in?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Nov 2013 07:09:52 GMT</pubDate>
    <dc:creator>zhangjay</dc:creator>
    <dc:date>2013-11-22T07:09:52Z</dc:date>
    <item>
      <title>Mouse not work with fsl-image-gui</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mouse-not-work-with-fsl-image-gui/m-p/293173#M36039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all, &lt;/P&gt;&lt;P&gt;I have built the fsl-image-gui by yocto, when booting it shows udev cannot setup, because my kernel doesn't support udev, so I add the "exit 0" at the top of /etc/iniit.d/udev,&lt;/P&gt;&lt;P&gt;then I can see the login part on terminal, but when I insert my usb mouse, it cannot work.&lt;/P&gt;&lt;P&gt;When inserting, log shows:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;root@imx53qsb:/# &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;root@imx53qsb:/# &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;root@imx53qsb:/# usb 2-1.3: USB disconnect, address 4&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;usb 2-1.4: new low speed USB device using fsl-ehci and address 5&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;input: USB Optical Mouse as /devices/platform/fsl-ehci.1/usb2/2-1/2-1.4/2-1.4:1.0/input/input8&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;generic-usb 0003:1BCF:0007.0003: input: USB HID v1.10 Mouse [USB Optical Mouse] on usb-fsl-ehci.1-1.4/input0&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I use the qt4e-demo-image, I can using my mouse for selecting each QT demo, but I cannot use it by fsl-image-gui.&lt;/P&gt;&lt;P&gt;Is there some command I forget to type in?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Nov 2013 07:09:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mouse-not-work-with-fsl-image-gui/m-p/293173#M36039</guid>
      <dc:creator>zhangjay</dc:creator>
      <dc:date>2013-11-22T07:09:52Z</dc:date>
    </item>
    <item>
      <title>Re: Mouse not work with fsl-image-gui</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mouse-not-work-with-fsl-image-gui/m-p/293174#M36040</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;is there any "startx" script in your filesystem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2013 04:06:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mouse-not-work-with-fsl-image-gui/m-p/293174#M36040</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-11-26T04:06:25Z</dc:date>
    </item>
    <item>
      <title>Re: Mouse not work with fsl-image-gui</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mouse-not-work-with-fsl-image-gui/m-p/293175#M36041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Zhang, this question can also be posted on the meta-freescale mailing list. So may get faster response for Yocto related issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2013 16:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mouse-not-work-with-fsl-image-gui/m-p/293175#M36041</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-11-26T16:38:57Z</dc:date>
    </item>
    <item>
      <title>Re: Mouse not work with fsl-image-gui</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mouse-not-work-with-fsl-image-gui/m-p/293176#M36042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2013 01:24:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mouse-not-work-with-fsl-image-gui/m-p/293176#M36042</guid>
      <dc:creator>zhangjay</dc:creator>
      <dc:date>2013-11-27T01:24:03Z</dc:date>
    </item>
  </channel>
</rss>