<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Advanced Toolkit Warning, i.MX vs ColdFire</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Advanced-Toolkit-Warning-i-MX-vs-ColdFire/m-p/293072#M36027</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Tom,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Advanced Toolkit is also called ATK tool which is used to burn images into flash on board based on i.mx SOC. But this tool has been replaced with MFG Tool , and Freescale will not support and maintence ATK Tool.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; So you will have to use MFG Tool to burn images into flash on i.mx53 board. you can download it from freescale offical website :&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&amp;amp;nodeId=018rH3ZrDR988D&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&amp;amp;nodeId=018rH3ZrDR988D&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39951i6665D9761DC5A655/image-size/large?v=v2&amp;amp;px=999" title="imx-mfg-tool.png" alt="imx-mfg-tool.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Sep 2013 10:27:14 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2013-09-06T10:27:14Z</dc:date>
    <item>
      <title>Advanced Toolkit Warning, i.MX vs ColdFire</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Advanced-Toolkit-Warning-i-MX-vs-ColdFire/m-p/293071#M36026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We're using the i.MX53 on a Karo TX53 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I managed (with help) to wipe out the RedBoot bootloader, and was then advised to use the "Advanced Toolkit" to reflash the boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The installer (possibly a little too old) was the file "FSL_ATK_TOOL_WINS_STD_INSTALL_1_68.exe". I've looked on Freescale's site and there doesn't seem to be anything newer, AND this isn't linked from the i.MX53 page, only the i.MX27.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The installation went and installed some USB Drivers. That's always a sign of problems.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The Toolkit wouldn't work. It couldn't find the i.MX53 at all. The interface implied it might work with a Serial Port or USB (it let me select Serial), but that didn't work either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I found that it had also wrecked my existing installation of the drivers for the P&amp;amp;E Micro USB ColdFire Multilink. They both use something called "Jungo", but they seem to be mutually incompatible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the Device Manager on my PC, the "Jungo / USB Multilink 2.0" icon had the yellow triangle next to it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luck for me, the "System Restore" was able to put my computer back before the failed install.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Sep 2013 06:58:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Advanced-Toolkit-Warning-i-MX-vs-ColdFire/m-p/293071#M36026</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2013-09-06T06:58:03Z</dc:date>
    </item>
    <item>
      <title>Re: Advanced Toolkit Warning, i.MX vs ColdFire</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Advanced-Toolkit-Warning-i-MX-vs-ColdFire/m-p/293072#M36027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Tom,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Advanced Toolkit is also called ATK tool which is used to burn images into flash on board based on i.mx SOC. But this tool has been replaced with MFG Tool , and Freescale will not support and maintence ATK Tool.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; So you will have to use MFG Tool to burn images into flash on i.mx53 board. you can download it from freescale offical website :&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&amp;amp;nodeId=018rH3ZrDR988D&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&amp;amp;nodeId=018rH3ZrDR988D&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39951i6665D9761DC5A655/image-size/large?v=v2&amp;amp;px=999" title="imx-mfg-tool.png" alt="imx-mfg-tool.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Sep 2013 10:27:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Advanced-Toolkit-Warning-i-MX-vs-ColdFire/m-p/293072#M36027</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2013-09-06T10:27:14Z</dc:date>
    </item>
    <item>
      <title>Re: Advanced Toolkit Warning, i.MX vs ColdFire</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Advanced-Toolkit-Warning-i-MX-vs-ColdFire/m-p/293073#M36028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2014 06:40:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Advanced-Toolkit-Warning-i-MX-vs-ColdFire/m-p/293073#M36028</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-24T06:40:20Z</dc:date>
    </item>
  </channel>
</rss>