<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックWhere to start?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Where-to-start/m-p/161968#M3583</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear developers,&lt;/P&gt;&lt;P&gt;I have taken on the task of porting CyanogenMod for a device which is based on i.MX515 and is called the &lt;A href="http://www.synrgic.com/index.php?option=com_content&amp;amp;view=article&amp;amp;id=95&amp;amp;Itemid=192&amp;amp;lang=en" target="_blank"&gt;Dreambook W7&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Where do I start? How do I flash a custom image for this thing? Which docs should I read?&lt;/P&gt;&lt;P&gt;Is there a prebuilt kernel? A whole android build? I'd love to know all these things and I bet they are documented somewhere.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Shahar&lt;/P&gt;&lt;P&gt;BTW, I'm documenting my work in a &lt;A href="https://docs.google.com/document/d/1inOUM8kZq8cTjNm6jZ9q_0H7m9rYnNKtWBqP6BEwgPk/edit?hl=en_GB" target="_blank"&gt;publicly editable Google Docs document&lt;/A&gt; as an experiment.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Jul 2011 21:42:12 GMT</pubDate>
    <dc:creator>ShaharOr</dc:creator>
    <dc:date>2011-07-11T21:42:12Z</dc:date>
    <item>
      <title>Where to start?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-to-start/m-p/161968#M3583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear developers,&lt;/P&gt;&lt;P&gt;I have taken on the task of porting CyanogenMod for a device which is based on i.MX515 and is called the &lt;A href="http://www.synrgic.com/index.php?option=com_content&amp;amp;view=article&amp;amp;id=95&amp;amp;Itemid=192&amp;amp;lang=en" target="_blank"&gt;Dreambook W7&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Where do I start? How do I flash a custom image for this thing? Which docs should I read?&lt;/P&gt;&lt;P&gt;Is there a prebuilt kernel? A whole android build? I'd love to know all these things and I bet they are documented somewhere.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Shahar&lt;/P&gt;&lt;P&gt;BTW, I'm documenting my work in a &lt;A href="https://docs.google.com/document/d/1inOUM8kZq8cTjNm6jZ9q_0H7m9rYnNKtWBqP6BEwgPk/edit?hl=en_GB" target="_blank"&gt;publicly editable Google Docs document&lt;/A&gt; as an experiment.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jul 2011 21:42:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-to-start/m-p/161968#M3583</guid>
      <dc:creator>ShaharOr</dc:creator>
      <dc:date>2011-07-11T21:42:12Z</dc:date>
    </item>
    <item>
      <title>Re: Where to start?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-to-start/m-p/161969#M3584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don´t know Dreambook W7 "personaly", but I believe you can handle this like any other imx51 like board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think a good start point may be:&amp;nbsp;&lt;A href="http://www.imxdev.org/wiki/index.php?title=Main_Page"&gt;http://www.imxdev.org/wiki/index.php?title=Main_Page&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is a "getting started" page. And please, feel free to fix and add anything.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can also contact CyanogenMod and Dreambook community.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does your board have sdcard connector? Does your board have serial port?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2011 16:12:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-to-start/m-p/161969#M3584</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2011-07-12T16:12:59Z</dc:date>
    </item>
    <item>
      <title>Re: Where to start?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-to-start/m-p/161970#M3585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Daiane!&lt;/P&gt;&lt;P&gt;I will read on in the wiki.&lt;/P&gt;&lt;P&gt;I will keep in touch with the CyanogenMod community. After all, my contribution will hopefully end up in CyanogenMod source code.&lt;/P&gt;&lt;P&gt;It does have an sdcard slot. There is no serial port on the outside of the product. I opened it up and I don't see a serial port connector on the board but I only looked at one side.&lt;/P&gt;&lt;P&gt;In the &lt;A href="http://www.imxdev.org/wiki/index.php?title=Getting_Started" target="_blank"&gt;getting started page&lt;/A&gt; the i.MX515 isn't listed. Am I right?&lt;/P&gt;&lt;P&gt;Thanks again,&lt;/P&gt;&lt;P&gt;Shahar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2011 16:37:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-to-start/m-p/161970#M3585</guid>
      <dc:creator>ShaharOr</dc:creator>
      <dc:date>2011-07-12T16:37:37Z</dc:date>
    </item>
    <item>
      <title>Re: Where to start?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-to-start/m-p/161971#M3586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I guess that the first step that I should take is to ensure that whatever I'd do to the software on the device - I will always have a way back. This is not a problem with development boards, since they have dip switches which enable boot from sdcard, for example. This device - I'm not sure it does because it is a production model and I would prefer not to open the case if it is not necessary.&lt;/P&gt;&lt;P&gt;So my question is: Does this device, which is most probably booting with u-boot, have some sort of "boot to bootloader" feature that I can use to boot from sdcard or better yet: I've read that u-boot is compatible with the fastboot protocol. This would allow me to flash new images (as long as I keep the same partition layout?) easily.&lt;/P&gt;&lt;P&gt;Is there a way to reach that u-boot state which allows using fastboot?&lt;/P&gt;&lt;P&gt;In other android devices I could just do 'adb reboot bootloader'.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jul 2011 10:34:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-to-start/m-p/161971#M3586</guid>
      <dc:creator>ShaharOr</dc:creator>
      <dc:date>2011-07-13T10:34:51Z</dc:date>
    </item>
    <item>
      <title>Re: Where to start?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Where-to-start/m-p/161972#M3587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well. I don´t know your board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think you should care about some questions:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;* How do you turn your board on?&lt;/P&gt;&lt;P&gt;* How can you access some "prompt"?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you don´t have any serial port, maybe you have some USB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any user manual for your board?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Look, uboot has fastboot support depending on version (or binary, you can disable it on ./configure)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jul 2011 11:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Where-to-start/m-p/161972#M3587</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2011-07-13T11:40:58Z</dc:date>
    </item>
  </channel>
</rss>