<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックBoot SSD</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-SSD/m-p/292541#M35826</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have just received a Sabre Lite board and trying to boot from the SSD drive (SATA connection).&lt;/P&gt;&lt;P&gt;I managed to mount the SSD drive when running a LTIB image, when booting up from the SD card (use the image provided from (&lt;A href="http://boundarydevices.com/ltib-4-0-0-images/" title="http://boundarydevices.com/ltib-4-0-0-images/"&gt;http://boundarydevices.com/ltib-4-0-0-images/&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I formatted the SSD in ext3 format (in Ubunut).&lt;/P&gt;&lt;P&gt;mkfs.ext3 -L ltib /dev/sdb&lt;/P&gt;&lt;P&gt;after that I mounted the disk and got /media/ltib&lt;/P&gt;&lt;P&gt;Then I unpacked the LTIB image into the SSD drive:&lt;/P&gt;&lt;P&gt;sudo tar zxvf ltib4-no-x-20130618.tar -C /media/ltib/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I boot up my SABRE Lite card (without the SD card) it seems like it is trying to boot from the SSD, but I get following messages:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SATA Device Info:&lt;/P&gt;&lt;P&gt;S/N: FF180738082600047077&lt;/P&gt;&lt;P&gt;Product model number: BP4 mSATA SSD&lt;/P&gt;&lt;P&gt;Firmware version: S8FM06.1&lt;/P&gt;&lt;P&gt;Capacity: 62533296 sectors&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SATA device 0: Model: BP4 mSATA SSD Firm: S8FM06.1 Ser#: FF180738082600047077&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Type: Hard Disk&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Supports 48-bit addressing&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Capacity: 30533.8 MB = 29.8 GB (62533296 x 512)&lt;/P&gt;&lt;P&gt;... is now current device&lt;/P&gt;&lt;P&gt;** No partition table - sata 0 **&lt;/P&gt;&lt;P&gt;** No partition table - sata 0 **&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seem like it doesn't like the partitioning on the SSD.&lt;/P&gt;&lt;P&gt;Do I need to create the bootable image on the SSD drive in a different way?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Sep 2013 22:00:15 GMT</pubDate>
    <dc:creator>niklasmolin</dc:creator>
    <dc:date>2013-09-05T22:00:15Z</dc:date>
    <item>
      <title>Boot SSD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-SSD/m-p/292541#M35826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have just received a Sabre Lite board and trying to boot from the SSD drive (SATA connection).&lt;/P&gt;&lt;P&gt;I managed to mount the SSD drive when running a LTIB image, when booting up from the SD card (use the image provided from (&lt;A href="http://boundarydevices.com/ltib-4-0-0-images/" title="http://boundarydevices.com/ltib-4-0-0-images/"&gt;http://boundarydevices.com/ltib-4-0-0-images/&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I formatted the SSD in ext3 format (in Ubunut).&lt;/P&gt;&lt;P&gt;mkfs.ext3 -L ltib /dev/sdb&lt;/P&gt;&lt;P&gt;after that I mounted the disk and got /media/ltib&lt;/P&gt;&lt;P&gt;Then I unpacked the LTIB image into the SSD drive:&lt;/P&gt;&lt;P&gt;sudo tar zxvf ltib4-no-x-20130618.tar -C /media/ltib/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I boot up my SABRE Lite card (without the SD card) it seems like it is trying to boot from the SSD, but I get following messages:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SATA Device Info:&lt;/P&gt;&lt;P&gt;S/N: FF180738082600047077&lt;/P&gt;&lt;P&gt;Product model number: BP4 mSATA SSD&lt;/P&gt;&lt;P&gt;Firmware version: S8FM06.1&lt;/P&gt;&lt;P&gt;Capacity: 62533296 sectors&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SATA device 0: Model: BP4 mSATA SSD Firm: S8FM06.1 Ser#: FF180738082600047077&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Type: Hard Disk&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Supports 48-bit addressing&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Capacity: 30533.8 MB = 29.8 GB (62533296 x 512)&lt;/P&gt;&lt;P&gt;... is now current device&lt;/P&gt;&lt;P&gt;** No partition table - sata 0 **&lt;/P&gt;&lt;P&gt;** No partition table - sata 0 **&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seem like it doesn't like the partitioning on the SSD.&lt;/P&gt;&lt;P&gt;Do I need to create the bootable image on the SSD drive in a different way?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2013 22:00:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-SSD/m-p/292541#M35826</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2013-09-05T22:00:15Z</dc:date>
    </item>
    <item>
      <title>Re: Boot SSD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-SSD/m-p/292542#M35827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found the problem.&lt;/P&gt;&lt;P&gt;I didn't do a sfdisk to create partitioning when I formatted the SSD drive.&lt;/P&gt;&lt;P&gt;Now I can boot direct from the SSD drive.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2013 22:31:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-SSD/m-p/292542#M35827</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2013-09-05T22:31:52Z</dc:date>
    </item>
  </channel>
</rss>