<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic u-boot support Camera/tv in display in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-support-Camera-tv-in-display/m-p/292115#M35651</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now in my project ,we have to do camera/tv in display in u-boot.&lt;/P&gt;&lt;P&gt;because I tried implement 'linux fast boot',it disable so many module ,maybe no sutiable our application.&lt;/P&gt;&lt;P&gt;Is there anyone have any solution or idea? thx!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Jun 2013 06:25:42 GMT</pubDate>
    <dc:creator>zhanxiaozhang</dc:creator>
    <dc:date>2013-06-14T06:25:42Z</dc:date>
    <item>
      <title>u-boot support Camera/tv in display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-support-Camera-tv-in-display/m-p/292115#M35651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now in my project ,we have to do camera/tv in display in u-boot.&lt;/P&gt;&lt;P&gt;because I tried implement 'linux fast boot',it disable so many module ,maybe no sutiable our application.&lt;/P&gt;&lt;P&gt;Is there anyone have any solution or idea? thx!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2013 06:25:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-support-Camera-tv-in-display/m-p/292115#M35651</guid>
      <dc:creator>zhanxiaozhang</dc:creator>
      <dc:date>2013-06-14T06:25:42Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot support Camera/tv in display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-support-Camera-tv-in-display/m-p/292116#M35652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We don't have the uboot use case, but you can reference to the followee link: it is a small linux kernel mode to do the fast camera solution.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-93619"&gt;https://community.freescale.com/docs/DOC-93619&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Test result of fast boot on Sabresd board for MIPI camera overly on LVDS screen: &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The main application be executed from the board be powered up is about 958ms.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2013 03:40:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-support-Camera-tv-in-display/m-p/292116#M35652</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2013-08-26T03:40:59Z</dc:date>
    </item>
  </channel>
</rss>