<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 fsl-mm-codecs source availability</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/fsl-mm-codecs-source-availability/m-p/291960#M35569</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is the source code for the fsl-mm-codecs available for the iMX53?&lt;/P&gt;&lt;P&gt;I have a customer that would to recompile the libraries with with the hard float option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this source code Freescale's, or was it provided by the IP vendor?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Mar 2013 15:59:39 GMT</pubDate>
    <dc:creator>bonzo</dc:creator>
    <dc:date>2013-03-12T15:59:39Z</dc:date>
    <item>
      <title>fsl-mm-codecs source availability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fsl-mm-codecs-source-availability/m-p/291960#M35569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is the source code for the fsl-mm-codecs available for the iMX53?&lt;/P&gt;&lt;P&gt;I have a customer that would to recompile the libraries with with the hard float option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this source code Freescale's, or was it provided by the IP vendor?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2013 15:59:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fsl-mm-codecs-source-availability/m-p/291960#M35569</guid>
      <dc:creator>bonzo</dc:creator>
      <dc:date>2013-03-12T15:59:39Z</dc:date>
    </item>
    <item>
      <title>Re: fsl-mm-codecs source availability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fsl-mm-codecs-source-availability/m-p/291961#M35570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, the source code is not available, if your customer wants to recompile, he would need to check with each IP vendor of each codec.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2013 16:28:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fsl-mm-codecs-source-availability/m-p/291961#M35570</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2013-03-14T16:28:33Z</dc:date>
    </item>
    <item>
      <title>Re: fsl-mm-codecs source availability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fsl-mm-codecs-source-availability/m-p/291962#M35571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there anyway we could have this library recompiled with hard float?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Mar 2013 22:14:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fsl-mm-codecs-source-availability/m-p/291962#M35571</guid>
      <dc:creator>bonzo</dc:creator>
      <dc:date>2013-03-15T22:14:41Z</dc:date>
    </item>
  </channel>
</rss>