<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: tvp5158 interleaved mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/tvp5158-interleaved-mode/m-p/291708#M35474</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The CSI&amp;nbsp; support inteleave mode, we have tired to connect two camera with one CSI before,&amp;nbsp; but IPU has two CSI, should meet your requiement, you could refer to the reference manual about the detail.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jun 2013 04:39:30 GMT</pubDate>
    <dc:creator>jack_mao</dc:creator>
    <dc:date>2013-06-24T04:39:30Z</dc:date>
    <item>
      <title>tvp5158 interleaved mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/tvp5158-interleaved-mode/m-p/291707#M35473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ww would like to acquire 4 video channel (pal or ntsc) using TVP5158 in pixel or line interleaved mode so we can have all 4 channels time sharing the same parallel video port (8 or 16 bit).&lt;/P&gt;&lt;P&gt;is it possible to acquire it using the parallel CSI of imx6Q? I mean the CSi can handle such kind of interleaving? and produce 4 different virtual channels (as the mipi seeem to do)??&lt;/P&gt;&lt;P&gt;any suggestion or&amp;nbsp; question?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Omar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2013 08:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/tvp5158-interleaved-mode/m-p/291707#M35473</guid>
      <dc:creator>Selea</dc:creator>
      <dc:date>2013-06-14T08:20:32Z</dc:date>
    </item>
    <item>
      <title>Re: tvp5158 interleaved mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/tvp5158-interleaved-mode/m-p/291708#M35474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The CSI&amp;nbsp; support inteleave mode, we have tired to connect two camera with one CSI before,&amp;nbsp; but IPU has two CSI, should meet your requiement, you could refer to the reference manual about the detail.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jun 2013 04:39:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/tvp5158-interleaved-mode/m-p/291708#M35474</guid>
      <dc:creator>jack_mao</dc:creator>
      <dc:date>2013-06-24T04:39:30Z</dc:date>
    </item>
  </channel>
</rss>