<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 file system</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/file-system/m-p/291482#M35406</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,All,&lt;/P&gt;&lt;P&gt;I build mini profile enviroment in custom board. The problem is that I can not login into system. I have try to use rootfs.tar.bz in MFG, it does not work.&lt;/P&gt;&lt;P&gt;But if I use ubuntu demo file system, it works well.&lt;/P&gt;&lt;P&gt;I think the problem is script about rc.conf or rcS,but I don't know how to modify it.If someone can give me a hint,that will be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The syslog shows below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EXT3-fs: barriers not enabled&lt;/P&gt;&lt;P&gt;24bit read error, ret = -5&lt;/P&gt;&lt;P&gt;24bit write error, ret = -5&lt;/P&gt;&lt;P&gt;kjournald starting.&amp;nbsp; Commit interval 5 seconds&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): using internal journal&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): recovery complete&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): mounted filesystem with writeback data mode&lt;/P&gt;&lt;P&gt;VFS: Mounted root (ext3 filesystem) on device 179:1.&lt;/P&gt;&lt;P&gt;Freeing init memory: 140K&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;starting pid 1171, tty '': '/etc/rc.d/rcS'&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Mounting /proc and /sys &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Starting the hotplug events dispatcher udevd&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Synthesizing initial hotplug events&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Setting the hostname to freescale&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Mounting filesystems&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;mount: mounting usbfs on /proc/bus/usb failed: No such file or directory&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;starting pid 2139, tty '': '-/sbin/getty -L ttymxc0 115200 vt100'&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;arm-none-linux-gnueabi-gcc (4.4.4_09.06.2010) 4.4.4&lt;/P&gt;&lt;P&gt;root filesystem built on Wed, 12 Jun 2013 19:18:43 +0800&lt;/P&gt;&lt;P&gt;Freescale Semiconductor, Inc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;freescale login: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reagrds,&lt;/P&gt;&lt;P&gt;Haifeng&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Jun 2013 01:31:47 GMT</pubDate>
    <dc:creator>caohaifeng</dc:creator>
    <dc:date>2013-06-14T01:31:47Z</dc:date>
    <item>
      <title>file system</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/file-system/m-p/291482#M35406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,All,&lt;/P&gt;&lt;P&gt;I build mini profile enviroment in custom board. The problem is that I can not login into system. I have try to use rootfs.tar.bz in MFG, it does not work.&lt;/P&gt;&lt;P&gt;But if I use ubuntu demo file system, it works well.&lt;/P&gt;&lt;P&gt;I think the problem is script about rc.conf or rcS,but I don't know how to modify it.If someone can give me a hint,that will be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The syslog shows below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EXT3-fs: barriers not enabled&lt;/P&gt;&lt;P&gt;24bit read error, ret = -5&lt;/P&gt;&lt;P&gt;24bit write error, ret = -5&lt;/P&gt;&lt;P&gt;kjournald starting.&amp;nbsp; Commit interval 5 seconds&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): using internal journal&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): recovery complete&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p1): mounted filesystem with writeback data mode&lt;/P&gt;&lt;P&gt;VFS: Mounted root (ext3 filesystem) on device 179:1.&lt;/P&gt;&lt;P&gt;Freeing init memory: 140K&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;starting pid 1171, tty '': '/etc/rc.d/rcS'&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Mounting /proc and /sys &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Starting the hotplug events dispatcher udevd&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Synthesizing initial hotplug events&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Setting the hostname to freescale&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Mounting filesystems&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;mount: mounting usbfs on /proc/bus/usb failed: No such file or directory&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;starting pid 2139, tty '': '-/sbin/getty -L ttymxc0 115200 vt100'&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;arm-none-linux-gnueabi-gcc (4.4.4_09.06.2010) 4.4.4&lt;/P&gt;&lt;P&gt;root filesystem built on Wed, 12 Jun 2013 19:18:43 +0800&lt;/P&gt;&lt;P&gt;Freescale Semiconductor, Inc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;freescale login: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reagrds,&lt;/P&gt;&lt;P&gt;Haifeng&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2013 01:31:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/file-system/m-p/291482#M35406</guid>
      <dc:creator>caohaifeng</dc:creator>
      <dc:date>2013-06-14T01:31:47Z</dc:date>
    </item>
    <item>
      <title>Re: file system</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/file-system/m-p/291483#M35407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the error on the MFG? BTW, the rootfs expected by MFG should end with bz2, not bz. Make sure the MFG's configuration matches the file you are placing on under the Profile folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2013 15:33:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/file-system/m-p/291483#M35407</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-06-14T15:33:54Z</dc:date>
    </item>
    <item>
      <title>Re: file system</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/file-system/m-p/291484#M35408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi,Leonardo,&lt;/P&gt;&lt;P&gt;I used rootfs.tar.bz2 built in the MFG.The u-boot.bin and uImage&amp;nbsp; are generated by ltib.&lt;/P&gt;&lt;P&gt;There is no error at the stage of downloading files. I can't login into file system when I input "root" in prompt &lt;STRONG&gt;&lt;EM&gt;freescale login&lt;/EM&gt;&lt;/STRONG&gt;:&lt;/P&gt;&lt;P&gt;as the same as I download these files by command &lt;EM&gt;&lt;STRONG&gt;dd&lt;/STRONG&gt;&lt;/EM&gt;. If I deselected the []boot up with a tty and login under ltib top menu,&lt;/P&gt;&lt;P&gt;the prompt shows that the currect user is root,but there is response yet if I input command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think the error caused by script. &lt;SPAN data-aligning="#src_2_1,#tran_2_0"&gt;How do&lt;/SPAN&gt; &lt;SPAN data-aligning="#src_2_0,#tran_2_1"&gt;you&lt;/SPAN&gt; &lt;SPAN data-aligning="#src_2_2,#tran_2_2"&gt;think&lt;/SPAN&gt; &lt;SPAN data-aligning="#src_2_3,#tran_2_3"&gt;of&lt;/SPAN&gt; this question?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Haifeng&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2013 01:09:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/file-system/m-p/291484#M35408</guid>
      <dc:creator>caohaifeng</dc:creator>
      <dc:date>2013-06-17T01:09:49Z</dc:date>
    </item>
  </channel>
</rss>