<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: JTAG Debugging On SabreLite/Nitrogen6X</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/JTAG-Debugging-On-SabreLite-Nitrogen6X/m-p/161780#M3531</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been using the Arium LC500S with the Sabrelite board and performed source level debugging.&lt;/P&gt;&lt;P&gt;Arium also has an adapter to go from the standard 20pin cable to the 10pin header on the Sabrelite board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Brett&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Nov 2012 19:27:42 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2012-11-01T19:27:42Z</dc:date>
    <item>
      <title>JTAG Debugging On SabreLite/Nitrogen6X</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/JTAG-Debugging-On-SabreLite-Nitrogen6X/m-p/161779#M3530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What JTAG interface and debug tools are being used successfully with IMX6Q on SabreLite or Nitrogen6X devel boards?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will be writing a custom U-Boot BSP and would like to have source-level debugging capability.&amp;nbsp; I tried a Segger J-Link with Segger 20-pin to 9-pin adapter and the latest version of Segger's GDB Server, but GDB does not seem to connect reliably with the IMX6Q on Nitrogen6X.&amp;nbsp; I also tried Segger's J-Link Commander as a test and I see the following in the GDB Server's log:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;Waiting for J-Link connection...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;J-Link is connected.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;Firmware: J-Link ARM V8 compiled Sep 20 2012 13:27:01&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;Hardware: V8.00&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;S/N: 58005844&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;Checking target voltage...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;Listening on TCP/IP port 2331&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;Connecting to target...WARNING: At least one of the connected devices is not JTAG compliant (IEEE Std 1149.1, 7.1.1.d, IR-cells). (NumDevices = 3, NumBitsSet = 2)&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;WARNING: Could not power-up system power domain&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Nov 2012 16:28:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/JTAG-Debugging-On-SabreLite-Nitrogen6X/m-p/161779#M3530</guid>
      <dc:creator>mlu</dc:creator>
      <dc:date>2012-11-01T16:28:31Z</dc:date>
    </item>
    <item>
      <title>Re: JTAG Debugging On SabreLite/Nitrogen6X</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/JTAG-Debugging-On-SabreLite-Nitrogen6X/m-p/161780#M3531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been using the Arium LC500S with the Sabrelite board and performed source level debugging.&lt;/P&gt;&lt;P&gt;Arium also has an adapter to go from the standard 20pin cable to the 10pin header on the Sabrelite board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Brett&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Nov 2012 19:27:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/JTAG-Debugging-On-SabreLite-Nitrogen6X/m-p/161780#M3531</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2012-11-01T19:27:42Z</dc:date>
    </item>
  </channel>
</rss>