<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Accessing fb1 on i.mx6 using QT5 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-fb1-on-i-mx6-using-QT5/m-p/290718#M35207</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the i.mx6, fb0 can be used as the background and fb1 can be used as a foreground. I currently have video playing on fb0 using video4linux and want to overlay some controls on fb1 using QT5 and EGLFS. However, I cannot get QT5 to use fb1. I dug down into the QPA for EGLFS and found it hard coded to use /dev/fb0. However, when I changed it to /dev/fb1 QT still used /dev/fb0. I even tried changing the hard coded value to /dev/fb10 which resulted in an error message and QT proceeded to use /dev/fb0 anyway. If I force my video4linux app to use fb1(in a reduced window size) and then run my QT app I can see both on the screen. However, I need the video to be full screen with the controls over layed. Can this be done with QT?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Jun 2013 15:17:36 GMT</pubDate>
    <dc:creator>davidmondou</dc:creator>
    <dc:date>2013-06-13T15:17:36Z</dc:date>
    <item>
      <title>Accessing fb1 on i.mx6 using QT5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-fb1-on-i-mx6-using-QT5/m-p/290718#M35207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the i.mx6, fb0 can be used as the background and fb1 can be used as a foreground. I currently have video playing on fb0 using video4linux and want to overlay some controls on fb1 using QT5 and EGLFS. However, I cannot get QT5 to use fb1. I dug down into the QPA for EGLFS and found it hard coded to use /dev/fb0. However, when I changed it to /dev/fb1 QT still used /dev/fb0. I even tried changing the hard coded value to /dev/fb10 which resulted in an error message and QT proceeded to use /dev/fb0 anyway. If I force my video4linux app to use fb1(in a reduced window size) and then run my QT app I can see both on the screen. However, I need the video to be full screen with the controls over layed. Can this be done with QT?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2013 15:17:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-fb1-on-i-mx6-using-QT5/m-p/290718#M35207</guid>
      <dc:creator>davidmondou</dc:creator>
      <dc:date>2013-06-13T15:17:36Z</dc:date>
    </item>
    <item>
      <title>Re: Accessing fb1 on i.mx6 using QT5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Accessing-fb1-on-i-mx6-using-QT5/m-p/290719#M35208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is more QT specific. Please post your question in QT developer forum.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Sep 2013 19:06:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Accessing-fb1-on-i-mx6-using-QT5/m-p/290719#M35208</guid>
      <dc:creator>PrabhuSundarara</dc:creator>
      <dc:date>2013-09-06T19:06:31Z</dc:date>
    </item>
  </channel>
</rss>