<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: android booting problem with binder issue on imx6 sabrelite</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290692#M35194</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sasidhar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using the .img file should configure the filesystem properly, and will include our boot script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The log you uploaded seems to cut off the end of some long lines, so I can't see the entire kernel command line:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt; Kernel command line: enable_wait_mode=off console=ttymxc1,115200 vmalloc=400M consoleblank=0 video=mxcfb0:dev=hdmi,bpp=32,1280x720M@60,if=RGB24 3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This does appear to be generated using the stock boot script though:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="https://github.com/boundarydevices/android_device_boundary/blob/boundary-imx_jb4.3_1.0.0-beta/nitrogen6x/6x_bootscript_jb.txt" title="https://github.com/boundarydevices/android_device_boundary/blob/boundary-imx_jb4.3_1.0.0-beta/nitrogen6x/6x_bootscript_jb.txt"&gt;android_device_boundary/nitrogen6x/6x_bootscript_jb.txt at boundary-imx_jb4.3_1.0.0-beta · boundarydevices/android_devic…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you put the SD card in your PC, do you see all of the partitions? Does your system auto-mount /system?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, can you run "mount" from the shell when trying to boot Android?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I'm getting at here is that the problem is most likely the SD card image, and specifically the /system partition (P5).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see it mount though:&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt; EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: (null)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally, can you run this command and capture the output for a minute or so?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # logcat V:* &amp;amp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This will produce a lot of output, and will likely repeat as Android attempts to re-start, but 60 seconds or so should give an idea of what is crashing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Jan 2014 14:44:17 GMT</pubDate>
    <dc:creator>EricNelson</dc:creator>
    <dc:date>2014-01-08T14:44:17Z</dc:date>
    <item>
      <title>android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290689#M35191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am trying to boot android jelly bean on imx6 sabrelite board but the problem is can not able to get desktop environment. Its struck over android splash screen and below is the error displayed. Please help me how to fix this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;warning: `zygote' uses 32-bit capabilities (legacy support in use)&lt;/P&gt;&lt;P&gt;request_suspend_state: wakeup (3-&amp;gt;0) at 20573687338 (2014-01-07 13:14:31.619795003 UTC)&lt;/P&gt;&lt;P&gt;eth0: Freescale FEC PHY driver [Micrel KSZ9021 Gigabit PHY] (mii_bus:phy_addr=1:06, irq=284)&lt;/P&gt;&lt;P&gt;ADDRCONF(NETDEV_UP): eth0: link is not ready&lt;/P&gt;&lt;P&gt;acc_open&lt;/P&gt;&lt;P&gt;acc_release&lt;/P&gt;&lt;P&gt;PHY: 1:06 - Link is Up - 100/Full&lt;/P&gt;&lt;P&gt;ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready&lt;/P&gt;&lt;P&gt;binder: release 2680:2692 transaction 5952 in, still active&lt;/P&gt;&lt;P&gt;binder: send failed reply for transaction 5952 to 2782:2782&lt;/P&gt;&lt;P&gt;binder: release 2680:2914 transaction 5955 in, still active&lt;/P&gt;&lt;P&gt;binder: send failed reply for transaction 5955 to 2809:2863&lt;/P&gt;&lt;P&gt;binder: release 2680:3013 transaction 5904 out, still active&lt;/P&gt;&lt;P&gt;binder: send failed reply for transaction 6012 to 2998:2998&lt;/P&gt;&lt;P&gt;binder: send failed reply for transaction 6023 to 2915:2962&lt;/P&gt;&lt;P&gt;binder: 2915:2962 transaction failed 29189, size 240-0&lt;/P&gt;&lt;P&gt;binder: 2998:2998 transaction failed 29189, size 2788-4&lt;/P&gt;&lt;P&gt;request_suspend_state: wakeup (0-&amp;gt;0) at 30898374005 (2014-01-07 13:14:41.944479003 UTC)&lt;/P&gt;&lt;P&gt;alarm_release: clear alarm, pending 0&lt;/P&gt;&lt;P&gt;binder: release 2884:2972 transaction 4582 out, still active&lt;/P&gt;&lt;P&gt;alarm_release: clear alarm, pending 0&lt;/P&gt;&lt;P&gt;init: untracked pid 2400 exited&lt;/P&gt;&lt;P&gt;binder: release 2405:2405 transaction 5904 in, still active&lt;/P&gt;&lt;P&gt;binder: send failed reply for transaction 5904, target dead&lt;/P&gt;&lt;P&gt;binder: release 2782:2943 transaction 4617 out, still active&lt;/P&gt;&lt;P&gt;init: untracked pid 2927 exited&lt;/P&gt;&lt;P&gt;init: untracked pid 2884 exited&lt;/P&gt;&lt;P&gt;init: untracked pid 3017 exited&lt;/P&gt;&lt;P&gt;init: untracked pid 2782 exited&lt;/P&gt;&lt;P&gt;init: untracked pid 2809 exited&lt;/P&gt;&lt;P&gt;init: untracked pid 2864 exited&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;binder: release 2946:2958 transaction 4582 in, still active&lt;/P&gt;&lt;P&gt;binder: send failed reply for transaction 4582, target dead&lt;/P&gt;&lt;P&gt;binder: release 2946:2977 transaction 4617 in, still active&lt;/P&gt;&lt;P&gt;binder: send failed reply for transaction 4617, target dead&lt;/P&gt;&lt;P&gt;init: untracked pid 2946 exited&lt;/P&gt;&lt;P&gt;init: untracked pid 2915 exited&lt;/P&gt;&lt;P&gt;init: untracked pid 2680 exited&lt;/P&gt;&lt;P&gt;request_suspend_state: wakeup (0-&amp;gt;0) at 35482847340 (2014-01-07 13:14:46.528955005 UTC)&lt;/P&gt;&lt;P&gt;init: untracked pid 3015 exited&lt;/P&gt;&lt;P&gt;acc_open&lt;/P&gt;&lt;P&gt;acc_release&lt;/P&gt;&lt;P&gt;init: untracked pid 2405 exited&lt;/P&gt;&lt;P&gt;binder: release 3358:3507 transaction 9596 out, still active&lt;/P&gt;&lt;P&gt;binder: release 3517:3531 transaction 9596 in, still active&lt;/P&gt;&lt;P&gt;binder: send failed reply for transaction 9596, target dead&lt;/P&gt;&lt;P&gt;binder: release 3517:3555 transaction 9752 in, still active&lt;/P&gt;&lt;P&gt;binder: send failed reply for transaction 9752 to 3455:3547&lt;/P&gt;&lt;P&gt;binder: release 3258:3269 transaction 10337 in, still active&lt;/P&gt;&lt;P&gt;binder: send failed reply for transaction 10337 to 3481:3481&lt;/P&gt;&lt;P&gt;binder: 3481:3481 transaction failed 29189, size 208-0&lt;/P&gt;&lt;P&gt;binder: 3481:3481 transaction failed 29189, size 4324-4&lt;/P&gt;&lt;P&gt;alarm_release: clear alarm, pending 0&lt;/P&gt;&lt;P&gt;alarm_release: clear alarm, pending 0&lt;/P&gt;&lt;P&gt;request_suspend_state: wakeup (0-&amp;gt;0) at 43142007674 (2014-01-07 13:14:54.188115006 UTC)&lt;/P&gt;&lt;P&gt;init: untracked pid 3038 exited&lt;/P&gt;&lt;P&gt;init: untracked pid 3037 exited&lt;/P&gt;&lt;P&gt;init: untracked pid 3502 exited&lt;/P&gt;&lt;P&gt;init: untracked pid 3432 exited&lt;/P&gt;&lt;P&gt;init: untracked pid 3417 exited&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;sasidhar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jan 2014 13:46:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290689#M35191</guid>
      <dc:creator>sasidhars</dc:creator>
      <dc:date>2014-01-07T13:46:42Z</dc:date>
    </item>
    <item>
      <title>Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290690#M35192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sasidhar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This type of error normally occurs if the filesystems (esp system) didn't mount properly, and might indicate a problem when creating your SD card or SATA image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using our (Boundary Devices) Android?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We added code to allow booting to either SD card, so you'll need to ensure that a kernel command-line parameter points at your boot device.&lt;/P&gt;&lt;P&gt;See &lt;A href="http://boundarydevices.com/android-jellybean-on-i-mx6-with-no-disclaimers/#sata" title="http://boundarydevices.com/android-jellybean-on-i-mx6-with-no-disclaimers/#sata"&gt;http://boundarydevices.com/android-jellybean-on-i-mx6-with-no-disclaimers/#sata&lt;/A&gt; for details and this section of the boot script for an example:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="https://github.com/boundarydevices/android_device_boundary/blob/boundary-imx_jb4.3_1.0.0-ga/nitrogen6x/6x_bootscript_jb.txt#L104" title="https://github.com/boundarydevices/android_device_boundary/blob/boundary-imx_jb4.3_1.0.0-ga/nitrogen6x/6x_bootscript_jb.txt#L104"&gt;android_device_boundary/nitrogen6x/6x_bootscript_jb.txt at boundary-imx_jb4.3_1.0.0-ga · boundarydevices/android_device_…&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jan 2014 15:15:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290690#M35192</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-01-07T15:15:18Z</dc:date>
    </item>
    <item>
      <title>Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290691#M35193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for your suggestion. I am using imx6-jb-sdcard-20130628.img.gz downloaded from the link &lt;A href="http://boundarydevices.com/android-jellybean-on-i-mx6-with-no-disclaimers/#sata" title="http://boundarydevices.com/android-jellybean-on-i-mx6-with-no-disclaimers/#sata"&gt;http://boundarydevices.com/android-jellybean-on-i-mx6-with-no-disclaimers/#sata&lt;/A&gt; and i am flashing it onto the sdcard using the command zcat /home/sasi/android_jb/imx6-jb-sdcard-20130628.img.gz | sudo dd of=/dev/sdb. still i'm facing the same issue (binder issue). The android_log.txt file has been attached for your reference. Waiting for your valuable suggestions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Sasidhar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jan 2014 07:48:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290691#M35193</guid>
      <dc:creator>sasidhars</dc:creator>
      <dc:date>2014-01-08T07:48:12Z</dc:date>
    </item>
    <item>
      <title>Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290692#M35194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sasidhar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using the .img file should configure the filesystem properly, and will include our boot script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The log you uploaded seems to cut off the end of some long lines, so I can't see the entire kernel command line:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt; Kernel command line: enable_wait_mode=off console=ttymxc1,115200 vmalloc=400M consoleblank=0 video=mxcfb0:dev=hdmi,bpp=32,1280x720M@60,if=RGB24 3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This does appear to be generated using the stock boot script though:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="https://github.com/boundarydevices/android_device_boundary/blob/boundary-imx_jb4.3_1.0.0-beta/nitrogen6x/6x_bootscript_jb.txt" title="https://github.com/boundarydevices/android_device_boundary/blob/boundary-imx_jb4.3_1.0.0-beta/nitrogen6x/6x_bootscript_jb.txt"&gt;android_device_boundary/nitrogen6x/6x_bootscript_jb.txt at boundary-imx_jb4.3_1.0.0-beta · boundarydevices/android_devic…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you put the SD card in your PC, do you see all of the partitions? Does your system auto-mount /system?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, can you run "mount" from the shell when trying to boot Android?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I'm getting at here is that the problem is most likely the SD card image, and specifically the /system partition (P5).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see it mount though:&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt; EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: (null)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally, can you run this command and capture the output for a minute or so?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # logcat V:* &amp;amp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This will produce a lot of output, and will likely repeat as Android attempts to re-start, but 60 seconds or so should give an idea of what is crashing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jan 2014 14:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290692#M35194</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-01-08T14:44:17Z</dc:date>
    </item>
    <item>
      <title>Re: Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290693#M35195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for your suggestions, My system is auto-mount, when i put SD card in my PC i can able to see all the partitions. And even i can able to run &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;mount from the shell when Android is booting. when i run&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;#&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt; logcat V:* &amp;amp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Each time i reboot IMX6 sabrelite board, i am getting different errors like&lt;/P&gt;&lt;P&gt;&amp;gt; Process com.android.launcher (pid 4815) has died.&lt;/P&gt;&lt;P&gt;&amp;gt; W/ActivityManager( 3816): Process com.android.phone has crashed too many times: killing!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I searched for NFS boot i got this below link&lt;/P&gt;&lt;P&gt;&lt;A href="http://boundarydevices.com/android-r13-4-ga-for-i-mx6-in-stages-stage-1-booting-over-nfs/" title="http://boundarydevices.com/android-r13-4-ga-for-i-mx6-in-stages-stage-1-booting-over-nfs/"&gt;http://boundarydevices.com/android-r13-4-ga-for-i-mx6-in-stages-stage-1-booting-over-nfs/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;but it is mentioned as android_kernel boot but not entire rootfs. Is there any chance to boot android rootfs through NFS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;The logcat ouput file has been attached for your reference. Please help me out in this issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jan 2014 09:59:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290693#M35195</guid>
      <dc:creator>sasidhars</dc:creator>
      <dc:date>2014-01-09T09:59:49Z</dc:date>
    </item>
    <item>
      <title>Re: Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290694#M35196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you forget the attachment?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jan 2014 16:18:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290694#M35196</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-01-09T16:18:29Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290695#M35197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I had attached the document in the previous reply. I am attaching it again for your reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Sasidhar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jan 2014 06:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290695#M35197</guid>
      <dc:creator>sasidhars</dc:creator>
      <dc:date>2014-01-10T06:04:23Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290696#M35198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sasidhar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure why I didn't see the attachment previously. Perhaps there's a delay on the Community site while the scanner runs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you forward the output from "print" at the U-Boot prompt and "netcfg" from the Android shell?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm suspicious about this bit from the boot loader:&lt;/P&gt;&lt;PRE&gt;U-Boot 2013.04-00316-g1903727 (Jul 23 2013 - 11:01:29)

CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6Q rev1.2 at 792 MHz
Reset cause: POR
Board: SABRE Lite
DRAM:&amp;nbsp; 2 GiB
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We don't sell 2GiB versions of SABRE Lite.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you sure that you have a 2GiB board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you upload a photo?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jan 2014 15:07:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290696#M35198</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-01-10T15:07:28Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Re: Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290697#M35199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am using IMX6 sabrelite board with DDR 1GB only. And Below mentioned details are the output from "print" at the U-Boot prompt and "netcfg" from the Android shell. I had attached images of IMX6 Sabrelite board which i am using for your reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; print&lt;/P&gt;&lt;P&gt;baudrate=115200&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;bootcmd=for dtype in sata mmc ; do for disk in 0 1 ; do ${dtype} dev ${disk} ;for fs in fat ext2 ; do ${fs}load ${dtype} ${disk}:1 10008000 /6x_bootscript&amp;amp;&amp;amp; source 10008000 ; done ; done ; done; setenv stdout serial,vga ; echo ; echo 6x_bootscript not found ; echo ; echo serial console at 115200, 8N1 ; echo ; echo details at &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://boundarydevices.com/6q_bootscript"&gt;http://boundarydevices.com/6q_bootscript&lt;/A&gt;&lt;SPAN&gt; ; usb start; setenv stdin serial,usbkbd&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;bootdelay=1&lt;/P&gt;&lt;P&gt;clearenv=if sf probe || sf probe || sf probe 1 ; then sf erase 0xc0000 0x2000 &amp;amp;&amp;amp; echo restored environment to factory default ; fi&lt;/P&gt;&lt;P&gt;console=ttymxc1&lt;/P&gt;&lt;P&gt;ethact=FEC&lt;/P&gt;&lt;P&gt;ethaddr=00:19:b8:01:1d:41&lt;/P&gt;&lt;P&gt;ethprime=FEC&lt;/P&gt;&lt;P&gt;loadaddr=0x12000000&lt;/P&gt;&lt;P&gt;loadsplash=if sf probe ; then sf read ${splashimage} c2000 ${splashsize} ; fi&lt;/P&gt;&lt;P&gt;upgradeu=for dtype in sata mmc ; do for disk in 0 1 ; do ${dtype} dev ${disk} ;for fs in fat ext2 ; do ${fs}load ${dtype} ${disk}:1 10008000 /6x_upgrade &amp;amp;&amp;amp; source 10008000 ; done ; done ; done&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@android:/ # netcfg&lt;/P&gt;&lt;P&gt;lo&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UP&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 127.0.0.1/8&amp;nbsp;&amp;nbsp; 0x00000049 00:00:00:00:00:00&lt;/P&gt;&lt;P&gt;can0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DOWN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.0.0.0/0&amp;nbsp;&amp;nbsp; 0x00000080 00:00:00:00:00:00&lt;/P&gt;&lt;P&gt;eth0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UP&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 192.168.1.32/24&amp;nbsp; 0x00001043 00:19:b8:01:1d:41&lt;/P&gt;&lt;P&gt;tunl0&amp;nbsp;&amp;nbsp;&amp;nbsp; DOWN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.0.0.0/0&amp;nbsp;&amp;nbsp; 0x00000080 00:00:00:00:00:00&lt;/P&gt;&lt;P&gt;sit0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DOWN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.0.0.0/0&amp;nbsp;&amp;nbsp; 0x00000080 00:00:00:00:00:00&lt;/P&gt;&lt;P&gt;ip6tnl0&amp;nbsp; DOWN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.0.0.0/0&amp;nbsp;&amp;nbsp; 0x00000080 00:00:00:00:00:00&lt;/P&gt;&lt;P&gt;root@android:/ # init: untracked pid 2873 exited&lt;/P&gt;&lt;P&gt;request_suspend_state: wakeup (0-&amp;gt;0) at 73434213011 (2014-01-11 06:45:39.070027002 UTC)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Sasidhar.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jan 2014 07:46:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290697#M35199</guid>
      <dc:creator>sasidhars</dc:creator>
      <dc:date>2014-01-11T07:46:13Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Re: Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290698#M35200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sasidhar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This explains a lot. You're running software for a 2GiB board on a machine with only 1GiB of DDR.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Please use our latest U-Boot package from &lt;A href="http://boundarydevices.com/u-boot-2013-10-release/"&gt;http://boundarydevices.com/u-boot-2013-10-release/&lt;/A&gt; to re-program things using &lt;SPAN style="color: #000000; font-family: Consolas, 'Bitstream Vera Sans Mono', 'Courier New', Courier, monospace; font-size: 16px; background-color: #f8f8f8;"&gt;u-boot.nitrogen6q&lt;/SPAN&gt; to fix that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After fixing this, I suspect things will start working.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jan 2014 16:03:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290698#M35200</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-01-11T16:03:18Z</dc:date>
    </item>
    <item>
      <title>Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290699#M35201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for your suggestions, Now i can able to boot android. But the problem is adb is not detecting the imx6 sabrelite board. And the output of adb is as follows :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ adb devices&lt;/P&gt;&lt;P&gt;List of devices attached&lt;/P&gt;&lt;P&gt;0123456789ABCDEF offline&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I went through the link &lt;A _jive_internal="true" href="https://community.nxp.com/thread/256677"&gt;https://community.freescale.com/thread/256677&lt;/A&gt; and followed the steps&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;SPAN style="font-style: inherit; font-family: inherit;"&gt;&lt;STRONG&gt;For Linux PC：&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;ADB function&lt;UL style="font-style: inherit; font-family: inherit;"&gt;&lt;LI style="margin-top: 0.5ex; margin-bottom: 0.5ex; font-style: inherit; font-family: inherit; list-style-type: inherit;"&gt;Download the Android SDK.&lt;/LI&gt;&lt;LI&gt;Update the adb configuration to scan for freescale's pid:&lt;UL style="font-style: inherit; font-family: inherit;"&gt;&lt;LI style="margin-top: 0.5ex; margin-bottom: 0.5ex; font-style: inherit; font-family: inherit; list-style-type: inherit;"&gt;Run the SDK's tools to generate a configure file:&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-style: inherit; margin: 0 0 0 120px; font-family: inherit;"&gt;android-sdk-linux_86/tools/android update adb&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Modify the files:~/.android/adb_usb.ini, to add freescale vendor id:&lt;/LI&gt;&lt;/UL&gt;&lt;TABLE bgcolor="#CCCCCC" border="1" cellspacing="0" style="border: 0px; font-family: inherit; font-style: inherit;" width="418"&gt;&lt;TBODY style="font-style: inherit; font-family: inherit;"&gt;&lt;TR style="border: 0px; font-style: inherit; font-family: inherit;"&gt;&lt;TD style="border: 1px solid black; padding-right: 4px; padding-left: 4px; font-style: inherit; font-family: inherit;" width="100%"&gt;# ANDROID 3RD PARTY USB VENDOR ID LIST -- DO NOT EDIT.&lt;BR /&gt;# USE 'android update adb' TO GENERATE.&lt;BR /&gt;# 1 USB VENDOR ID PER LINE.&lt;BR /&gt;0x15a2&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Create a new udev rule file under the PC's /etc/udev/rules.d/ named: imx-android.rules. And fill in the following line into the file:&lt;/LI&gt;&lt;/UL&gt;&lt;TABLE bgcolor="#CCCCCC" border="1" cellspacing="0" style="border: 0px; margin-left: 80px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;TBODY style="font-style: inherit; font-family: inherit;"&gt;&lt;TR style="border: 0px; font-style: inherit; font-family: inherit;"&gt;&lt;TD style="border: 1px solid black; padding-right: 4px; padding-left: 4px; font-style: inherit; font-family: inherit;" width="100%"&gt;&lt;SPAN style="font-style: inherit; font-family: inherit;"&gt;SUBSYSTEM=="usb", SYSFS{idVendor}=="15a2", MODE="0666"&lt;/SPAN&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN style="font-style: inherit; font-family: inherit;"&gt;Change the new udev rule file's permission:&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-style: inherit; margin: 0 0 0 80px; font-family: inherit;"&gt;chmod a+r /etc/udev/rules.d/imx-android.rules&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN style="font-style: inherit; font-family: inherit;"&gt;Connect the Android Device&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="font-style: inherit; font-family: inherit;"&gt;Restart the adb server&lt;/SPAN&gt;&lt;UL style="font-style: inherit; font-family: inherit;"&gt;&lt;LI&gt;&lt;SPAN style="font-style: inherit; font-family: inherit;"&gt;a&lt;/SPAN&gt;db kill-server&lt;/LI&gt;&lt;LI&gt;adb start-server&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i followed the above steps but still iam facing the same issue, Please guide me to fix this issue&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Sasidhar.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2014 10:01:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290699#M35201</guid>
      <dc:creator>sasidhars</dc:creator>
      <dc:date>2014-01-22T10:01:25Z</dc:date>
    </item>
    <item>
      <title>Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290700#M35202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sasidhar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should see a prompt on your display to authorize your PC to run ADB. The "offline" message seems to indicate "unauthorized".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There's also a way to place a file in the /data partition, but I can't recall off-hand where the file is or where to get the data to place in the file.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2014 13:42:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290700#M35202</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-01-22T13:42:16Z</dc:date>
    </item>
    <item>
      <title>Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290701#M35203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I had enabled "USB DEBUGGING" in developer options. When i connect IMX6 board to PC i can see a prompt on display "usb Debugging connected", but still i am getting unauthorized output for adb in PC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;$ adb devices&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;List of devices attached&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;0123456789ABCDEF unauthorized&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Sasidhar.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2014 14:15:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290701#M35203</guid>
      <dc:creator>sasidhars</dc:creator>
      <dc:date>2014-01-22T14:15:45Z</dc:date>
    </item>
    <item>
      <title>Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290702#M35204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sasidhar,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have you tried running adb server as root? I typically use this command-line to start ADB on my PC:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ~/$ sudo `which adb` devices&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is mainly to save on edits to the files in /etc/udev/.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Jan 2014 01:01:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290702#M35204</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-01-25T01:01:29Z</dc:date>
    </item>
    <item>
      <title>Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290703#M35205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sasidhar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As an alternative to using the on-screen prompt for authorization, you can also place your public key into /data/misc/adb/adb_keys as described here:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A class="loading" href="http://stackoverflow.com/questions/15746917/adb-over-network-without-previous-usb-pairing"&gt;http://stackoverflow.com/questions/15746917/adb-over-network-without-previous-usb-pairing&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Essentially, on your PC:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ~/$ cat $HOME/.android/adbkey.pub&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then paste the key into /data/misc/adb/adb_keys on the Android machine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Jan 2014 01:25:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290703#M35205</guid>
      <dc:creator>EricNelson</dc:creator>
      <dc:date>2014-01-25T01:25:47Z</dc:date>
    </item>
    <item>
      <title>Re: android booting problem with binder issue on imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290704#M35206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got one issue regarding booting of android - 5.0.2 lollipop in sabresd-imx6q board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;init: cannot expand '$ro.product.manufacturer' while writing to '/sys/class/android_usb/android0/iManufac'&lt;/P&gt;&lt;P&gt;init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead&lt;/P&gt;&lt;P&gt;init: property 'ro.product.model' doesn't exist while expanding '$ro.product.model'&lt;/P&gt;&lt;P&gt;init: cannot expand '$ro.product.model' while writing to '/sys/class/android_usb/android0/iProduct'&lt;/P&gt;&lt;P&gt;android_usb: already disabled&lt;/P&gt;&lt;P&gt;read descriptors&lt;/P&gt;&lt;P&gt;read strings&lt;/P&gt;&lt;P&gt;mtp_bind_config&lt;/P&gt;&lt;P&gt;binder: 147:147 transaction failed 29189, size 0-0&lt;/P&gt;&lt;P&gt;binder: 147:147 transaction failed 29189, size 0-0&lt;/P&gt;&lt;P&gt;binder: 147:147 transaction failed 29189, size 0-0&lt;/P&gt;&lt;P&gt;binder: 147:147 transaction failed 29189, size 0-0&lt;/P&gt;&lt;P&gt;binder: 147:147 transaction failed 29189, size 0-0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This binder: 147:147 transaction failed 29189, size 0-0 message keep on occur in my serial terminal but in sabresd board dispaly i didn't get anything...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;help me to solve this one thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Nov 2015 12:14:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-booting-problem-with-binder-issue-on-imx6-sabrelite/m-p/290704#M35206</guid>
      <dc:creator>chandrasekharma</dc:creator>
      <dc:date>2015-11-27T12:14:14Z</dc:date>
    </item>
  </channel>
</rss>