<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Restrict Wi-Fi access in Android device</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Restrict-Wi-Fi-access-in-Android-device/m-p/290458#M35117</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to configure wi-fi of my android device so that it can connect only to predefined set of access points. Can I do it by checking the MAC address of access points? In android wi-fi manager the SSID and MAC id is used in many places. Can I compare MAC id of access point with my specified set of MAC ids here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please share your thoughts. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Apr 2013 06:52:34 GMT</pubDate>
    <dc:creator>Mats1z</dc:creator>
    <dc:date>2013-04-30T06:52:34Z</dc:date>
    <item>
      <title>Restrict Wi-Fi access in Android device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Restrict-Wi-Fi-access-in-Android-device/m-p/290458#M35117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to configure wi-fi of my android device so that it can connect only to predefined set of access points. Can I do it by checking the MAC address of access points? In android wi-fi manager the SSID and MAC id is used in many places. Can I compare MAC id of access point with my specified set of MAC ids here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please share your thoughts. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Apr 2013 06:52:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Restrict-Wi-Fi-access-in-Android-device/m-p/290458#M35117</guid>
      <dc:creator>Mats1z</dc:creator>
      <dc:date>2013-04-30T06:52:34Z</dc:date>
    </item>
    <item>
      <title>Re: Restrict Wi-Fi access in Android device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Restrict-Wi-Fi-access-in-Android-device/m-p/290459#M35118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Successfully completed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In wpa_supplicant.c , there is a file there is a function wpa_drv_associate() , compare macids here using os_memcmp() and perform assocaiation based on it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now my android device wifi can connect to only one macid :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 May 2013 13:10:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Restrict-Wi-Fi-access-in-Android-device/m-p/290459#M35118</guid>
      <dc:creator>Mats1z</dc:creator>
      <dc:date>2013-05-23T13:10:47Z</dc:date>
    </item>
  </channel>
</rss>