<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX25 SDIO</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289868#M34923</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;For the Q2, could you tell me more details ? what interrupt is called? which bit you expected to be 1 in IRQSTAT?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Dec 2013 06:49:46 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2013-12-24T06:49:46Z</dc:date>
    <item>
      <title>i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289862#M34917</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am developing the SDIO driver of i.MX257.&lt;BR /&gt;It is using eSDHC2.&lt;/P&gt;&lt;P&gt;There are two questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 1:&lt;BR /&gt;Teach the way of controlling the clock of the SD bus by the SDCLKEN bit of SystemControlRegister.&lt;BR /&gt;To want to be realized is to make the inside of the 1 bit mode stop the clock of the SD bus and to accept SDIO interruption.&lt;BR /&gt;It sets PEREN, HCKEN, IPGEN of SystemControlRegister to 1.&lt;BR /&gt;SION of the following register is set.&lt;BR /&gt;・IOMUXC_SW_MUX_CTL_PAD_SD1_CMD&lt;BR /&gt;・IOMUXC_SW_MUX_CTL_PAD_SD1_CLK&lt;BR /&gt;・IOMUXC_SW_MUX_CTL_PAD_CSI_D6&lt;BR /&gt;・IOMUXC_SW_MUX_CTL_PAD_CSI_D7&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 2:&lt;BR /&gt;It sometimes becomes 0x00000000 when reading InterruptStatusRegister by the SD interruption handler.&lt;BR /&gt;What is thought of ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Nov 2013 09:29:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289862#M34917</guid>
      <dc:creator>KatsumiKaneko</dc:creator>
      <dc:date>2013-11-20T09:29:05Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289863#M34918</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think you need to enable the esdhc2 clock first.&lt;/P&gt;&lt;P&gt;For more details, please read the i.MX25 reference manual. Chapter 15.3.3.4 Clock Gating Control Register 0 (CGCR0).&lt;/P&gt;&lt;P&gt;AHB Clock Gating[6]&amp;nbsp; ---&amp;nbsp; hclk_esdhc2&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2013 08:32:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289863#M34918</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-11-27T08:32:09Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289864#M34919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanking you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Set to ClockGatingControlRegister0 to use eSDHC2.&lt;/P&gt;&lt;P&gt;Besides, what is thought of?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Nov 2013 00:22:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289864#M34919</guid>
      <dc:creator>KatsumiKaneko</dc:creator>
      <dc:date>2013-11-29T00:22:07Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289865#M34920</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Please check the IOMUX. As you mentioned you will use eSDHC2, but your IOMUX setting is for eSDHC1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Dec 2013 03:20:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289865#M34920</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-12-02T03:20:18Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289866#M34921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanking you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry, that the reply is slow.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It stopped the setting of IOMUXC_SW_MUX_CTL_PAD_SD1_CMD and IOMUXC_SW_MUX_CTL_PAD_SD1_CLK.&lt;BR /&gt;However, the operation didn't change.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is using ATL2 mode in IOMUXC_SW_MUX_CTL_PAD_CSI_D6.&lt;BR /&gt;It is CMD of eSDHC2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is using ALT2 mode in IOMUXC_SW_MUX_CTL_PAD_CSI_D7.&lt;BR /&gt;It is CLK of eSDHC2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a problem in this setting?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Dec 2013 04:22:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289866#M34921</guid>
      <dc:creator>KatsumiKaneko</dc:creator>
      <dc:date>2013-12-06T04:22:45Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289867#M34922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jimmychan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;For&amp;nbsp; Question 1,&amp;nbsp; Could you please refer to the following,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="1007" data-containertype="700" data-objectid="315257" data-objecttype="1" href="https://community.freescale.com/thread/315257"&gt;https://community.freescale.com/thread/315257&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;It seems that the SDCLKEN bit doesn't exist in i.MX25.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;For Question 2,&amp;nbsp;&amp;nbsp; the customer found that although&amp;nbsp; the value of&amp;nbsp; Interrupt Status Register (IRQSTAT) is 0x00000000, the inturrpt handler is called.&amp;nbsp; Could you please help&amp;nbsp; the problem ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Yu &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Dec 2013 06:06:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289867#M34922</guid>
      <dc:creator>yuhe-r64908</dc:creator>
      <dc:date>2013-12-24T06:06:21Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289868#M34923</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;For the Q2, could you tell me more details ? what interrupt is called? which bit you expected to be 1 in IRQSTAT?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Dec 2013 06:49:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289868#M34923</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-12-24T06:49:46Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289869#M34924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kaneko-san,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Q2 ,&amp;nbsp; Could you please give the detailed info to Jimmychan ?&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt; what interrupt is called? which bit you expected to be 1 in IRQSTAT?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Yu &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Dec 2013 07:04:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289869#M34924</guid>
      <dc:creator>yuhe-r64908</dc:creator>
      <dc:date>2013-12-24T07:04:27Z</dc:date>
    </item>
    <item>
      <title>Re: Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289870#M34925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanking you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is as the following in the details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;・The interruption is 8th of the interrupt vector (eSDHC2).&lt;BR /&gt;・It occurs by the communication of CMD53.&lt;BR /&gt;・The communication of CMD53 has ended.&lt;/P&gt;&lt;P&gt;・It is not each time but the occurring frequency is high.&lt;BR /&gt;・It expects Card interrupt but Interrupt Status Register (IRQSTAT) is 0x00000000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It attaches the screen shot of the occurrence time.&lt;BR /&gt;The tool is EWARM.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Dec 2013 07:15:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289870#M34925</guid>
      <dc:creator>KatsumiKaneko</dc:creator>
      <dc:date>2013-12-24T07:15:00Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289871#M34926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Hi Jimmychan,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;The customer has been waiting for your solution.&amp;nbsp; Could you please help it ASAP ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Yu &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jan 2014 01:28:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289871#M34926</guid>
      <dc:creator>yuhe-r64908</dc:creator>
      <dc:date>2014-01-06T01:28:04Z</dc:date>
    </item>
    <item>
      <title>Re: Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289872#M34927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the Reference manual,&lt;/P&gt;&lt;P&gt;" In 4-bit mode, the card interrupt signal is sampled during the interrupt cycle, which may introducing some delay between the interrupt signal from the SDIO card and the interrupt to the host system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Writing 1 to this bit clears it, but if the interrupt factor from the SDIO card is not cleared then the bit is immediately set again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;&lt;SPAN style="color: #3366ff; text-decoration: underline;"&gt;When CINT has been set to 1, it is the host driver’s responsibility to clear the card interrupt signal enable bit in the interrupt signal enable register, so that the eSDHC stops driving the interrupt while it is being serviced.&lt;/SPAN&gt;&lt;/SPAN&gt; After the card interrupt service is completed, and the interrupt factors in the SDIO card have been reset, then the host driver can write 1 to clear this bit and set the card interrupt signal enable to 1. This causes the eSDHC to restart sampling the interrupt signal. "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In you ISR, have you clear the "card interrupt signal enable bit"? &lt;/P&gt;&lt;P&gt;so the eSDHC stops driving the interrupt while it is being serviced.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jan 2014 06:56:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289872#M34927</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2014-01-06T06:56:09Z</dc:date>
    </item>
    <item>
      <title>Re: Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289873#M34928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanking you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt; In you ISR, have you clear the "card interrupt signal enable bit"? &lt;/P&gt;&lt;P&gt;Yes.&lt;BR /&gt;It clears the CINTIEN bit of Interrupt Signal Enable Register and CINTSEN bit of Interrupt Status Enable Register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The processing is as the following.&lt;/P&gt;&lt;P&gt;1:The card interrupt occurrence.&lt;BR /&gt;2:In ISR clears the CINTIEN bit of Interrupt Signal Enable Register and CINTSEN bit of Interrupt Status Enable Register.&lt;BR /&gt;3:Writes interrupt factor clear in the SDIO card using CMD52.&lt;BR /&gt;4:Confirms interrupt clearance in the SDIO card using CMD52.&lt;BR /&gt;5:Reads data using CMD53.(data size is 1.5Kbytes)&lt;BR /&gt;6:Sets the CINTIEN bit of Interrupt Signal Enable Register and CINTSEN bit of Interrupt Status Enable Register.&lt;BR /&gt;7:The card interrupt occurrence.(Interrupt Status Register is 0x00000000)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that it occurs when the DAT1 signal becomes LOW before the 6th processing.&lt;BR /&gt;When doing the 6th processing between the 4th and the 5th, the frequency falls.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Kaneko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jan 2014 08:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289873#M34928</guid>
      <dc:creator>KatsumiKaneko</dc:creator>
      <dc:date>2014-01-06T08:04:53Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289874#M34929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kaneko-san,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please check &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Jimmychan&lt;/SPAN&gt;'s comments and give the feedback ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jan 2014 08:05:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289874#M34929</guid>
      <dc:creator>yuhe-r64908</dc:creator>
      <dc:date>2014-01-06T08:05:57Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289875#M34930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Hi Jimmychan,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;Could you please check and help with it ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Yu&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jan 2014 01:35:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289875#M34930</guid>
      <dc:creator>yuhe-r64908</dc:creator>
      <dc:date>2014-01-08T01:35:46Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289876#M34931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi yuhe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't have any new idea for this issue. I will try to ask an expert for help this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jan 2014 01:47:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289876#M34931</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2014-01-08T01:47:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289877#M34932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jimmychan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Hope the issue can be solved ASAP.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Yu&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jan 2014 05:35:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289877#M34932</guid>
      <dc:creator>yuhe-r64908</dc:creator>
      <dc:date>2014-01-09T05:35:06Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289878#M34933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Hi Jimmychan,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any update to this issue ?&amp;nbsp;&amp;nbsp;&amp;nbsp; If needed, could you escalate the issue to R&amp;amp;D ? since the customer has been waiting for the solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jan 2014 01:54:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289878#M34933</guid>
      <dc:creator>yuhe-r64908</dc:creator>
      <dc:date>2014-01-14T01:54:02Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289879#M34934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had escalated this issue to the expert team. I will try to ask them for help again to speed up the process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jan 2014 02:11:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289879#M34934</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2014-01-14T02:11:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289880#M34935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Hi Jimmychan,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Any progress on the issue ?&amp;nbsp; Is a CT ticket assigned ?&lt;/P&gt;&lt;P&gt;&amp;nbsp; Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Yu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jan 2014 08:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289880#M34935</guid>
      <dc:creator>yuhe-r64908</dc:creator>
      <dc:date>2014-01-23T08:25:51Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX25 SDIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289881#M34936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;sorry, I cannot create CT ticket. May need help from &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/karinavalencia"&gt;karinavalencia&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jan 2014 08:44:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX25-SDIO/m-p/289881#M34936</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2014-01-23T08:44:33Z</dc:date>
    </item>
  </channel>
</rss>