<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSD2_CLK not detected in mx53 based design with customized R10.4 BSP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SD2-CLK-not-detected-in-mx53-based-design-with-customized-R10-4/m-p/289845#M34916</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My board is based on mx53_smd ref design. A WLAN module is connected to SD2 interface. It is detected as SDIO device. This SD2 is configured without card detection. It is configured as mmc2 device and card_inserted_state is hardcoded as 1 in mxc_mmc_platform_data mmc2 structure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I'm unable to detect the SD2_CLK . I have made no other changes in the BSP regarding this section.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it the driver that should load the device? Then only the CLK will be provided??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please share your thoughts&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Jun 2013 07:01:14 GMT</pubDate>
    <dc:creator>Mats1z</dc:creator>
    <dc:date>2013-06-13T07:01:14Z</dc:date>
    <item>
      <title>SD2_CLK not detected in mx53 based design with customized R10.4 BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SD2-CLK-not-detected-in-mx53-based-design-with-customized-R10-4/m-p/289845#M34916</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My board is based on mx53_smd ref design. A WLAN module is connected to SD2 interface. It is detected as SDIO device. This SD2 is configured without card detection. It is configured as mmc2 device and card_inserted_state is hardcoded as 1 in mxc_mmc_platform_data mmc2 structure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I'm unable to detect the SD2_CLK . I have made no other changes in the BSP regarding this section.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it the driver that should load the device? Then only the CLK will be provided??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please share your thoughts&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2013 07:01:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SD2-CLK-not-detected-in-mx53-based-design-with-customized-R10-4/m-p/289845#M34916</guid>
      <dc:creator>Mats1z</dc:creator>
      <dc:date>2013-06-13T07:01:14Z</dc:date>
    </item>
  </channel>
</rss>