<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX233 boot from SPI flash</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX233-boot-from-SPI-flash/m-p/289274#M34710</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;0x80501003 is ERROR_ROM_LDR_SIGNATURE, that means image is not properly flashed. &lt;/P&gt;&lt;P&gt;The image header has incorrect signature. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x80502008 means&amp;nbsp; ERROR_ROM_USB_CONNECT_TIMEOUT&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the boot ROM is unable to boot from the device, indicated by the boot mode &lt;/P&gt;&lt;P&gt;(SD, NAND), then it falls back to the USB interface. This error code indicates &lt;/P&gt;&lt;P&gt;that the USB boot failed as well.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Mar 2013 02:42:18 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2013-03-11T02:42:18Z</dc:date>
    <item>
      <title>iMX233 boot from SPI flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX233-boot-from-SPI-flash/m-p/289273#M34709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to boot from SPI flash on imx233. I prepared a sb file with bootlet and kernel and programmed it to a SPI flash. The SPI flash is connected to SPI1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I already set boot mode to boot from SPI1, but I get &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x80502008&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; H0x80501003&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder if someone can give me any advise on it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;JJ&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Mar 2013 22:09:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX233-boot-from-SPI-flash/m-p/289273#M34709</guid>
      <dc:creator>PotatoChip</dc:creator>
      <dc:date>2013-03-09T22:09:44Z</dc:date>
    </item>
    <item>
      <title>Re: iMX233 boot from SPI flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX233-boot-from-SPI-flash/m-p/289274#M34710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;0x80501003 is ERROR_ROM_LDR_SIGNATURE, that means image is not properly flashed. &lt;/P&gt;&lt;P&gt;The image header has incorrect signature. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x80502008 means&amp;nbsp; ERROR_ROM_USB_CONNECT_TIMEOUT&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the boot ROM is unable to boot from the device, indicated by the boot mode &lt;/P&gt;&lt;P&gt;(SD, NAND), then it falls back to the USB interface. This error code indicates &lt;/P&gt;&lt;P&gt;that the USB boot failed as well.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2013 02:42:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX233-boot-from-SPI-flash/m-p/289274#M34710</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-03-11T02:42:18Z</dc:date>
    </item>
    <item>
      <title>Re: iMX233 boot from SPI flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX233-boot-from-SPI-flash/m-p/289275#M34711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I programmed .sb file to a spi flash programmer and other thread said that program sb file to address 0x00 is what needed to be done. I don't know why it give 0x80501003 error. Any suggestion?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Mar 2013 17:02:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX233-boot-from-SPI-flash/m-p/289275#M34711</guid>
      <dc:creator>PotatoChip</dc:creator>
      <dc:date>2013-03-13T17:02:02Z</dc:date>
    </item>
    <item>
      <title>Re: iMX233 boot from SPI flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX233-boot-from-SPI-flash/m-p/289276#M34712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Note, i.MX23 SPI bootloader supports only 2-byte addresses for EEPROMs and 3-byte addresses for NORs.&lt;/P&gt;&lt;P&gt;Next, please check if optional configuration block is located (and correct) &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;at byte address 0, as described &lt;BR /&gt;&lt;/SPAN&gt;in section 35.6.1 (Media Format) of the i.MX23 Reference Manual.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Mar 2013 11:08:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX233-boot-from-SPI-flash/m-p/289276#M34712</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-03-27T11:08:31Z</dc:date>
    </item>
  </channel>
</rss>