<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCRC Unit in SDMA</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CRC-Unit-in-SDMA/m-p/289011#M34602</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Did somebody used the CRC Unit in the SDMA Core of the i.mx53? I actually tried, but can't access them like Burst or Per Functional Registers via stf/ldf instructions. Something like : &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; stf Greg[3],CA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # Greg3 preloaded with 2 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ( Hex-Inst. =&amp;gt; 0x6b80 )&lt;/P&gt;&lt;P&gt;to load the Polynomial Register (CA) did not work. Where could be the Bug?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;some hint's will be very helpful&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards &lt;/P&gt;&lt;P&gt;Lars&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Mar 2013 16:28:08 GMT</pubDate>
    <dc:creator>larstraeger</dc:creator>
    <dc:date>2013-03-08T16:28:08Z</dc:date>
    <item>
      <title>CRC Unit in SDMA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CRC-Unit-in-SDMA/m-p/289011#M34602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Did somebody used the CRC Unit in the SDMA Core of the i.mx53? I actually tried, but can't access them like Burst or Per Functional Registers via stf/ldf instructions. Something like : &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; stf Greg[3],CA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # Greg3 preloaded with 2 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ( Hex-Inst. =&amp;gt; 0x6b80 )&lt;/P&gt;&lt;P&gt;to load the Polynomial Register (CA) did not work. Where could be the Bug?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;some hint's will be very helpful&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards &lt;/P&gt;&lt;P&gt;Lars&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Mar 2013 16:28:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CRC-Unit-in-SDMA/m-p/289011#M34602</guid>
      <dc:creator>larstraeger</dc:creator>
      <dc:date>2013-03-08T16:28:08Z</dc:date>
    </item>
    <item>
      <title>Re: CRC Unit in SDMA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CRC-Unit-in-SDMA/m-p/289012#M34603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Lars, have you tried following the steps of table 66-5 of the i.MX53 RM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Apr 2013 03:06:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CRC-Unit-in-SDMA/m-p/289012#M34603</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-04-16T03:06:17Z</dc:date>
    </item>
    <item>
      <title>Re: CRC Unit in SDMA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CRC-Unit-in-SDMA/m-p/289013#M34604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Grant,&lt;/P&gt;&lt;P&gt; yes i use the recommendet order. first load CA, then init CS and process data. But everytime i read 0x00 from the CS Register.&lt;/P&gt;&lt;P&gt;I also tried to load the CA register with a value (0x2)&amp;nbsp; and read it back after channel script finished from the channel context area. But the value was 0x00. So i think i use the wrong opcodes for CRC ldf/stf instructions? &lt;/P&gt;&lt;P&gt;Is the opcode/hex-inst. right?:&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; stf Greg[3],CA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # Greg3 preloaded with 2 &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ( Hex-Inst. =&amp;gt; 0x6b80 )&lt;/P&gt;
&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lars&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Apr 2013 07:41:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CRC-Unit-in-SDMA/m-p/289013#M34604</guid>
      <dc:creator>larstraeger</dc:creator>
      <dc:date>2013-04-16T07:41:53Z</dc:date>
    </item>
  </channel>
</rss>