<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: uImage for  mfgtool in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/uImage-for-mfgtool/m-p/288954#M34591</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kyle,&lt;/P&gt;&lt;P&gt;The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware is used for mfgtool. You can use default supplied in mfgtool by freescale, or you can generate it through manually build BSP. The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\file is the kernel uImage ,when you have completed building BSP by LTIB, the kernel image and the U-Boot images are located at: rootfs/boot/. Hope this can help you ~~&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Nov 2013 05:50:36 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2013-11-20T05:50:36Z</dc:date>
    <item>
      <title>uImage for  mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uImage-for-mfgtool/m-p/288953#M34590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone know where I could find the source for the uImage use in the mfgtool. It is found in Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware. Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kyle&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2013 23:53:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uImage-for-mfgtool/m-p/288953#M34590</guid>
      <dc:creator>kylekenj</dc:creator>
      <dc:date>2013-11-19T23:53:11Z</dc:date>
    </item>
    <item>
      <title>Re: uImage for  mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uImage-for-mfgtool/m-p/288954#M34591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kyle,&lt;/P&gt;&lt;P&gt;The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware is used for mfgtool. You can use default supplied in mfgtool by freescale, or you can generate it through manually build BSP. The uImage under Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\file is the kernel uImage ,when you have completed building BSP by LTIB, the kernel image and the U-Boot images are located at: rootfs/boot/. Hope this can help you ~~&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Nov 2013 05:50:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uImage-for-mfgtool/m-p/288954#M34591</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2013-11-20T05:50:36Z</dc:date>
    </item>
  </channel>
</rss>