<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: iMX6 and eMMC 4.5</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Re-iMX6-and-eMMC-4-5/m-p/288818#M34581</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MMC 4.4.1 is using in Customized imx6 board as boot device, after booting android (R13_04_ga), media files are detecting from MMC, SD, and USB taking long time also all applications taking long time for loading.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for eMMC is selected as default storage, changes are done in "vold.fstab" file,&lt;/P&gt;&lt;P&gt;if i select SD card as boot device, media files are detecting very fast, what are the changes i have to done for MMC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kalil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Apr 2013 09:04:22 GMT</pubDate>
    <dc:creator>mohamedkalilull</dc:creator>
    <dc:date>2013-04-22T09:04:22Z</dc:date>
    <item>
      <title>Re: iMX6 and eMMC 4.5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Re-iMX6-and-eMMC-4-5/m-p/288818#M34581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MMC 4.4.1 is using in Customized imx6 board as boot device, after booting android (R13_04_ga), media files are detecting from MMC, SD, and USB taking long time also all applications taking long time for loading.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for eMMC is selected as default storage, changes are done in "vold.fstab" file,&lt;/P&gt;&lt;P&gt;if i select SD card as boot device, media files are detecting very fast, what are the changes i have to done for MMC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kalil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Apr 2013 09:04:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Re-iMX6-and-eMMC-4-5/m-p/288818#M34581</guid>
      <dc:creator>mohamedkalilull</dc:creator>
      <dc:date>2013-04-22T09:04:22Z</dc:date>
    </item>
  </channel>
</rss>