<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6Q RWS_EN for Bayer/Raw image capture in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-RWS-EN-for-Bayer-Raw-image-capture/m-p/288790#M34568</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is just another way to do it,&amp;nbsp; the IPU it is very flexible and allows different ways to get the same task. So the we use in the BSP&amp;nbsp; the general way to do it, but can be done just like you mention&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Sep 2013 13:55:33 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2013-09-20T13:55:33Z</dc:date>
    <item>
      <title>i.MX6Q RWS_EN for Bayer/Raw image capture</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-RWS-EN-for-Bayer-Raw-image-capture/m-p/288789#M34567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Section 37.5.142 of the Reference Manual (IPUx_IC_CONF) refers to RWS_EN (Raw Sensor Enable).&amp;nbsp; It looks like this and &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;CSI_MEM_WR_&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;EN need to be set correctly to enable raw/Bayer/Monochrome sensors.&amp;nbsp; Yet I don't see this setting being set in the CSI_MEM case in the enable tasks method of ipu_ic.&amp;nbsp; Is this setting necessary to enable raw image capture, or is there another way to do it?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2013 18:04:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-RWS-EN-for-Bayer-Raw-image-capture/m-p/288789#M34567</guid>
      <dc:creator>davemcmordie</dc:creator>
      <dc:date>2013-09-03T18:04:07Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6Q RWS_EN for Bayer/Raw image capture</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-RWS-EN-for-Bayer-Raw-image-capture/m-p/288790#M34568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is just another way to do it,&amp;nbsp; the IPU it is very flexible and allows different ways to get the same task. So the we use in the BSP&amp;nbsp; the general way to do it, but can be done just like you mention&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Sep 2013 13:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6Q-RWS-EN-for-Bayer-Raw-image-capture/m-p/288790#M34568</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2013-09-20T13:55:33Z</dc:date>
    </item>
  </channel>
</rss>