<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 SD2 Card Detect pin disable in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SD2-Card-Detect-pin-disable/m-p/288756#M34562</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&amp;nbsp; friends,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Right now we designed a i.MX6 Solo board with a Wifi Module (RTL8189es) wired to the SD2 bus.&amp;nbsp; However, we did not know which SD2_CD_B pin should be used and our module does not require that pin either.&amp;nbsp; In that case, we let NANDF_D2 (used in the SABRESD EVB) and GPIO_4 (listed in the reference manual) float.&amp;nbsp; Later on we discovered that there is an error message output "uSDHC1: No card-detect pin available!" message on the boot log output.&amp;nbsp; In addition, the system seems to have to problem to recognize there is a Wifi module plugged into SD2 bus.&amp;nbsp; Is there anyway we could fix this by letting the system know the module is plugged in the software?&amp;nbsp; Any help is greatly appreciated!&amp;nbsp; We are running Android 4.0.4 on a board similar to i.MX6 Sabresd EVB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vincent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Jan 2014 01:22:42 GMT</pubDate>
    <dc:creator>vincentchou</dc:creator>
    <dc:date>2014-01-07T01:22:42Z</dc:date>
    <item>
      <title>i.MX6 SD2 Card Detect pin disable</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SD2-Card-Detect-pin-disable/m-p/288756#M34562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&amp;nbsp; friends,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Right now we designed a i.MX6 Solo board with a Wifi Module (RTL8189es) wired to the SD2 bus.&amp;nbsp; However, we did not know which SD2_CD_B pin should be used and our module does not require that pin either.&amp;nbsp; In that case, we let NANDF_D2 (used in the SABRESD EVB) and GPIO_4 (listed in the reference manual) float.&amp;nbsp; Later on we discovered that there is an error message output "uSDHC1: No card-detect pin available!" message on the boot log output.&amp;nbsp; In addition, the system seems to have to problem to recognize there is a Wifi module plugged into SD2 bus.&amp;nbsp; Is there anyway we could fix this by letting the system know the module is plugged in the software?&amp;nbsp; Any help is greatly appreciated!&amp;nbsp; We are running Android 4.0.4 on a board similar to i.MX6 Sabresd EVB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vincent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jan 2014 01:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SD2-Card-Detect-pin-disable/m-p/288756#M34562</guid>
      <dc:creator>vincentchou</dc:creator>
      <dc:date>2014-01-07T01:22:42Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 SD2 Card Detect pin disable</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SD2-Card-Detect-pin-disable/m-p/288757#M34563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can check SDHC configuration in your board file&lt;/P&gt;&lt;P&gt;static const struct esdhc_platform_data mx6q_sabresd_sd2_data __initconst = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .cd_gpio = SABRESD_SD2_CD,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .wp_gpio = SABRESD_SD2_WP,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .keep_power_at_suspend = 1,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .support_8bit = 1,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .delay_line = 0,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .cd_type = ESDHC_CD_CONTROLLER,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .runtime_pm = 1,&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;enum cd_types {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ESDHC_CD_NONE,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* no CD, neither controller nor gpio */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ESDHC_CD_CONTROLLER,&amp;nbsp;&amp;nbsp;&amp;nbsp; /* mmc controller internal CD */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ESDHC_CD_GPIO,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* external gpio pin for CD */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ESDHC_CD_PERMANENT,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* no CD, card permanently wired to host */&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can consider set cd_type as ESDHC_CD_PERMANENT&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jan 2014 07:53:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SD2-Card-Detect-pin-disable/m-p/288757#M34563</guid>
      <dc:creator>lily_zhang</dc:creator>
      <dc:date>2014-01-07T07:53:09Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 SD2 Card Detect pin disable</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SD2-Card-Detect-pin-disable/m-p/288758#M34564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI!&amp;nbsp; Xiaoli,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Happy Chinese New Year!&amp;nbsp; We did follow the same configuration as EMMC and set the SD2.&amp;nbsp; Thanks a lot!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vincent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jan 2014 22:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SD2-Card-Detect-pin-disable/m-p/288758#M34564</guid>
      <dc:creator>vincentchou</dc:creator>
      <dc:date>2014-01-30T22:40:46Z</dc:date>
    </item>
  </channel>
</rss>